- Precise Time Synchronization according to IEEE 1588
- High Availability Seamless Redundancy (HSR) and Parallel Redundancy Protocol (PRP) according to IEC 62439-3
- Reduced risk of downtime and communication disruption
- Certified for Electric Power, Transportation and Oil & Gas markets
Siemens is expanding its Ruggedcom portfolio with two new compact Ethernet switches. The Ruggedcom RSG907R and the Ruggedcom RSG909R compact Gigabit IEEE 1588 compatible Ethernet switches support HSR and PRP according to the IEC 62439-3 standard. At a time when the electric power industry worldwide is rapidly transitioning to fully digital systems, such as digital substations, the Ruggedcom RSG907R and the Ruggedcom RSG909R help to avoid revenue loss by mitigating the risk of communication disruptions and downtime with a redundant fault tolerant network supporting high bandwidth. In addition to the seamless redundancy Ethernet networking features the device is equipped with redundant power supply inputs for additional reliability. The RSG907R and RSG909R come with a comprehensive set of approvals enabling digitalization in Electric Power, Transportation and Oil & Gas markets.
- High bandwidth to handle growing amounts of data
- Ideal for digital substations, transportation and oil & gas industries
- Built-to-order with simplified field installation and modification
Siemens is expanding its Ruggedcom portfolio with a new Ethernet 19 inch rack switch. The Ruggedcom RST2228 is a rugged Layer 2 rack switch with 4 integrated 1/10 Gbit/s uplinks and up to 24 field modular 10/100/1000 Mbit/s interfaces supporting IEEE 1588 Transparent Clock. Its high port density helps significantly reduce capital expenses by reducing the number of network devices needed. The combination of precision timing and network communication on a single network eliminates maintenance costs related to timing solutions that require dedicated wiring. The device is rugged rated and features an operating temperature from -40 to +85 degrees Celsius, as well as Electromagnetic interference (EMI) immunity. The product can be used in the harsh environments of Electric Power, Transportation and Oil & Gas industries and is ideal to handle ever growing amounts of data.
- Joint research project launched
- Test plant will produce "green" chemistry and serve as an energy store for eco-electricity
- First plants will have potential to produce 20,000 tonnes a year
Evonik and Siemens are planning to use electricity from renewable sources and bacteria to convert carbon dioxide (CO2) into specialty chemicals. The two companies are working on electrolysis and fermentation processes in a joint research project called Rheticus. The project was launched today and is due to run for two years. The first test plant is scheduled to go on stream by 2021 at the Evonik facility in Marl, Germany which produces chemicals such as butanol and hexanol, both feedstocks for special plastics and food supplements, for example. The next stage could see a plant with a production capacity of up to 20,000 tonnes a year. There is also potential to manufacture other specialty chemicals or fuels. Some 20 scientists from the two companies are involved in the project.
Per January 1st, 2018 Siemens has rebranded and renamed its full subsidiary NEM Energy into Siemens Heat Transfer Technology (HTT). Siemens HTT is a specialist in the field of Heat Recovery Steam Generators for power plants.
- Diverse suite of financial solutions provide necessary capital to expand growing energy storage sector
- Granting customers access to a combination of proven, bankable energy storage solutions with tailored financing
- Leasing and project finance options for qualified projects using Fluence's industry-leading trio of energy storage platforms
Siemens Financial Services (SFS) and Fluence, a Siemens and AES company, announce a comprehensive financing program to support customers in their investments in energy storage solutions. The new financing program will offer customers leasing and project finance options for qualified projects using Fluence's industry-leading trio of energy storage platforms. Fluence's combination of unmatched energy storage experience, proven technical solutions, and the availability of tailored financial solutions will further drive down the total system costs of energy storage and accelerate the growth of this dynamic segment of the power market, estimated by Bloomberg New Energy Finance (BNEF) to be a $100 billion market opportunity by 2030.
- Metro Line to connect Ahmedabad in two corridors
- Order volume worth more than €76 million
The Indian mass-transit operator Metro Link Express for Gandhinagar and Ahmedabad (MEGA) has commissioned Siemens to electrify a 39.2-kilometer metro line in the Indian metropolis Ahmedabad. The line, currently under construction, will run in Ahmedabad city in two corridors, East-West and North-South.
- The world’s first 1,100 kv transformer for the world’s largest HVDC project in China
- Development, manufacturing and testing in the lead factory in Nuremberg
- The world’s most powerful HVDC transformer with 587 MVA
The world’s first transformer, which Siemens developed and manufactured for high-voltage direct-current (HVDC) transmission systems with what is currently the highest transmission voltage of ± 1,100 kilovolts (kV), recently passed its type test. Siemens developed, manufactured and tested the HVDC transformer in its transformer factory in Nuremberg. It is the first of a total of seven ±1,100 kV transformers that Siemens and a partner company are building for what is currently the world’s largest HVDC transmission system. This type of transformer is among the most powerful single-phase units in the world, with a transmission capacity of 587.1 megavolt amperes (MVA). Siemens is building the transformers in its network of factories led by its Nuremberg plant, in cooperation with its factory for HVDC transformers in Guangzhou, China, as well as another Chinese partner. These factories are manufacturing the machines according to the specifications and documentation of the lead factory in Nuremberg. Commissioning of the world’s largest HVDC link – and thus also the transformers – is scheduled for 2018.
Talks were held yesterday in Munich between Michael Kretschmer, Prime Minister of the German state of Saxony, and Joe Kaeser, President and CEO of Siemens AG. The two leaders had a good, constructive dialogue in which both sides expressed their understanding of the business and political framework conditions. The conversation took place in an open and trust-based atmosphere.
LO3 Energy, an energy-tech company set to disrupt energy grids across the globe, announced an investment from Siemens closing out its series A. In late 2015 Siemens and LO3 started collaborating on projects beginning with the Brooklyn Microgrid. Self-sufficient microgrids play an important role in an energy market that is growing through distributed energy systems — whether they are based on wind, sun, water or biomass — such grids are becoming increasingly significant. LO3 Energy is benefiting from Siemens' development of microgrids such as the one that has been operating in Wildpoldsried, a village in southern Germany, since 2014. While the Brooklyn Microgrid continues to grow, insights from the proliferation of the prosumers and consumers provides Siemens the rationale for building resilient grid systems based on local marketplaces. To date, the initial project has attracted more than 60 community members participating in the Brooklyn Microgrid, and LO3 and Siemens expect to partner on further projects across the globe. Specific terms of the investment were not disclosed.
- Order volume totals €380 million
- 13-year service agreement
Siemens has received an order from its customer Nizhnekamskneftekhim to build a combined cycle power plant on a turnkey basis in Tatarstan. Nizhnekamskneftekhim is a member of the TAIF Group headquartered in Kazan, Tatarstan, Russia. The corresponding contract was signed today by Azat Bikmurzin, General Director of Nizhnekamskneftekhim, and the CEO of Siemens Russia Dietrich Moeller in the presence of the President of Tatarstan His Excellency Rustam Minnikhanov, Deputy Prime Minister of Bavaria Ilse Aigner, TAIF CEO Albert Shigaboutdinov and Siemens CEO Joe Kaeser.