Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release22 January 2018Process Industries and DrivesNuremberg
A high port density IEEE 1588 Ethernet switch simplifies migration to fiber optic networks
The picture shows the Ruggedcom RST2228 Switch.
The 24 10/100/1000 Mbit/s interfaces are field modular based on 6 module slots, each of which can support 4 interfaces. The product can be ordered pre-configured with modules installed, but also allows for quick in-field set-up and modifications with the separately orderable media modules Ruggedcom RMM2973-4RJ45, RMM2973-4FC and RMM2972-4SFP. This enables simplified migration from copper to fiber optic networks – one of the major challenges of digitalization. Further savings can be found by purchasing only the necessary modules for the RST2228 to meet the immediate need.
For further information, refer to www.siemens.com/rst2228
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 7-26616