- Real-time data analysis from 29 gas turbines across multiple locations will increase availability, reduce forced outages and enable proactive, prescriptive maintenance
- Digitalization to improve availability, efficiency, productivity and flexibility
Siemens will install state-of-the-art Remote Diagnostic Services (RDS) for GAIL (India) Limited covering 29 gas turbines operating across the Hazira-Vijaipur-Jagdishpur (HVJ) pipeline and the Vijaipur C2/C3 Plant. The scope includes the supply of RDS hardware, site installation and commissioning including remote Operational Service Desk (OSD) and helpdesk services. The OSD will be accessible 24/7, equipped with machine learning tools and manned by technical experts to provide faster, high quality troubleshooting and guidance for problem resolution.
- Designed to optimize customers' asset value and performance for coal and steam-based power plants
- Siemens experts will work alongside customers to co-create solutions that help deliver higher efficiency, reliability and flexibility in operations
Siemens experts will work alongside customers to co-create solutions that help deliver higher efficiency, reliability and flexibility in operationsSiemens has officially opened its new MindSphere Application Center in India. The facility is a state-of-the-art digitalized technology center, supported by Siemens’ MindSphere, an open, cloud-based IoT operating system that lets customers connect machines and physical infrastructure to the digital world and their thermodynamic digital twins.
The Siemens Zug campus features a new office building with 1,000 work spaces and a newly constructed production building. The Siemens Zug campus is one of the first new projects to use Building Information Modeling (BIM) for design and construction. The campus complex is equipped with building automation, security and fire safety technology from Siemens BT and particular emphasis was placed on sustainability and energy efficiency of the buildings.
On September 26, 2017 Siemens and Alstom have signed a Memorandum of Understanding to combine Siemens' mobility business, including its rail traction drives business, with Alstom. The transaction brings together two innovative players of the railway market with unique customer value and operational potential. The two businesses are largely complementary in terms of activities and geographies. Siemens will receive newly issued shares in the combined company representing 50 percent of Alstom's share capital on a fully diluted basis.On February 6, 2019 the European Commission has announced its decision to prohibit the proposed combination of the Siemens and Alstom mobility businesses. As a result of this prohibition, the merger will not proceed. Siemens and Alstom regret that the remedies they offered, including recent improvements, have been considered insufficient by the EU Commission.
The Fund for the Future that Siemens and the company’s Central Works Council agreed to establish in May 2018 is now available to finance qualification projects in Germany. Until the end of fiscal 2022, Siemens will provide up to €100 million for such projects, in addition to the company’s regular annual budget of around €500 million for training and continuing education, thereof €290 million in Germany. The Fund for the Future is a key element with which Siemens and the Central Works Council are shaping the structural transformation of today’s economy – a transformation that is changing the working world to an unimaginable degree. Siemens, the company's Central Works Council and the IG Metall labor union agreed on a Future Pact in May 2018. This pact, which includes the Fund for the Future, established the main framework for addressing the structural transformation now taking place in Germany.
Additive manufacturing has the potential to become a new key technology. For example it opens up new attractive prospects in the manufacture of gas turbines. This is why Siemens has been investing in this innovative technology right from its inception, and is now driving the industrialization and commercialization of these processes. Additive Manufacturing is a process that builds parts layer-by-layer from sliced CAD models to form solid objects. This enables highly precise solutions to be formed from powdered high-performance materials. Siemens is a pioneer in Additive Manufacturing and already uses the technology for rapid prototyping. Furthermore the company is now developing solutions ready for series-production for manufacturing gas turbine burner nozzles and repairing burner heads. Just recently Siemens achieved yet another breakthrough: the first gas turbine blades ever to be produced using Additive Manufacturing have successfully finished performance testing under full-load conditions.
The need for electromobility is growing, as is the need for an efficient charging infrastructure. As a pioneer in electromobility, Siemens has global experience, maintains a strong portfolio along the entire value chain, and plays an active role in advancing the development and standardization of charging solutions worldwide.Siemens is part of the "FastCharge" research project together with BMW Group as consortium leader, Allego GmbH, Phoenix Contact E-Mobility GmbH as well as Dr. Ing. h.c. F. Porsche AG. This project is investigating the technological requirements that vehicles and infrastructure must meet in order to be able to use extremely high charging capacities. The industrial companies involved in the research project presented the latest advancements in the field of fast and convenient energy supply for electrically powered vehicles on December 12, 2018. The prototype of a charging station with a capacity of up to 450 kW was inaugurated in Jettingen-Scheppach, Bavaria. At this ultra-fast charging station, electrically powered research vehicles created as part of the project are able to demonstrate charging times of less than three minutes for the first 100 kilometres of range or 15 minutes for a full charge (10-80 % State of Charge (SOC)).The energy supply system of Siemens used in the project contains both high-power electronics for the charging connections as well as the communication interface to the electric vehicles. For the connection to the public power grid, a charging container was implemented with two charging connections for CCS-compatible vehicles. One connection has an unprecedented charging capacity of max. 450 kW while the second can deliver up to 175 kW.
South-west Germany is counting on Siemens: from 2020 onward, DB Regio AG will be operating its Rhine Valley rail network exclusively with new trains from Siemens. The German Railways order covers 15 Desiro HC and 24 Mireo trains in total, and goes hand in hand with a restructuring of the rail transport services in the Rhine Valley. There is a clear separation between a rapid train system for fast cross-regional services and a regional suburban rail system (S-Bahn) with stops at all stations. The Mireo will be deployed as a regional train (RB) service along the line section from Offenburg via Freiburg to Basel/Neuenburg (Switzerland) as well as in the Kaiserstuhl area on Sundays between Freiburg and Endingen/Breisach. The line section from Karlsruhe via Offenburg and Freiburg to Basel (Switzerland) will be operated with the Desiro HC as a regional express service.
- Siemens successfully completed the first phase of its shallow water test of the Subsea Power Grid.
- The development program was conducted in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge.
- This will be the world's first Subsea Power Grid for medium voltage power distribution using pressure compensated technology.
Siemens has successfully concluded the first phase of its Subsea Power Grid shallow water test in Trondheim, Norway. Siemens, in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge, is in the final stages of a program to develop a barrier-breaking system that will become the world’s first Subsea Power Grid designed for distribution of medium voltage power using pressure compensated technology.