In 2014, the Departments of Transportation of California, Illinois and Maryland ordered an initial lot of 34 Charger locomotives from Siemens, with an option for a total of 222 locomotives. The contract back then was valued at approximately €165 million ($225 million). Due to orders from other states as well as by the private rail operator All Aboard Florida, the total number of Chargers ordered amounts to 81 in 2017. The locomotives are deployed in corridors of the US states for regional and mainline trains travelling for Caltrains (California) as Amtrak Pacific Surfliner, in Washington as Amtrak Cascades and in Maryland with the regional network MARC. Under the "Brightline" brand, ten Chargers are being deployed in high-speed rail services between Miami and West Palm Beach; Orlando is due to follow at a later date.
- Digital service to ensure nearly 99% availability of the 82 RRX trains
- Predictive service and maintenance for over 32 years
- Test operations as of mid-2018 in 70,000 square meters of depot property
Today the cornerstone was laid in Dortmund-Eving, Germany, for the service and maintenance depot being built for the Rhine-Ruhr-Express (RRX) trains. Test operations at the depot are scheduled to begin in mid-2018. In the future, all 82 RRX trains will be serviced and maintained here for a period of 32 years. Siemens will create 75 jobs for the depot and is investing a mid-double-digit-million euro sum in the facility.
- First order for 24 articulated trains based on the new Mireo platform
- 15 double-decker trainsets from the proven Desiro train family
- Commissioning in the summer of 2020
Beginning in 2020, DB Regio AG will operate its Rhine Valley rail network in southwest Germany exclusively with new trains supplied by Siemens. The mass transit arm of Deutsche Bahn has ordered 39 trainsets specifically for this purpose. The order comprises 15 Desiro HC and 24 Mireo trains. This marks the first order for the company's new articulated Mireo regional train platform that was recently premiered at Innotrans, the world's biggest rail trade fair.
- Multisystem locomotives equipped for the D-A-CH-I corridor
- Deliveries to begin in December 2017
- Initial service with SBB Cargo International
Together with the infrastructure fund of Reichmuth Infrastruktur Schweiz AG, the leasing company LokRoll AG has ordered 18 multisystem Vectron locomotives from Siemens. They will be used for cross-border operation along the Germany-Austria-Switzerland-Italy corridor. In addition to having national train control systems, all locomotives will also be equipped with the European Train Control System (ETCS). The locomotives will have a maximum output of 6,400 KW and a top speed of 160 km/h. LokRoll will lease the locomotives to the Swiss freight transport firm SBB Cargo International for a period of 15 years.
- Framework contract of up to 200 Vectron locomotives
- First tranche for 30 Vectron MS
- Delivery to begin in summer of 2018
Austrian Railways (ÖBB) has signed a framework contract with Siemens for the delivery of up to 200 Vectron locomotives. Under the contract, up to 100 alternating current (AC) locomotives, 50 alternating current (AC) locomotives with diesel power modules, and 50 multisystem (MS) locomotives can be called up. A firm order for 30 MS locomotives was placed at the signing. The locomotives will be built in the Siemens plant in Munich-Allach, Germany. The first units are to be delivered beginning in summer of 2018.
China's megacities alone are home to more than 260 million people. These gigantic conurbations have recently undergone rapid growth of almost two percent per year, and are suffering increasing traffic problems caused by the soaring rate of car use. Hence the correspondingly strong demand for solutions for the further development of urban rail transport. The Nanjing customer has now commissioned Siemens to equip metro Ninghe Line with the CBTC automatic train protection system Trainguard MT. The contract includes the CBTC trackside equipment for the 36 kilometer line as well as the ATC equipment of the 24 trains. In the long term more than ten metro lines will be built in Nanjing – of which five alone will or already been feature Siemens signaling technology.Siemens can look back on a long partnership in China with the Nanjing Metro Corporation. Siemens equipped metro line 1, which started running in 2005 and is now 47 kilometers long, as well as metro line 2 in 2010. Line 2 serves 26 stations and forms the east-west tangent of the city of Nanjing in eastern China. Following the extension of the city's metro with line 2, the rail network now covers 85 kilometers. Line 10, Nangjing's first cross-Yangtze river metro line was put into operation on July 1, 2014. Its first phase runs 23.6 kilometers with 14 stations. The latest Nanjing metro line fitted with signaling technology from Siemens is Nanjing Metro Line 3, which went on public operation on April 1, 2015.
The Velaro D is the fourth generation of high-speed trains that Siemens has developed on the basis of the Velaro platform. Deutsche Bahn AG (DB) classifies the train as the new Series 407 ICE 3 (predecessors: Series 403 and Series 406 ICE 3). In December 2013, Germany's Federal Railway Authority (EBA) approved the trains' operation – also in multiple-unit or so-called double-traction mode – on the Deutsche Bahn rail network. Passenger operation started on December 21, 2013.
Authorization for operation in single-traction mode in France was granted in April 2015. Since June 2015 the trains have been travelling to Paris in regular passenger operation. In addition to Germany and France, the Velaro D is also intended for cross-border operation in Belgium.
Since 2007, trains based on the Velaro platform have operated with high reliability for more than one billion kilometers in China, Russia, Spain and Turkey – equal to roughly 25,000 times around the globe.
- Light rail vehicles (LRVs) type S70 for Sound Transit's expanding system
- Serving the Greater Seattle and Central Puget Sound area
- Operator Sound Transit will nearly triple their fleet
Siemens has been awarded a contract to provide 122 new S70 light rail vehicles (LRVs) for Sound Transit, the regional transit system serving the Seattle and Central Puget Sound area in the US state of Washington. The order, the largest single contract in Sound Transit's history, will nearly triple the system's current fleet from today's 62 cars to 184. The S70s light rail vehicles will be built at the Siemens rail manufacturing hub in Sacramento, California. The fleet is expected to begin testing in 2019.
Our world is becoming increasingly digitalized – influencing everything from our communication with one another to the way we develop, produce and consume goods and services. The digitalization megatrend has not bypassed the rail sector. Siemens has kept pace here, too, and was exhibiting at the Innotrans 2016 with a focus on the digital transformation of rail transport.
Siemens will deliver 1,140 commuter rail carriages to the British capital. This is the largest order that Siemens has ever won in Great Britain and one of the biggest orders for Siemens' global rolling stock business. The first Desiro City train for the Thameslink network in Greater London was delivered and entered service in June 2016. By the end of 2018, a total of 115 trains will have been delivered. Siemens will take over the complete long-term servicing and maintenance for this new fleet of trains. The Thameslink north-south commuter route runs through London, connecting Bedford, located to the north east of the capital, with Brighton, on the south coast.
Introducing a high capacity, high frequency service of longer trains, extended platforms and new stations, the project is regarded as one of the largest rail infrastructure projects in the UK.