Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release29 September 2016MobilityMunich
122 light rail vehicles for Seattle and Central Puget Sound area

The new vehicles will be designed and built to help meet the needs of Sound Transit's growing light rail network and increasing ridership. The LRVs will feature a sleek appearance and include a more spacious interior with additional room for passengers. Additionally, the vehicles will include extra space for luggage and hooks to store up to four bicycles per vehicle.
"Passenger numbers in the Greater Seattle area are steadily climbing, and Sound Transit can adapt and further expand its traditionally excellent service with our modern light rail trains," said Jochen Eickholt, CEO of the Siemens Mobility Division. "I believe it's important that we can make this contribution toward expanding a highly efficient and environmentally friendly mass transit system in one of America's most dynamic metropolitan regions."
The new LRVs from Siemens are part of the 2008 voter-approved Sound Transit 2 Plan (ST2) which adds 30 miles of new light rail to create about a 50-mile regional system. With the new extensions, the Seattle-based system will stretch to Lynnwood in the north, cross Lake Washington to reach Bellevue and the Microsoft campus to the east and south to the Federal Way area.
Further information about the Mobility Division can be found at: www.siemens.com/mobility
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of gas and steam turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2015, which ended on September 30, 2015, Siemens generated revenue of €75.6 billion and net income of €7.4 billion. At the end of September 2015, the company had around 348,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Ellen Schramke
Siemens AG
Nonnendammallee 101
13629 Berlin
Germany
13629 Berlin
Germany
+49 (30) 386-22370