- €110 million contract to provide a fully automated yard management system
and maintenance services for the Kijfhoek marshalling yard
- Automated
and digital systems will optimize yard operations and improve efficiency,
reliability, and safety
- Kijfhoek is the
largest freight yard in the Netherlands and a vital link
between the Rotterdam ports and major industrial areas in Europe
Siemens Mobility has been
awarded a €110 million contract by ProRail B.V. to modernize and
optimize the Kijfhoek freight railyard, the largest yard in the
Netherlands and a vital link between the Rotterdam ports and major industrial
areas in Europe. This contract includes
providing a state-of-the-art fully automated system to manage yard operations and
15 years of maintenance services. Located south-east of
Rotterdam, the Kijfhoek marshalling yard encompasses 50 hectares, with 14 arrival
tracks, 41 classification tracks and 12 stabling tracks.
- Padam Mobility is a Software as a Service (SaaS) provider for
on-demand and paratransit software solutions
- Empowers cities and transit operators to make transportation
more efficient
- Acquisition
enhances Siemens Mobility's portfolio for intermodal mobility
Siemens Mobility is pleased to
announce that it has acquired Padam Mobility, a technology company that provides
AI-powered platforms and applications for on-demand and paratransit services. The
leading software as a service (SaaS) organization helps transit operators to
provide more efficient transportation in both urban and rural areas. This acquisition enhances Siemens Mobility's
intelligent infrastructure portfolio focused on intermodal transportation. It
supports transport operators in their effort to integrate and coordinate
different modes of transportation which seamlessly provides travel from the
first mile to the last.
- Consortium of Siemens Mobility and Stadler win €114.5 million contract for Lisbon Metro
- Siemens Mobility to install CBTC across three lines
- Stadler to supply a new fleet of modern trains
The consortium of Siemens Mobility and Stadler have won a €114.5 million contract to provide the Lisbon Metro with a state of the art signaling system and a new fleet of modern trains. Stadler will supply 14 three-car metro trains, while Siemens Mobility will install its Communications-Based Train Control (CBTC) system Trainguard MT on the Blue, Yellow and Green lines, and will upgrade the existing equipment. This will include installing its on-board CBTC technology across 70 trains of the existing fleet, as well as on the 14 new Stadler trains.
- CBTC signaling system to be implemented across five-kilometer
extension of Salvador Metro in Salvador, Bahia, Brazil
- The
automated signaling system will provide greater availability, enhanced
operations, and better passenger experience
Siemens Mobility has been awarded a contract by Companhia de
Transportes do Estado da Bahia to install a Communications-Based Train Control system (CBTC), GoA2, on
the extension of Line 1 in Salvador, Bahia, Brazil. The CBTC
signaling system will be fully implemented across the approximately
five-kilometer extension that will connect Pirajá to Águas Claras/Cajazeiras,
including two new stations. The full
integration of the extension to the existing Line 1 will provide
for greater availability, enhanced operations, and a better passenger
experience. This contract builds on the already
well-established relationship Siemens Mobility has with the Salvador Metro and
CCR Metrô Bahia.
The Berlin
Transport Association (BVG) and Siemens Mobility have signed a contract for the
construction of a Sicas ECC electronic interlocking at Alexanderplatz subway
station. The new interlocking is to cover the approximately 3.5-kilometer route
between the Rosa-Luxemburg-Platz and Spittelmarkt subway stations. In addition
to the indoor system, the scope of order includes new cables, a cable system
and around 150 K140 signals (main, pre, emergency and protection signals). The
line, which comprises a total of five stations, runs underground on two tracks
in a tunnel with a small clearance gauge. The project, which has a total volume
of around €13 million, will start laying cables in November 2021 and will be
completed in summer 2024.
Our state of the art Inspiro trains and Communications
Based Train Control (CBTC) Trainguard MT (TGMT) systems will serve the final
section of Line 3 of the Bulgarian capital, which was opened on the 24th
April 2020.
The products in Siemens Mobility trains meet the
highest cyber security standards. This was recently confirmed by TÜV SÜD, which
approved Siemens Mobility Rolling Stock with the IEC 62443 4-1 certificate.
This award confirms, 18 months after the IEC 62443 2-4 / 3-3 certification, the cyber
security throughout the entire product development process.
Media representatives got a first-hand impression of the new Vienna Metro during a test drive on the 14th April 2021 – in the presence of Public Transport City Councillor Peter Hanke, Wiener-Linien Managing Director Günter Steinbauer and Siemens Mobility CEO Arnulf Wolfram. After the successful approval of operation, the so-called 'X-Wagen' will be in use for all Viennese on the four lines U1 to U4 from 2022. With the completion of the new U5 in 2026, the new vehicles will also be running fully automatically.
S-Bahn Berlin GmbH has signed a framework contract with the consortium of Stadler Pankow GmbH and Siemens for the delivery of up to 1,380 vehicles. A firm order was placed for the first 106 trains. The 85 four-section and 21 two-section trains have a high triple-digit million-euro order volume. S-Bahn Berlin, a subsidiary of Deutsche Bahn, plans to use the new trains on the Ringbahn lines (S 41 and S 42) as well as on the system's southeastern feeder lines S 47, S 46 and S 8. These lines comprise roughly one-third of the entire S-Bahn network in Berlin. The first ten vehicles will be ready to enter service as of 2020. Subsequently, all remaining vehicles will be delivered continuously to the Berlin system up to 2023. The vehicles will be manufactured and assembled at the Berlin plant operated by Stadler Pankow GmbH.
Shifting freight transport to rail has its limitations. Therefore, a share of this transport will need to be carried out by trucks that combine reliable service with minimum environmental impact. The eHighway system is twice as efficient as conventional internal combustion engines. This Siemens Mobility innovation supplies trucks with power from an overhead contact line. This reduces local air pollution and contributes significantly to the decarbonization of the transport sector.