- New IP routers and IP interfaces ensure secure data and access-proof KNX communication over IP
- KNX IP Secure devices meet the highest security requirements in smart buildings
- More flexibility in power supply minimizes KNX bus current consumption
Siemens Smart Infrastructure expands the proven Gamma instabus building system with new IP routers and IP interfaces that support the latest KNX IP Secure standard. This extension of the KNXnet/IP protocol enables fully encrypted transmission of data telegrams, thus ensuring secure data- and access-proof communication between KNX IP routers within a single network.
- Spectrum Power ADMS to provide reliable energy supply for 1.5 million people
- One multi-site system to handle all voltage levels
Hafslund Nett, Norway's largest grid company has contracted Siemens to supply a new Advanced Distribution Management System (ADMS) for the operation of the regional power grid in Akershus, Oslo and Østfold. The fully integrated grid operating center will enable monitoring and control of the complete power grid covering all (high-, medium-, low-) voltage levels. At the same time, it will allow easy integration of third-party IT/OT systems, such as customer information systems, workforce management or geographical information systems. The project is expected to be operational at the beginning of 2022.
- New rail-mounted devices added to Gamma instabus product line
- New switch actuators with load current detection, new switching/dimming actuators and new sun protection actuators
- Powerful and universal applications across all devices, short installation times, low maintenance costs
Siemens Smart Infrastructure is expanding its Gamma instabus KNX-based product line with new switch actuators with load current detection, new switching/dimming actuators and new sun protection actuators. The new actuators are designed for residential and commercial buildings and provide reliable switching and monitoring of loads, switching and dimming of fluorescent lamps via 1 to 10 Volt control outputs, and control of alternating current motors for sunshades and ventilation valves.
- Safer and more efficient: Catania Airport is updated with integrated building automation by Siemens
- More reliable and accurate fire detection using Sinteso connected to the Desigo CC building management software
- Cloud-based Navigator software to optimize energy consumption
With almost ten million passengers in 2018, Catania Airport is continuing to grow, solidifying its number one position in southern Italy. This makes the hub an increasingly important strategic part of the Mediterranean aviation network. As a result, however, it faces greater security and energy efficiency challenges. This is the context in which the Sicilian airport made the decision to entrust Siemens with its integrated building automation project, intended to increase security levels and monitor overall energy consumption at the hub.
- Stimulating two senses through acoustic (EN 54-3) and optical (EN 54-23) alarm devices
- Voice messages can be emitted in two languages for faster evacuation
- High alarming reliability thanks to daily disturbance-free tests
Siemens Smart Infrastructure has launched new ceiling- and wall-mounted alarm devices. The expanded portfolio includes both acoustic and optical alarm devices in accordance with European Standards EN 54-3 / EN 54-23 and EN 54-17. One highlight of the expanded portfolio are the voice sounders with built-in voice messages because they improve the reaction time to alarms.
On the first day of the Hannover Messe, April 1, Klaus Helmrich welcomed you to the annual Siemens Press Conference. As member of the Managing Board of Siemens AG, Klaus Helmrich is responsible for the Digital Industries Operating Company. The Press Conference took place at 6:30 PM in the Trade Fair's Convention Center, Room 1 A/B.
Mr. Helmrich talked about the latest developments of digitalization and the next step towards the digital transformation in the manufacturing and process industries under the theme "Digital Enterprise – Thinking industry further!".
At ISH, the leading international trade show for building, energy and air conditioning technology and renewable energy sources that took place in March 2019 in Frankfurt, Germany, Siemens did exhibit its current portfolio of products, systems and solutions for energy-efficient rooms and buildings as well as heating, ventilation and air conditioning (HVAC) technology.
With the Junelight Smart Battery, Siemens is offering its first battery storage specially geared to the requirements in private homes for the storage and use of self-generated energy. The lithium-ion storage combines functions for intelligent and safe energy management and a modern design. Homeowners can use it to maximize the share of their self-generated energy, e.g. from photovoltaic systems, for their own consumption, to minimize their energy procurement costs and to make a long-term contribution towards the reduction of CO2 emissions. The Junelight Smart Battery coordinates the predictive charging and discharging procedures depending on the weather-related yield forecast of the photovoltaic system and the individual consumption profile of the household. Using the mobile Junelight Smart App, all energy flows – from production, through storage, right down to consumption and grid in-feed – can always be monitored in real time. The storage capacity can be flexibly adapted to individual needs at any time, encompassing up to 19.8 kilowatt hours (kWh). The Junelight Smart Battery is now available in Germany and will be launched in Austria in April 2019.
The Siemens Zug campus features a new office building with 1,000 work spaces and a newly constructed production building. The Siemens Zug campus is one of the first new projects to use Building Information Modeling (BIM) for design and construction. The campus complex is equipped with building automation, security and fire safety technology from Siemens BT and particular emphasis was placed on sustainability and energy efficiency of the buildings.
The need for electromobility is growing, as is the need for an efficient charging infrastructure. As a pioneer in electromobility, Siemens has global experience, maintains a strong portfolio along the entire value chain, and plays an active role in advancing the development and standardization of charging solutions worldwide.Siemens is part of the "FastCharge" research project together with BMW Group as consortium leader, Allego GmbH, Phoenix Contact E-Mobility GmbH as well as Dr. Ing. h.c. F. Porsche AG. This project is investigating the technological requirements that vehicles and infrastructure must meet in order to be able to use extremely high charging capacities. The industrial companies involved in the research project presented the latest advancements in the field of fast and convenient energy supply for electrically powered vehicles on December 12, 2018. The prototype of a charging station with a capacity of up to 450 kW was inaugurated in Jettingen-Scheppach, Bavaria. At this ultra-fast charging station, electrically powered research vehicles created as part of the project are able to demonstrate charging times of less than three minutes for the first 100 kilometres of range or 15 minutes for a full charge (10-80 % State of Charge (SOC)).The energy supply system of Siemens used in the project contains both high-power electronics for the charging connections as well as the communication interface to the electric vehicles. For the connection to the public power grid, a charging container was implemented with two charging connections for CCS-compatible vehicles. One connection has an unprecedented charging capacity of max. 450 kW while the second can deliver up to 175 kW.