[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
New actuators for lighting and sun protection from Siemens
New rail-mounted devices added to Gamma instabus product line
New switch actuators with load current detection, new switching/dimming actuators and new sun protection actuators
Powerful and universal applications across all devices, short installation times, low maintenance costs
Siemens Smart Infrastructure is expanding its Gamma instabus KNX-based product line with new switch actuators with load current detection, new switching/dimming actuators and new sun protection actuators. The new actuators are designed for residential and commercial buildings and provide reliable switching and monitoring of loads, switching and dimming of fluorescent lamps via 1 to 10 Volt control outputs, and control of alternating current motors for sunshades and ventilation valves.
New rail-mounted devices added to Gamma instabus product line
New switch actuators with load current detection, new switching/dimming actuators and new sun protection actuators
Powerful and universal applications across all devices, short installation times, low maintenance costs
Siemens Smart Infrastructure is expanding its Gamma instabus KNX-based product line with new switch actuators with load current detection, new switching/dimming actuators and new sun protection actuators. The new actuators are designed for residential and commercial buildings and provide reliable switching and monitoring of loads, switching and dimming of fluorescent lamps via 1 to 10 Volt control outputs, and control of alternating current motors for sunshades and ventilation valves.
The new switch actuators are suitable for high, capacitative, inductive and ohmic loads, especially those with high inrush peaks. The additional load current monitoring can identify changes in load behavior, thus improving building energy efficiency and room comfort.
The switching/dimming actuators are used for intelligent lighting control and ensure very comfortable lighting. They support low-energy switching and dimming of LEDs and fluorescent lamps via 1 to 10 Volt control outputs or LED drivers.
The new sun protection actuators keep workspaces glare-free during the day and prevent rooms from heating up. The automatic travel time determination ensures easy and fast commissioning. Flexible override blocks protect the shades from wind, rain and frost. When used in combination with a weather station, the actuators can meet complex requirements of a state-of-the-art sun protection control solution.
Reduced installation time and simplified commissioning All actuators can be commissioned quickly using the new, vendor-neutral ETS5 KNX configuration software. Maintenance-free clamping screws considerably shorten the installation time for the new switch actuators. For efficient commissioning, the front of the devices features a status display with sliding switches or a membrane keypad for direct operation.
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 71,000 employees worldwide.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.