- Siemens forms strategic cooperation in digitalization with Swire Coca-Cola, to jointly build 18 digital plants in future
- In 2020 Siemens established a global strategic partnership with the Coca-Cola Cross Enterprise Procurement Group (CEPG)
- The Manufacturing Information System (MIS) customized for Swire Coca-Cola successfully launched in Hangzhou and to extended to about 100 production lines in the next two years
- To support Swire Coca-Cola build a group level data collection, analysis and presentation platform with software and hardware products and solutions covering big data, AI and MindSphere
- MIS to become the benchmark and standard for the manufacturing information systems of Swire Coca-Cola worldwide
Siemens and Swire Coca-Cola China Co., Ltd today formed a strategic partnership on digitalization. The two sides will carry out in-depth cooperation in fields such as digital plant construction, supply chain intelligent management and training for digital talents, and to jointly build digital plant benchmarks in the beverage industry, aiming to promote digital transformation of Swire Coca-Cola in China and around the world. In addition, the Manufacturing Information System (MIS) customized by Siemens for Swire Coca-Cola has been successfully applied to its digital production line in Hangzhou, Zhejiang province. Upon the implementation of the project, Swire Coca-Cola will unlock an annual production capacity of 550 million cans of Coca-Cola.
- Simotics S-1FS2 in stainless steel housing with specific features for use in the pharmaceutical and F&B industries
- Servo planetary gearmotors Simotics S-1FK2 for optimum adjustment of speed, torque and mass inertia
- Simotics S-1FT2 in protection class IP67 with 26 bit encoder, higher rated speed and other selectable features
Siemens is adding new servo motors to its proven Sinamics S210 single-cable servo drive system, thereby expanding its range of applications. Specifically, for use in the pharmaceutical and food industries, the company is launching the Simotics S-1FS2, a motor version with a stainless-steel housing, the highest degree of protection IP67/IP69, and high-resolution 22-bit absolute multiturn encoders. The servo motor thus meets all hygienic conditions and can be used for mixing and stirring, air conditioning and ventilating, dosing and filling, as well as conveying, packaging and storing a wide variety of end products in the food and beverage sector and in the pharmaceutical industry.
- Access Points and the first industrial Wi-Fi 6 Client Module available on the market
- Reliable and high-performance wireless connectivity with maximum data transmission rates
- Devices available with high protection class and industry-specific approvals
With a view to the increasing demands posed by digitalization, Siemens is expanding its offerings for network components for industrial WLAN solutions: The new Scalance WUM766-1 Client Module is the first industrial client module on the market that satisfies the latest Wireless LAN Standard IEEE 802.11ax (“Wi-Fi 6”), enabling reliable and high-performance wireless connectivity. By combining the Client Module with the new Scalance WAM766-1 Access Points, users can now implement demanding Industry 4.0 applications such as augmented reality or remote-controlled cranes. At gross data transmission rates of 1201 Mbit/s, the Access Points can link a large number of mobile devices in confined spaces, for example shuttle systems in intra-logistics.
- New Sinamics DriveSim Basic software solution for fast and easy simulation of drive constellations
- Seamless integration of models into commercially available simulation programs
- Validated function units accelerate development phase
With Sinamics DriveSim Basic, Siemens presents a new software solution with which for the first-time drive constellations and their behavior in machines and plants can be simulated, adapted, and optimized. With the new solution, Siemens offers a quick and easy entry into the simulation of drive technology and enables machine and plant manufacturers to accelerate their own development phase.
- Simotics SD motor series from Siemens is now consistently available in efficiency class Super Premium Efficiency (IE4)
- Exceeds increasingly stringent requirements of ErP Directive 2019/1781, which takes effect in two steps in July 2021 and July 2023
- Users can meet long-term efficiency standards, save energy, lower operating costs, and reduce CO2 emissions
Siemens is presenting the Simotics SD motor series as part of the Digital Enterprise Virtual Experience at the Hannover Messe 2021. The standard version of Simotics SD is offered in the efficiency class Super Premium Efficiency (IE4) across the entire power spectrum from 2.2 to 1,000 kW and for the number of poles 2, 4, as well as from 75 kW for 6 poles and from 55 kW for 8 poles. Simotics SD in IE4 thus exceeds the so-called ErP Directive 2019/1781 (energy-related products) – both the first stage, which will be valid by July 2021, as well as the next, which will apply from July 2023. The directive defines the eco-design requirements for electric motors and speed control systems.
- Mercedes-Benz and Siemens to expand the digitalization of sustainable production methods, expanding a long-standing successful cooperation in the field of engineering and production
- Partnership to develop innovative solutions for the qualification of employees, digitalization and for increasing energy efficiency in production
Mercedes-Benz and Siemens plan to cooperate on advancing digitalization and automation in the automotive industry, supported by the State of Berlin. Mercedes-Benz AG aims to digitize its production processes. Siemens, a leading supplier in the field of automation, industrial software and smart infrastructure, will bring its expertise and technologies to the partnership to develop highly flexible, efficient and sustainable automotive production together with Mercedes-Benz.
- New Offering Seamlessly Combines Next-Generation Virtual Platform, Hardware Emulation, and FPGA Prototyping Technologies to Help Accelerate Verification Cycles
- Expansion of the Customer-Proven Veloce Family Sets New Standard in Hardware-assisted Verification
Siemens Digital Industries Software today unveiled its next-generation Veloce™ hardware-assisted verification system for the rapid verification of highly sophisticated, next-generation Integrated Circuit (IC) designs. This is the first complete, integrated offering that combines best-in-class virtual platform, hardware emulation, and Field Programmable Gate Array (FPGA) prototyping technologies, and paves the way to leverage the latest powerful hardware-assisted verification methodologies.
This year, the 1.4 million square meter Deutsche Messe exhibition site in Hanover, Germany will become 5G-ready. Deutsche Messe, which organizes international capital goods trade shows, has obtained a frequency allocation in the 3.7-3.8 GHz range from the Bundesnetzagentur (Federal Network Agency) and will set up one of the largest 5G zones in Europe, spanning 30 halls and buildings as well as the entire open-air ground. Siemens is playing a very specific role in this achievement. As one of the key exhibitors at the HANNOVER MESSE, Siemens is setting up a private 5G campus network with a focus on industrial use in one of the exhibition halls in Hanover. The network can be used by exhibitors during trade shows and, outside of trade show times, can be used by companies for tests and field trials.
- Siemens expands long-standing relationship supporting U.S. Air Force with proven digital capabilities to innovate in the defense industry
Siemens today announced the U.S. Air Force has selected
Teamcenter® software as the foundational system of record to support its digital acquisition and sustainment strategy for critical systems and technologies across the service. The selection of Teamcenter as the Air Force enterprise standard follows a 2019 indefinite-delivery / indefinite-quantity contract for $24.6 million to Siemens for licensing, maintenance and support.
- FIA and Siemens extend partnership to provide the ‘FIA Mobility Advocate’— a unique software and hardware toolkit — for FIA Mobility Member Clubs to strengthen advocacy of future transport solutions
As an
“Official Supplier of Urban Mobility Advocacy Solutions” for the Fédération Internationale de l’Automobile (FIA), the governing body of world motor sport and
the federation of the world's leading motoring organisations, Siemens plans to
develop a toolkit of software solutions for FIA Member Clubs to help them
provide an evidence-based approach to advocate for the implementation of mobility
policies and strategies. The ‘FIA Mobility Advocate’ combines modeling for
mobility, autonomous vehicles, and the environment, with enhanced analysis
outputs to help meet current future mobility goals.