[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release08 April 2021Digital IndustriesNuremberg
Quick and easy simulation of drives with Sinamics DriveSim Basic
New Sinamics DriveSim Basic software solution for fast and easy simulation of drive constellations
Seamless integration of models into commercially available simulation programs
Validated function units accelerate development phase
With Sinamics DriveSim Basic, Siemens presents a new software solution with which for the first-time drive constellations and their behavior in machines and plants can be simulated, adapted, and optimized. With the new solution, Siemens offers a quick and easy entry into the simulation of drive technology and enables machine and plant manufacturers to accelerate their own development phase.
New Sinamics DriveSim Basic software solution for fast and easy simulation of drive constellations
Seamless integration of models into commercially available simulation programs
Validated function units accelerate development phase
With Sinamics DriveSim Basic, Siemens presents a new software solution with which for the first-time drive constellations and their behavior in machines and plants can be simulated, adapted, and optimized. With the new solution, Siemens offers a quick and easy entry into the simulation of drive technology and enables machine and plant manufacturers to accelerate their own development phase.
With Sinamics DriveSim Basic, Siemens presents a new software solution with which for the first-time drive constellations and their behavior in machines and plants can be simulated, adapted, and optimized.
Sinamics DriveSim Basic bridges the gap between the logical and mechanical simulation worlds. The application focus is on simulation support of the customer application, i.e. the components that interact with the drive. The simulation provides answers to drive questions even before a concrete product selection has been made. For the virtual commissioning of the PLC control with known Profidrive telegrams or complex mechanics on the virtual drive shaft, the model provides a reliable representation of the drive system in the required level of detail.
One possible application scenario is the coupling of PLC and mechanical model via Sinamics DriveSim Basic. The calculated load profiles can then be loaded into the TIA Selection Tool or the Sizer and a drive selection can be made.The necessary drive parameters and the interfaces known from reality are available for the simulation. The user configures only the part of the drive that he needs for his simulation purpose. A time-consuming complete virtual commissioning of the drive is not required, which saves time and costs. The models in Sinamics DriveSim Basic link seamlessly to the existing drive documentation and have been validated against the real Sinamics drives using the same test vectors.
For easy handling, Sinamics DriveSim Basic is available as a standardized FMU (Functional Mockup Unit) model. The software offers the same FMU file for every Sinamics drive. The Sinamics S120 and G120 drives including the motor can already be represented. Further drives will follow. This FMU can be imported directly into the simulation program used. Sinamics DriveSim Basic is compatible with many commercially available simulation programs, such as Simit, Simcenter Amesim, NX Motion or Matlab Simulink. Together with other virtual Siemens solutions such as Simatic S7 PLCSIM Advanced or NX Mechatronics Concept Designer, a consistent model-based development process can be implemented.
For further information regarding the Siemens Digital Enterprise Virtual Experience at Hannover Messe 2021 please see
www.siemens.com/press/hm21
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020. In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of €57.1 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.