- New cooling concept combines cooling fins and tubes
- Greater power density, longevity and reliability due to improved temperature distribution and vibration-optimized, robust housing
- Outstanding flexibility for customer interfaces
- Connection to the Sidrive IQ digital platform with Simotics Connect 600
The Simotics HV C air-cooled range from Siemens completes the Simotics HV C platform for compact high-voltage motors up to 3.2 megawatts (MW). The innovative cooling concept, involving a clever combination of fin and tube cooling, delivers improved temperature distribution in the motor, thus increasing the power density significantly. With their vibration-optimized, robust housing design, the Simotics HV C air-cooled motors score highly in terms of increased reliability. The new high-voltage motors feature an enclosed internal circulation (IC 411) and are equally suitable for use in areas where there is no danger of explosions (safe areas) and areas where explosions are not likely to occur (explosion protection zone 2) as well as being available in ignition-proof types Ex ec and Ex tc. The motors can be connected to the Sidrive IQ digital platform using the Simotics Connect 600 connector box: This provides access to cloud-based analysis of the condition data which allows the drive system to be optimized. The compact motors are used in pumps, fans, compressors, extruders, grinders, stirrers, mixers, conveyors and rollers in industries as diverse as energy, chemical, cement, paper and pulp, and mining.
- Siemens makes strong commitment for shaping the future of Germany as a location for industry
- Investment in the future of work in connection with manufacturing, researching, learning, and residential living in the new "Siemensstadt 2.0"
- Biggest single investment in the history of Siemens in Berlin
A commitment to Berlin and Germany: at the time-honored Siemens industrial estate in Berlin's Spandau district, Siemens AG plans to make its biggest single investment ever in the company's history in Berlin. In the coming years, up to €600 million are to be invested in a new world of working and living: Siemensstadt ("Siemens City") 2.0. This project, which covers an area of 70 hectares, aims to transform this large industrial area into a modern, urban district of the future for a diverse range of purposes. A further goal is to strengthen selected key technologies and innovation fields in collaboration with the scientific and business communities. To make this possible, this section of Berlin is to become home to centers of research and expertise, to start-up incubators and to research and scientific institutes as well as their partner companies.
- Sidrive IQ improves drive systems along the entire life cycle up to the megawatt range
- Cloud-based application based on networked drive systems from Siemens
- Increased productivity, reliability and ease of maintenance
- Standardized link enabled by Sinamics Connect 500 and Simotics Connect 600 connectivity modules
Sidrive IQ from Siemens provides a digital platform enabling the evaluation and utilization of data gathered from drive systems. On the basis of networked drive systems from Siemens, this cloud-based application is now also available for motors and converters in the medium and high-voltage range. This opens up an array of benefits for plant and machine operators, from optimized maintenance activity and maximum availability to increased productivity, from low outputs through to the megawatt range across the entire life cycle. Connectivity modules such as Simotics Connect 600 and Sinamics Connect 500 enable high-voltage motors and medium-voltage converters to be simply linked up to Sidrive IQ. With the latest generation of its Remote Services and Condition Monitoring Services offered as part of the Sidrive IQ Services portfolio, Siemens is making available corrective measures for fixing faults, preventive maintenance offers and proactive services for optimized performance. The optimized drive systems are used in pumps, fans and compressors across different sectors of industry such as oil and gas, mining, food and beverage, water and wastewater, metals and cement.
- Highly efficient gas-fired combined cycle plant project in Lomé, Togo
- Siemens collaborates with the Government of the Arab Republic of Egypt on industrialization, education and training
- Siemens, Volkswagen (VW) and the German Development Agency for International Cooperation (GIZ) collaborating on e-mobility in Rwanda
Siemens will partner even more closely with the African countries Togo, Egypt and Rwanda in the areas of power supply, industry, transport and vocational training. Egypt and Togo have signed the corresponding Memoranda of Understanding (MoUs) on the sidelines of the G20 Compact with Africa Investment Summit in Berlin in the presence of Joe Kaeser, President and Chief Executive Officer of Siemens AG, the Presidents of Egypt and Togo and further high-ranking personalities from these partner countries.
- Motor management system with new Simocode pro V PN GP basic unit, operator control block, and current measuring and multifunction module
- Simple integration of motor management solutions in Profinet networks
- Suitable for direct-on-line, reversing, and star-delta (wye-delta) starters and for controlling soft starters
- Monitors, protects and controls constant-speed motors with predictive maintenance functions.
Siemens has extended the Simocode pro motor management system to include a new basic unit for standard motor applications. Simocode pro V PN GP has a Profinet connection, which facilitates easy entry into Profinet communication. The basic unit is supplemented by a current measuring module. It can be optionally extended by an operator control block and a multifunction module – with additional inputs/outputs, and temperature and ground fault detection. The new compact system for easy, economical motor management is suitable for direct-on-line, reversing, and star-delta (wye-delta) starters as well as for controlling a soft starter.
- Research project for an optimized transport system (OTS)
- Mobility offering for the first and last mile
- Testing the interplay of intelligent infrastructure, cloud-based software services and autonomous electric vehicles
Siemens Mobility is launching a field test for autonomous driving at the Siemens campus in Munich-Perlach, Germany. Working with partners IAV GmbH, Institute for Climate Protection, Energy and Mobility (IKEM) e.V., emm Solutions GmbH, UTB Projektmanagement GmbH and the Technical University of Munich (TUM), Siemens Mobility is initiating a research project and field test. The test route runs through the campus and enables traffic simulation in a variety of real-life situations.
- Detailed digitalization roadmap including schedule, technology recommendations and return-on-investment data
- By implementing the roadmap, Steklarna Hrastnik aims to improve its productivity, quality and efficiency
The digital transformation in the glass industry is in full swing. The Digital Enterprise portfolio from Siemens encompasses integrated hardware, software and services for enterprises of all sizes, and allows companies across the glass industry to leverage the benefits of Industrie 4.0 already today. As part of a joint digitalization consulting project, Siemens and Steklarna Hrastnik collaborated to create a detailed strategy for the glass manufacturer’s digital transformation over the next five years.
- Fulcrum's municipal solid waste-to-fuels plant will contribute to a sustainable future
Abengoa, a Spanish engineering, procurement and construction (EPC) contractor, recently selected Siemens to supply a compressor train for Fulcrum BioEnergy's Sierra BioFuels Plant that will use gasification technology to produce low-carbon fuels from municipal solid waste. The plant will be located in Storey County outside of Reno Nevada and is expected to produce approximately 11 million gallons of biofuel per year that will be used by the aviation industry.
- Agreement to cooperate with Ministry of Electricity of Iraq to add 11 gigawatts of power generation capacity in four years
- Roadmap proposes cost savings in billions of USD and generating additional electricity 24/7 for 23 million people
- Plan envisions creating tens of thousands of jobs
- Focuses on energy infrastructure, education, anti-corruption and financing
Siemens and the Ministry of Electricity of the Republic of Iraq have entered a milestone agreement to seek the implementation of the company's roadmap for repowering Iraq. Signed by Qasim Al-Fahdawi, Minister of Electricity, and Joe Kaeser, President and CEO of Siemens AG, the Memorandum of Understanding (MoU) will examine a series of short, medium and long-term plans to meet the reconstruction goals of Iraq and support the country's economic development.
- Padam is a fast-growing Software as a Service (SaaS) provider for on-demand transport
- Padam closes an investment round with strategic investment of Siemens Mobility
- Enhances Siemens Mobility's intelligent infrastructure portfolio for intermodal mobility
- The transaction was executed in October 2018
- Padam remains a standalone, founder-led company
Siemens Mobility and Padam, headquartered in Paris, France and a fast-growing turnkey AI-powered technology provider that operates on-demand transport (microtransit) services, are launching a partnership to enhance demand responsive transportation options and improve passenger experience. The investment will enhance Siemens Mobility's intelligent infrastructure portfolio that is focused on intermodal transportation, offering public transportation operators a first/last mile transportation solution that optimizes vehicle utilization at lower costs. Siemens has made a significant investment in Padam. Both companies have agreed to maintain confidentiality regarding financial details of the deal. Padam's white-label platform, Padam Live, is a software platform that is rebranded by public transportation operators to integrate microtransit services. It offers cities worldwide an advanced management system.