Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release02 November 2018Process Industries and DrivesNuremberg
Simotics HV C air-cooled: Innovative cooling concept for greater power density

The picture shows the Simotics HV C air-cooled high-voltage motor.
The increased performance density is based on the new cooling concept: Tube cooling elements, which have proven themselves over decades in the most demanding conditions, have been integrated by Siemens into the high-voltage
motor's rib-cooled housing. The motor cooling is improved by the addition of a modern fan design – unlike conventional methods, this reduces the internal temperature of the motor considerably. This provides a compact and light-weight motor design which increases performance by up to 15 percent and extends the operating life of components without changing the overall size. The highly flexible motor design allows it to be matched to customer interfaces on a project-by-project basis, for example, the connection leads can be located in many different positions. Due to a standardized design and management principle for compact, air-cooled motors with or without explosion protection, the cost is reduced across the whole lifecycle – from planning and procurement, through engineering and plant integration, to service, warehousing and spare parts management. Extended maintenance intervals and service times increase the availability of the drive system and thus the whole plant. Simotics HV C air-cooled motors from Siemens extend the range beyond the existing flameproof and water-jacket-cooled designs.
Simotics Connect 600: The interface to the digital world
Simotics HV C motors are an integral component of Sidrive IQ, the digital platform for optimizing drive systems. The Simotics HV C motors have an optional connectivity module for integration into the digital, cloud-based solution. This uses temperature and vibration sensors to capture and process data such as bearing temperatures, winding temperatures, and housing vibrations and transmits this information for analysis in the cloud. The connectivity module Simotics Connect 600 used on the Simotics HV C is specifically adapted to the requirements of Sidrive IQ. Sidrive IQ uses the data received to monitor, analyze and optimize the Simotics HV C motor drive: This increases the availability, efficiency and performance of the motors and improves service efficiency. As Simotics HV C motors are frequently used as part of the core process of a plant or system, connecting to Sidrive IQ increases the transparency of the drive system significantly, thus providing productivity gains for the whole system.
For further information on Simotics HV C, please see www.siemens.com/simotics-hv-c
For this press release

Event: Siemens at the SPS IPC Drives 2018
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Stefan Rauscher
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7952