- Companies will jointly offer a technology portfolio for buildings, including everything from energy efficiency and user experience to connectivity, security and data analysis
Siemens Smart Infrastructure in Spain, a market leader in innovation and technology for smart buildings, and Telefónica Tech, Telefónica’s holding company for digital businesses with high growth potential in IoT, Big Data, Blockchain, Cybersecurity and Cloud, will be offering the Spanish market their services and solutions for smart buildings in one package.
- Certification up to SIL 3 / PL e for high personal and system safety
- Force-guided operation allows for use in railroad, signaling and elevator applications
- Simple assembly reduces time required for building control panels
The Sirius 3RQ1 series completes Siemens Smart Infrastructure’s portfolio of coupling relays for electrical systems in industry and infrastructure. With wide-range supply voltage from 24 to 240V AC/DC, the new force-guided devices are designed for universal use. They are certified up to Safety Integrity Level (SIL) 3 and Performance Level (PL) e and approved for very high safety requirements. Among other things, coupling relays are used to amplify or multiply signals to and from controllers. The Sirius 3RQ1 coupling relays can also switch electrical loads directly. Thanks to their force-guided operation in accordance with IEC 60947-5-1 (IEC 61810-3), the devices offer maximum safety for people and systems. They are particularly well suited for use in railroad and signaling applications as well as in elevators and industrial production facilities, making it possible to safely control brakes and doors, for example, and to switch traffic lights, conveyor belts or packaging machines.
- Client PBW is in charge of public parking for universities and government offices
- Initially, about 200 of a total of 500 charging stations from different providers will be connected to the software, with more to follow quickly
- E-Car OC backend solution enables easy access to the charging infrastructure through different billing and payment systems
The chargers of Parkraumgesellschaft Baden-Württemberg mbH (PBW) will soon be managed using the E-Car Operation Center (E-Car OC) software from Siemens Smart Infrastructure. The goal is to manage the charging infrastructure in public parking garages and parking lots in a flexible and future-proof manner. The software also allows the administration of power and billing data from charging stations of different manufacturers. This will make it possible to charge electric cars conveniently and flexibly in PBW parking lots – for example, at hospitals or universities – and to pay with a variety of payment systems via Giro-e, using an EC card. Initially, the software will manage about 200 charging stations, with more to follow in the near future.
- 2-loop fire control panel connects up to 252 devices
- EN 54-23 compliant alarm devices and dedicated peripherals
- Time-saving tools such as auto configuration and on-board web server
- License free programming
With the launch of the new version of the fire protection system, Cerberus FIT, Siemens Smart Infrastructure expands its offering for the small to medium-sized buildings market. Various small to medium-sized buildings can now be covered with a simple and cost-efficient solution. Cerberus FIT maximizes fire safety, thanks to greater functionality and enhanced productivity for those working on protecting the buildings. The intuitive interface as well as the auto configuration tool allow the technician to install, commission and maintain the system in a fast, easy and reliable way. With the delayed alarm function staff will be informed first to identify what an alarm is about in order to assess the situation. This ensures business continuity and reduces disturbances to occupants of smaller buildings such as small-to-medium sized hotels, kindergartens or nursing homes.
- Charging infrastructure to power 24 new electric buses for the Ostrava Transit Authority in Czech Republic
- Software to automatically adapt the charging processes to the bus schedules and to optimize energy consumption
- Operations are scheduled to start in mid-2022
Siemens Smart Infrastructure will provide a charging solution for Dopravní podnik Ostrava (Ostrava Transit Authority), which will expand its fleet with 24 Solaris electric buses. The largest order for electric buses in the Czech Republic to date will include four Sicharge UC charging stations from Siemens. These high-power chargers provide an effective maximum of 400 kW each. Furthermore, Siemens will deliver 28 mobile chargers, electrical infrastructure as well as energy automation software.
- Reliable protection with minimal space requirements
- For power distribution and industrial plants
Siemens Smart Infrastructure presents the new Siprotec 5 Compact device, specially designed to address the demands of industrial applications, infrastructure and distribution grids. With its compact size, large number of inputs and outputs, and universal range of functions, it can be configured to meet the specific requirements associated with protecting feeders and motors. As a space-saving universal device, it is ideally suited to help optimize investment and operating costs in power distribution.
- High transparency through integrated communication and measurement functionality
- Faster response to faults minimizes downtime
- Easy retrofitting of existing systems without additional space requirements
Siemens Smart Infrastructure has launched the new Sentron 3NA COM LV HRC fuse link with integrated communication and measurement functionality. The compact device is designed for 400 volts low-voltage grids and can be used in secondary substations and industrial plants. The LV HRC fuse link protects grids and plants against short circuits and overloads and is capable of measuring current. The collected data is sent wirelessly to the new 7KN Powercenter 1000 data transceiver where it can be retrieved. In addition, it can be transferred to local or cloud-based grid and energy management systems. Among other things, the data provides insight about the current network load, phase symmetry and any irregularities. This makes it possible to increase the supply security and optimize maintenance and service. Thanks to faster fault detection and location, the duration of power outages can be significantly reduced.
- Climate-neutral insulating medium “Clean Air” consists exclusively of components of ambient air
- Innovative load-break switch enables F-gas-free power distribution on the secondary distribution level, up to 24 kilovolts
- Same compact dimensions, consistent handling enable simple, future-proof transition to sustainable power distribution
Siemens Smart Infrastructure has introduced the 8DJH 24 switchgear, a ring main unit (RMU) for line voltages up to 24 kilovolts (kV), completely free of fluorinated gases. This medium-voltage switchgear for secondary electrical distribution has the same compact dimensions as the variant with sulfur hexafluoride (SF6) but uses the climate-neutral insulation medium “Clean Air”, which consists exclusively of natural components from ambient air. The core of the unit is a three-position load-break switch with vacuum interrupter in the auxiliary path (blue switch). This new technological development from Siemens eliminates SF6 as an insulating medium, as well as any gas mixture based on fluorine (F-gases). As a result, the new switchgear also reduces the CO2 footprint of grid operators. Other benefits include easy and safe handling of the switchgear and effortless recycling at the end of its service life. In addition to the high level of environmental compatibility, digital applications make the new switchgear future-proof and cost-efficient for the grid of tomorrow. The new unit has been in use since fall 2020 in a local substation in the Oberallgäu region of Germany as part of a development cooperation with German distribution grid operator Netze BW.
- Italian start-up On launches new integrated e-mobility service
- 120 Sicharge AC22 charging stations to be installed to charge various e-vehicles in the city
- Siemens provides cloud-based platform for charging infrastructure management
Siemens Smart Infrastructure is delivering charging stations as well as a cloud-based software for charging infrastructure management to On in Italy. The solutions provide the basis for a new electric vehicle sharing service in the city of Rome developed by the Italian start-up. The first 23 charging stations have already been installed in the center of Rome; the rest will follow during the year.
- Integration of more devices for advanced building management
- Better user experience with improved Flex Client
- Enhanced cybersecurity with IEC62443-3-3 SL2 compliance
Siemens Smart Infrastructure has updated its Desigo CC smart building management platform to version V5.0, which marks the software’s opening for more systems and devices. The platform now offers improved connectivity and support for more integrations, such as EV charging stations. In addition, it provides new functions for easier and more flexible usability. Desigo CC V5.0 further strengthens the level of cybersecurity protection and enables a wide variety of buildings to become future-proof and easy to manage.