Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release19 April 2021Smart InfrastructureZug
Siemens’ fire protection system effortlessly protects small to medium-sized buildings
Cerberus FIT
Safety and business continuity in every situation
The Cerberus line offers a broad portfolio of detection and alarming devices including pre-configured Cerberus FIT device to choose from: from fast and reliable fire detectors to configurable alarming devices (including EN 54 compliant sounder and voice sounder beacons) which enables smart evacuation. The newest portfolio member, the updated Cerberus FIT fire protection system now allows for second loop, supporting a maximum number of 252 addressable peripherals and devices, such as detectors as well as alarm devices. All detectors and peripheral devices have an integrated line separator. In case of an interruption, the loop turns into two stub lines while making sure the system is running. This significantly increases the safety of building occupants and ensures business continuity. Because every device is also powered by the loop, less wiring is needed, enabling the customer to achieve cost-efficiency.
Intuitive and easy operation
The new version of the Cerberus FIT control panel comes with an intuitive interface, including LED indicators with self-explanatory icons and an easy-to-read display. This avoids extensive training and allows facility staff to perform simple operational tasks on their own, without the help of experts. Thanks to its auto configuration feature, the Cerberus FIT control panel detects and automatically reads-in all connected devices, providing immediate and simple operation. The integrated 'Panel Configurator' enables the configuration to be changed quickly and easily on a PC or laptop, without additional software.
Cerberus FIT is an EN-compliant fire protection system. It is approved and certified by the independent certification body LPCB and can be used in accordance with the application standard DIN VDE V 0826-2. The new Cerberus FIT version will be available globally, maximizing the fire safety of smaller buildings as well as enhancing the productivity of everyone involved in their protection.
For more information on Siemens Smart Infrastructure, see
www.siemens.com/smart-infrastructure
www.siemens.com/smart-infrastructure
For this press release
Follow us on Twitter
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the
future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems,
buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source –
with products, systems, solutions and services from the point of power generation all the way to consumption. With
an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward
protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters
in Zug, Switzerland. As of September 30, 2020, the business had around 69,600 employees worldwide.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence,
innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company
focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and
digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to
benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road
transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in
the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology
and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the
transmission and generation of electrical power that has been listed on the stock exchange since
September 28, 2020. In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of
€57.1 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000
employees worldwide. Further information is available on the Internet at
www.siemens.com.