[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release13 April 2021Digital IndustriesZug (Switzerland)
New LV HRC fuse link from Siemens increases supply security in power grids
High transparency through integrated communication and measurement functionality
Faster response to faults minimizes downtime
Easy retrofitting of existing systems without additional space requirements
Siemens Smart Infrastructure has launched the new Sentron 3NA COM LV HRC fuse link with integrated communication and measurement functionality. The compact device is designed for 400 volts low-voltage grids and can be used in secondary substations and industrial plants. The LV HRC fuse link protects grids and plants against short circuits and overloads and is capable of measuring current. The collected data is sent wirelessly to the new 7KN Powercenter 1000 data transceiver where it can be retrieved. In addition, it can be transferred to local or cloud-based grid and energy management systems. Among other things, the data provides insight about the current network load, phase symmetry and any irregularities. This makes it possible to increase the supply security and optimize maintenance and service. Thanks to faster fault detection and location, the duration of power outages can be significantly reduced.
High transparency through integrated communication and measurement functionality
Faster response to faults minimizes downtime
Easy retrofitting of existing systems without additional space requirements
Siemens Smart Infrastructure has launched the new Sentron 3NA COM LV HRC fuse link with integrated communication and measurement functionality. The compact device is designed for 400 volts low-voltage grids and can be used in secondary substations and industrial plants. The LV HRC fuse link protects grids and plants against short circuits and overloads and is capable of measuring current. The collected data is sent wirelessly to the new 7KN Powercenter 1000 data transceiver where it can be retrieved. In addition, it can be transferred to local or cloud-based grid and energy management systems. Among other things, the data provides insight about the current network load, phase symmetry and any irregularities. This makes it possible to increase the supply security and optimize maintenance and service. Thanks to faster fault detection and location, the duration of power outages can be significantly reduced.
The new Sentron 3NA COM LV HRC fuse link protects grids and plants against short circuits and overloads and is capable of measuring current.
“Increasingly distributed energy systems pose new challenges for distribution networks,” said Martin Moosburger, Vice President of Product Management, Electrical Products Business Unit, at Siemens Smart Infrastructure. “Among other things, smart grids must be able to balance fluctuations in energy production and demand and coordinate multidirectional power flows. This can only be done with the help of digital technology. Our new fuse is a small but very effective component in the digitalization of the energy landscape by providing valuable data for grid monitoring.”
The new 3NA COM LV HRC fuse link gives companies in the industry and infrastructure sector greater transparency over their power distribution. They can use the collected data for operational energy management and to optimize their energy efficiency as well as for service and maintenance.
Easy retrofit of existing plants
The communication-capable fuse is easy to install and retrofit without requiring additional space. It has the same dimensions as conventional LV HRC fuses, but consists of two components that can be plugged together: an LV HRC fuse link with a shortened ceramic body and a multifunctional electronic module. As is typical with LV HRC fuses, the fuse link trips in the event of a short circuit and overload. The electronic module additionally measures the current flow at selected points in the grid and provides insight into the current operating status at any time. Faults such as creeping grid or phase overload are reliably detected and can be localized quickly.
For additional processing, the measured values from up to 24
fuses are sent wirelessly to the 7KN Powercenter 1000 data transceiver. From
there, the data can be retrieved directly via Bluetooth using a mobile device
or transmitted to higher-level gateways via Modbus TCP. The 7KN Powercenter
3000 IoT data platform, for example, can be used to transfer data to
MindSphere, the cloud-based IoT operating system from Siemens. Data can be visualized
either locally, for instance using the Sentron “powerconfig” or Sentron
“powermanager” software, or in the cloud using the Sentron “powermind” app.
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2020, the business had around 69,600 employees worldwide.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020.
In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of €57.1 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.