- Valley Metro orders 14 additional light rail vehicles from Siemens Mobility
- Improved availability and enhanced passenger experience
The Valley Metro Regional Public Transportation Authority has ordered 14 S700 light rail vehicles (LRV) from Siemens Mobility. The new trains will operate in Phoenix, Arizona, in the U.S. They will be built at the Siemens Mobility facility in Sacramento, California. Valley Metro previously ordered 11 light rail trains from Siemens Mobility in 2017.
- Communications-Based Train Control (CBTC) signaling system to be installed on 24km of elevated Jurong Region Line in Singapore
- Half-height Platform Screen Doors to be installed at 24 stations throughout line
- The intelligent infrastructure will provide greater availability, enhanced operations, and will improve passenger experience
Siemens Mobility has been awarded a contract of approximately 135 million Euros by the Singapore Land Transport Authority (LTA) to install an automatic train control signaling system and half-height platform screen doors on the Jurong Region Line (JRL). Siemens Mobility will utilize its Trainguard Sirius solution and modern interlocking product Westrace to implement a Communication Based Train Control (CBTC) signaling system across the entire 24 kilometers of track. In addition, Siemens Mobility will install platform screen doors at the 24 stations being built, which will support the GoA 4 automation of the line and allow for full unattended/automatic train operation. The project has been designed by an international team of Siemens Mobility in Singapore and Spain.
- Early delivery of three locomotives to Danish State Railways DSB
- Vectron approved in 20 countries
On September 15, 2020, the AC version of the Vectron locomotive received official approval from the Danish safety authority “Trafik-, Bygge og Boligstyrelsen” for operating in Denmark. The approval marks an important milestone for the commissioning of 42 Vectron locomotives ordered by Danish State Railways (DSB) from Siemens Mobility over the last two years. The first three locomotives will be delivered in September 2020.
Less
diesel, less CO
2, even greener: DB Cargo is renewing its fleet of shunting and
mainline locomotives and is procuring new Vectron Dual Mode dual-power
locomotives from Siemens Mobility. The framework agreement comprises up to 400
vehicles and investment volume corresponds to well over one billion Euros.
The locomotives
of the type Vectron Dual Mode will be delivered with specific adaptations for
the range of applications planned by DB Cargo. The locomotives can be operated
both with diesel and electric power.
In September 2020, DB Cargo ordered 100 locomotives, followed by a second call for another 50 locomotives in January 2022.
The German operator
Bremer Straßenbahn AG (BSAG) has ordered a new tram fleet for the Free
Hanseatic City. The order is for 77 Avenio trams. The four-section trains are
to be delivered step by step for service in Bremen's tram network beginning in
the summer of 2020. On August 30, the "Nordlicht" was presented online.
- New metro line 3 in Sofia, Bulgaria, went into service today
- Modern Inspiro platform was developed with a special emphasis on sustainability, availability and noise reduction
Siemens Mobility's modern Inspiro trains and Communications Based Train Control (CBTC) Trainguard MT (TGMT) systems have gone into passenger service today on Line 3 of the Sofia Metro. The trains and systems will serve the third metro line of the Bulgarian capital, which was opened today in the presence of the Minister of Transport Rosen Zhelyazkov, the Mayor of Sofia Mrs. Yordanka Fandakova and the Executive Director of "Metropoliten" EAD Prof. Dr. Stoyan Bratoev.
- Communications-Based Train Control signaling system to be installed on 11km of ‘D’ Metro Line in Buenos Aires, Argentina
- The automated signaling system will provide greater availability, enhanced operations and passenger experience
Siemens Mobility has been awarded a contract by Subterráneos de Buenos Aires, Sociedad del Estado (SBASE) to install a Communications-Based Train Control system (CBTC) on the ‘D’ Metro Line in Buenos Aires, Argentina. The CBTC signaling system will be fully implemented across the entire 11 kilometer line that incorporates 16 stations between “Catedral”, located in the historic Plaza de Mayo, and “Congreso de Tucumán”, located in the northern part, close to the borders of the city of Buenos Aires. The system will include the installation of onboard units on 24 existing cars, as well as a radio system, electronic interlockings, and wayside equipment. All elements of the system will be coordinated by a newly established operations control center. As part of the overall SBASE project to renovate the ‘D’ Metro Line, Siemens Mobility will also provide a passenger information system.
- Co-CEO Sabrina Soussan to leave the company at her own request
- Michael Peter stands for strong expertise in digitalization and
connectivity as well as for continuity in Siemens Mobility’s top management
Michael
Peter will be Siemens Mobility’s sole CEO, effective July 10, 2020. Sabrina Soussan,
who has been his Co-CEO until now, will leave the company at her own request to
take on a new challenge outside Siemens AG. Until her contract ends on December
31, 2020, Ms. Soussan will remain available to Siemens Mobility in an
advisory capacity.
- Greater comfort for passengers
- Environmentally friendly, energy-saving trains with proven technology
After the first C2 metro train from the first option in 2016 entered service in May, Stadtwerke München (SWM) has also called up the second and final options for 22 six-car metro trains from Siemens. When all trains are delivered, Münchner Verkehrsgesellschaft (MVG) will operate a total of 67 C2 trains on its system.