Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release26 August 2020Siemens Mobility GmbHMunich
Start of Siemens Mobility’s Inspiro trains and automatic train control systems for Metro Sofia
At the official opening of the Medical University metro station, the attendees had the opportunity to experience the comfort and high reliability of the Inspiro trains during a demonstration trip with the new trains.
Michael Peter, CEO Siemens Mobility, said: “We are proud to have delivered one of the most successful and environmentally friendly trains in the field of urban rail transport, which will change the way people travel across Sofia. Our Inspiro trains were developed with a special emphasis on low energy consumption, optimized maintenance, access for everyone and environmental considerations. At the end of its service life, up to 95 percent of the rolling stock can be recycled.”
In March 2016 Metropolitan EAD commissioned a consortium consisting of Siemens and the Polish train manufacturer Newag to equip the new metro line 3 in the capital of Bulgaria. The initial order was related to the first phase of this construction project for the first eight kilometers with seven stations and comprised the delivery of 20 Inspiro type metro trains along with the automatic Communication-Based Train Control (CBTC, onboard and wayside) system Trainguard MT, the Trackguard Westrace MKII interlocking, Clearguard-ACM-200 axle counter system, the automatic train supervision system Controlguide OCS, the voice radio and data transmission system, the Power SCADA Sitras RSC system, the wayside digital communication network, the passenger information displays in the stations including the Digital Station Manager (DSM) and half-height platform screen doors for the stations.

Siemens provides trains and automatic train control system for new metro line in Sofia
Later, the order was extended with an option for ten more trains as well as the required automation system for the metro operation. The extended contract included the delivery of CBTC, Interlocking, ATS, voice radio, Power SCADA, DSM and platform screen doors for a further five additional stations. The last train will be delivered by April 2021.
The Inspiro car bodies have been built at Siemens Mobility plant in Vienna, Austria, while the bogies are manufactured at the Siemens Mobility plant in Graz. Final assembly, factory train testing, and static commissioning of the trains takes place at Newag's plant in Nowy Sacz, Poland.
The trains can travel at speeds of up to 80 kilometers per hour. Their floor is a weight-saving, sound-absorbent composite cork-aluminum plate. They also feature a highly redundant traction and brake system (bogie-oriented), ensuring a high level of availability and electrodynamic braking almost down to standstill.

For further information about the topic,
please see
https://www.mobility.siemens.com/global/en/portfolio/references/metro-sofia.html
Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2019, which ended on September 30, 2019, the former Siemens Mobility Division posted revenue of €8.9 billion and had around 36,800 employees worldwide. Further information is available at: www.siemens.com/mobility.
Reference Number: HQMOPR202008255976EN
Contact
Silke Thomson-Pottebohm
Siemens Mobility GmbH
Nonnendammallee 101
13629 Berlin
Germany
13629 Berlin
Germany
+49 (174) 3063307