Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release24 September 2020Siemens Mobility GmbHMunich
Siemens Mobility to install CBTC on Jurong Region Line in Singapore
“We are delighted to have the opportunity to build on our existing technology partnership with Singapore’s Land Transport Authority and deliver intelligent mobility solutions that support Singapore’s continued efforts to effectively manage their urban development,” said Michael Peter, CEO of Siemens Mobility. “The state-of-the-art CBTC signaling technology for the Jurong Region Line will allow this new rail option to operate with superior availability and automation, featuring a high degree of service reliability and passenger experience.”
The JRL is currently under development and once completed will be Singapore’s seventh MRT line. The line will be comprised of three branches, 24 stations, and span 24 kilometers of track. It will serve both existing and future development in the western part of Singapore and will significantly improve connectivity of the region and support the development of the Jurong area. The JRL is expected to put 60,000 more households in Jurong within a 10-minute walk from a train station. The JRL is scheduled to open in 3 stages – with the final stage being finalized in 2028.
Trainguard Sirius is the Siemens Mobility high-performance CBTC system which lets operators maximize their network capacity and throughput. The radio-based technology provides real-time data on vehicle position and speed conditions, allowing system operators to safely increase the number of vehicles on a rail line. Additionally, the technology precisely locates each train on the tracks and controls speed, improving safety for riders and employees, while also providing the ability for continuous updates on system status that results in fewer delays and up-to-date travel information. Trainguard Sirius is currently being used for the Downtown Line in Singapore, Turkey, Brazil, Spain, China and Venezuela.
This project will build on the already well-established relationship, Siemens Mobility has with Singapore. That includes providing the signalling and the test center for the Downtown Line (DTL), one of the world´s longest suburban fully automated metro lines, as well as providing electrification for two other mass transit projects: Circle Line Stage 6 and North East Line extension. Siemens Mobility also operates one of its digital labs in Singapore, which is transforming the future of road traffic by conducting extensive autonomous driving research with its partner CETRAN.

Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2019, which ended on September 30, 2019, the former Siemens Mobility Division posted revenue of €8.9 billion and had around 36,800 employees worldwide. Further information is available at: www.siemens.com/mobility.
Reference Number: HQMOPR202009155991EN
Contact
Silke Thomson-Pottebohm
Siemens Mobility GmbH
Nonnendammallee 101
13629 Berlin
Germany
13629 Berlin
Germany
+49 (174) 306 3307