- Desigo CC Compact for small and medium-sized buildings
- Improved connectivity to support KNX and M-Bus protocols
- Powermanager module for efficient energy systems and demand optimization
- New cloud application
Desigo CC, the integrated building management platform from Siemens Smart Infrastructure, has been updated to version V4, making it suitable for use across a wider range of buildings. The technology enables building operators to boost energy efficiency while ensuring the comfort and safety of tenants. Every construction, from commercial and residential buildings to educational and medical facilities is compatible with Desigo CC. Equipped with multidiscipline support, including fire safety, power management, lighting, HVAC and physical security, Desigo CC turns buildings into living environments that can interact with their occupants and adapt to their changing needs by collecting and analyzing building-generated data. Now, with the product portfolio extension, Desigo CC Compact, provides precise scalability and flexibility in usage also for small and medium-sized buildings.
Independent industry research company Verdantix has recently ranked
Siemens Smart Infrastructure as a leading provider of the Internet of Things
(IoT) platforms for smart buildings. The “Green Quadrant IoT platforms for
Smart Buildings 2019” report assesses 13 companies that Verdantix considers as
shaping the market, which is still at its infancy but seeing strong
competition.
- Five sensors in a single device for optimal ambient conditions and maximum energy savings
- Control of lighting, ventilation and heating systems
- Precise readings, monitoring and control of energy consumption
- Fast installation thanks to a single KNX cable
The new presence detector WIDE UP 258Dx1 from Siemens Smart Infrastructure can now for the first time contribute to energy-efficient lighting and climate control without having to rely on additional accessories thanks to its built-in multi-sensor technology. It is part of the GAMMA instabus building system technology portfolio, a series of products based on the worldwide KNX standard and with five different sensors for HVAC and lighting control. Dedicated sensors record presence, brightness, temperature, humidity and CO2 levels, guaranteeing perfect room conditions in commercial buildings with substantial room depth and high occupancy fluctuations.
- New devices for electrical installations in industrial and infrastructure environments with a lower nominal current of 0.1 to 0.4 amperes
- Firmware update with improved control and diagnostic functions
- Failsafe group shutdown function without additional wiring
Siemens Smart Infrastructure is adding four new devices to its portfolio of Simatic ET 200SP motor starters, which can be used to start electric drives with a power output from 0.1 to 0.4 amperes (A). These types of drives are found in fans and coolant pumps, for example. The compact motor starters are installed in control cabinets and are designed to start single and three-phase motors of machines and systems, protecting them against overloads and short-circuits. They are each available in standard and safety variants.
- Exact recording of energy consumption and electrical parameters
- Secure data transfer over existing communication networks
- Flexible use in industrial and commercial buildings as well as data centers
Siemens Smart Infrastructure has added the 7KM PAC3220 and 7KM PAC3120 measuring devices to its Sentron power monitoring portfolio. These devices capture energy and system data from buildings, infrastructure and industrial facilities and transfer them via standard communication protocols to higher-level energy management, automation and IoT systems. This data can then be used to identify energy hogs, detect system malfunctions as early as possible and proactively prevent downtimes. This allows companies to sustainably boost their energy efficiency and system availability. The new devices offer higher accuracy than the previous models and have a new design.
- New trend to supply renewable energy for mines as secure and cost-efficient alternative to fossil fuels
-
- Siemens' proven microgrid controller serves as technical basis for juwi's Hybrid IQ microgrid solutions
- Two projects in Australia successfully delivered, paving way for partners to roll-out solution in other countries
Siemens and the renewable energy developer juwi have joined forces to enter into a strategic technology partnership to focus on microgrids in the mining industry. A corresponding agreement was signed today. The two companies aim to roll-out and continually develop the advanced microgrid control system that enables the seamless integration of power from renewable energy to a mine's off-grid power supply. The Siemens Sicam based microgrid control platform is a proven and tested technology which is the basis for juwi's Hybrid IQ microgrid controller. juwi, on the other hand, brings industry-specific domain know-how and an excellent track record of planning and executing renewable energy projects at mine sites.
- Designed for future power networks and digital substations
- Enhanced cyber security and communications
- User-friendly interfaces and software
With the new Reyrolle 5 series of protection relays, Siemens is further developing its offerings for medium-voltage and industrial power networks. The protection, control, monitoring and measuring of power networks is a vital element in managing electrical assets, increasing reliability, sustainability and the safety of operating personnel. The first device applications of the new generation of protection relay will be overcurrent and earth fault protection and transformer protection in substations. It includes comprehensive functionality as standard, with enhanced process data such as faults, events and waveform records enabling the power network to be effectively managed. The small number of device variants allows easy ordering and efficient engineering while the improved hardware platform makes it even easier to operate and manage the protection relays.
- New Grid Diagnostic Suite offers unique comprehensive insights
- Gain a grid-wide view of energy automation systems
- Market launch of initially four cloud-enabled applications
- Enhances cost efficiency and availability of smart grids
- Support through digitalization in increasingly complex power grids
Siemens is presenting for the first time its new Grid Diagnostic Suite at the European Utility Week in Paris. The Grid Diagnostic Suite initially includes four cloud-based applications which collect data from new or existing field devices for protection, distribution automation and power quality. These data are stored and analyzed in the cloud. This requires almost no additional engineering effort. Distribution grid operators and operators of electricity grids in industrial parks can quickly tap into useful information from devices installed anywhere in the smart grid. This will enable grid faults, for example, to be detected at an early stage and quickly rectified. After information is collected, vulnerabilities can be identified, and necessary measures can be implemented before any damage occurs. In this way, Internet of Things (IoT) applications in the Grid Diagnostic Suite enhance the availability of power grids while enabling them to be operated cost-efficiently.
- Highly compact design, up to 110 kiloamps
- Maintenance-free up to 10,000 interrupting cycles at current of 15 kA
- Based on proven HB3 generator platform with vacuum switching tech
Siemens is expanding its HB3 generator circuit-breaker portfolio with a new compact version. The HB3-Compact (HB3-C) offers the possibility for vertical or horizontal mounting and uses maintenance-free vacuum switching technology. These features make it especially valuable for retrofit applications in power plants, where the highest security of supply is crucial, and space is limited due to existing installations. The new system will be presented for the first time at the European Utility Week 2019, taking place in Paris from November 12 to 14.
- First soft starter series with integrated Safe Torque Off function
- Enhanced protection when shutting down electric motors
- High functional density saves space and decreases cost
Siemens Smart Infrastructure expanded its soft starters portfolio for motors, with the launch of Sirius 3RW55 Failsafe and Sirius 3RW50. Soft starters ensure electrical motors used in industry and infrastructure are protected during startup and ramp-down. The Sirius 3RW55 Failsafe soft starters are the first to feature the integrated Safe Torque Off (STO) function. As specified in safety standards, the protection function for electrical drive systems ensures that torque-generating energy stops acting when motors are turned off, preventing an unwanted restart. Control panel manufacturers no longer require using separate individual components to have this function, which reduces the time and effort for wiring and maintenance works and saves space in the control cabinet. In addition, the switching time of the integrated solution is significantly shorter than for conventional, electromechanical components.