Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release26 November 2019Smart InfrastructureZug
Siemens launches new starters for smaller motors and improved system monitoring

The Simatic ET 200SP motor starters are part of an end-to-end distributed peripheral system with outputs of up to 5.5 kilowatts (kW) and cover nearly all motor applications in industry and infrastructure. The new failsafe devices ensure full functionality at elevations up to 4,000 meters.
Other portfolio innovations include updated firmware and a simplified group shutdown function. The updated V1.2.0 firmware makes it possible to control the Simatic ET 200SP motor starters directly from the Siemens Totally Integrated Automation (TIA) Portal and perform tests with the connected motor. It also offers more comprehensive and precise diagnostic capabilities. System and current values detected by the motor starters can be visualized in the TIA Portal and used for operational energy management. This makes it possible to draw conclusions about wear or operating faults as the basis for energy-efficient operation and predictive maintenance.
The firmware also includes a parameter lock, which prevents settings from being unintentionally changed or deactivated, as well as a class-off mode for operating motors without additional protective function.
The firmware also includes a parameter lock, which prevents settings from being unintentionally changed or deactivated, as well as a class-off mode for operating motors without additional protective function.
The failsafe group shutdown function has been optimized as well. New base units to which the devices are connected now enable command signals to be forwarded from the input point directly to other motor switches in the Simatic ET 200SP series over the associated rail with digital input module (F-DI). No additional wiring is needed for this purpose.
For further information on Siemens Smart Infrastructure, please see
www.siemens.com/smart-infrastructure
For further information on Simatic ET 200SP motor starts, please see
www.siemens.com/et200sp-motorstarter
www.siemens.com/smart-infrastructure
For further information on Simatic ET 200SP motor starts, please see
www.siemens.com/et200sp-motorstarter
For this press release
Social Media
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 72,000 employees worldwide.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR201911135681en
Contact
Heidi Fleissner
Smart Infrastructure
Siemensstr. 10
93055 Regensburg
Germany
93055 Regensburg
Germany
+49 (941) 790 2212