- Edge Devices to collect and process large data volumes directly at the machine
- Secure, future-proof basis for the execution of Industrial Edge applications
- Simple update procedure and software rollouts through secure link to central Edge Management System
- Savings through edge computing in the Siemens Electronics Factory Amberg
At the SPS IPC Drives 2018 in Nuremberg, Siemens will be showcasing a newly developed hardware platform for edge applications as part of its Siemens Industrial Edge concept: The compact Simatic Edge Device works on the basis of the embedded industrial PC Simatic IPC227E, and features integrated connectivity to automation on the machine level. This allows manufacturing data to be captured and processed directly at the point of production. If there is a change to the framework conditions underlying the industrial application, Industrial Edge offers facility to adjust software applications on the Edge Device, keeping them right up to date using functional, feedback-free updates. The hardware comes with a closed all-metal housing, ensuring maximum industrial functionality for flexible, maintenance-free use under even the harshest of conditions. Rapid commissioning is guaranteed using pre-installed Edge software.
The Supervisory Board of Siemens AG has extended the appointment of Managing Board member Lisa Davis (55) ahead of schedule. Her term of office will now continue until the end of October 2020. This move is a sign of continuity in the context of the implementation of the company's new Vision 2020+ strategy program. Her contract will subsequently extend automatically by one year until the end of October 2021, provided that neither Lisa Davis nor the Supervisory Board objects.
- Industrial PC for use as an IoT gateway enables data to be managed directly in the production environment
- Based on Windows or Linux, for networking machinery of different manufacturers and of different technological versions
- Fitted with up to 3 LAN interfaces for high connectivity
- Pre-configured versions available from stock
Siemens has expanded its product portfolio of Simatic industrial PCs to include the Simatic IPC127E. The newly developed industrial PC is suitable, for example, for use as a gateway and enables data to be managed directly in the production environment. Whether it is based on Windows or Linux, the Simatic IPC127E makes it possible to network existing systems with machinery of different manufacturers and different technological versions. Thanks to the compact enclosure of just 0.3 liters, it can be integrated with a minimum space requirement in the cabinet or directly at the machine.
- New Sinamics converter family series optimized for pump and fan infrastructure applications
- 0.75 to 630 kW power range allows operation with any motor
- Stable running under any network conditions thanks to integrated DC link reactor
- Sinamics G120X is digitalization-ready and can be linked directly to the cloud with Sinamics Connect 300
Siemens will be presenting a brand new converter series at this year's SPS IPC Drives. The converters of the new Sinamics G120X series are especially suited for use in pump and fan applications in industries such as water/wastewater, building technology or also in industrial environments. With a power range of 0.75 to 630 kW, Sinamics G120X converters can be operated with any motor. The converters are at their most effective running with synchronous reluctance motors from Siemens. Sinamics G120X are configured throughout for cost-optimized and resource-saving operation across all voltages and supply networks, and their characteristic compact design saves space in the control cabinet. Although not featuring an additional output reactor, the converters enable motor cable lengths of up to 150 meters. The integrated safety functions are certified to SIL3.
- New TM NPU module for the S7-1500 and ET 200MP with integral AI-capable chip: Intel Myriad X
- Evaluation of input data such as video, sound or CPU data by means of neural networks
- Use of machine-learning algorithms in production processes
- Efficient implementation of pick-and-place applications or quality checks on the basis of (human) expert knowledge
Siemens is launching onto the market a new module for the Simatic S7-1500 controller and the ET 200MP I/O system, which has a chip with artificial intelligence (AI) capability: The S7-1500 TM NPU (neural processing unit) is equipped with the Intel Movidius Myriad X Vision processing unit, thus enabling the efficient processing of neural networks. The module gets its function from the provision of a trained neural system on an SD card and is equipped with the USB 3.1 interfaces and a Gigabit Ethernet port. On the basis of the neural network, data from a connected sensor system or from the CPU program can be processed. By using machine-learning algorithms, for example, visual quality checks in production plants or image-guided robot systems can be efficiently realized. This makes a considerably more efficient and more "human-like" behavior possible. With this module, Siemens is taking another step toward the integration of future technologies into industrial applications.
- VAG Verkehrs-Aktiengesellschaft Nürnberg exercises first option
- A total of 27 metro trains to be delivered
- Greater passenger comfort and optimized passenger flows
VAG Verkehrs-Aktiengesellschaft, Nuremberg's public transport operator, has ordered six additional type G1 metro trains from Siemens Mobility, exercising one of two options in the contract signed in December 2015. All in all, Siemens Mobility will now be supplying 27 new metro trains for Nuremberg. The new four-car G1 trains in the first option are planned for use on the U1 metro line as of 2021 and will replace twelve type DT2 two-car trains.The metro trains will be built at the Siemens Mobility plant in Vienna, Austria. Various vehicle components, such as drive converters, motors, auxiliary converters and control systems, will be manufactured in Nuremberg. Project management, development and service support will be handled in Erlangen.
- Integration of artificial intelligence and edge computing into Digital Enterprise portfolio
- Networking concepts from factory floors to corporate offices
- Growing ecosystem surrounding MindSphere
By expanding its Digital Enterprise portfolio and integrating future technologies, Siemens is driving forward the digital transformation of the discrete and process industries. "An ever-increasing number of industrial enterprises, particularly SMEs, are well on the way towards Industrie 4.0, and are already improving their competitive standing with digital solutions," explained Klaus Helmrich, Member of the Management Board of Siemens AG, at the SPS IPC Drives. "This applies to all sectors of industry with rapidly changing market demands in which products have to be manufactured ever more quickly, flexibly and in diminishing quantities. With the further integration of technologies such as artificial intelligence (AI) and edge computing into our portfolio, we're paving the way for the future of industry." Siemens will be present at the fair with an array of innovations and industry-specific applications, ranging from automation and edge devices using artificial intelligence in applications such as machine tools, production machinery and process plants through to integrated networking concepts from factory floors to corporate offices. These all help to drive forward the use of innovative automation and software solutions.
The digital transformation of the producing industry is gaining momentum. Companies from a wide variety of industries are already unlocking this potential – they are using end-to-end digitalization to create a lasting competitive edge by reducing time to market and increasing flexibility, efficiency, and quality. With Siemens Digital Enterprise solutions the technical prerequisites for the implementation of Industrie 4.0 are available and can be deployed in every application and companies of all sizes. At the SPS IPC Drives in Nuremberg, Germany, from November 27 to 29, 2018 – which took place this year under the motto "Digital Enterprise – Implement now" – Siemens showed in hall 11 how this can be done.
- Active support of OPC UA and Time-Sensitive Networking (TSN) technology
- Commitment to driving OPC UA with TSN forward within the OPC Foundation
- Comprehensive support of the OPC Foundation with Profisafe domain know-how for functional safety communication based on OPC UA
- Profinet based on TSN as mainstream solution at the field level
Siemens welcomes the initiative previously published by the OPC Foundation to further enable OPC UA adoption throughout industrial automation by extending standardization and harmonization activities for OPC UA, including TSN-enabled Ethernet networks at the field level. Siemens, as a founding and board member of the OPC Foundation, is a strong supporter of the OPC UA technology and has been active in core standardization working groups for many years.