[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release28 November 2018Digital Factory Nuremberg
Compact Industrial PC Simatic IPC127E connects machines with each other and with the cloud
Industrial PC for use as an IoT gateway enables data to be managed directly in the production environment
Based on Windows or Linux, for networking machinery of different manufacturers and of different technological versions
Fitted with up to 3 LAN interfaces for high connectivity
Pre-configured versions available from stock
Siemens has expanded its product portfolio of Simatic industrial PCs to include the Simatic IPC127E. The newly developed industrial PC is suitable, for example, for use as a gateway and enables data to be managed directly in the production environment. Whether it is based on Windows or Linux, the Simatic IPC127E makes it possible to network existing systems with machinery of different manufacturers and different technological versions. Thanks to the compact enclosure of just 0.3 liters, it can be integrated with a minimum space requirement in the cabinet or directly at the machine.
Industrial PC for use as an IoT gateway enables data to be managed directly in the production environment
Based on Windows or Linux, for networking machinery of different manufacturers and of different technological versions
Fitted with up to 3 LAN interfaces for high connectivity
Pre-configured versions available from stock
Siemens has expanded its product portfolio of Simatic industrial PCs to include the Simatic IPC127E. The newly developed industrial PC is suitable, for example, for use as a gateway and enables data to be managed directly in the production environment. Whether it is based on Windows or Linux, the Simatic IPC127E makes it possible to network existing systems with machinery of different manufacturers and different technological versions. Thanks to the compact enclosure of just 0.3 liters, it can be integrated with a minimum space requirement in the cabinet or directly at the machine.
Compact Industrial PC Simatic IPC127E connects machines with each other and with the cloud
The Simatic IPC127E is equipped with a powerful 2 or 4-core Atom processor with 2 or 4 GB RAM and a solid state drive (up to 128 GB). The 3 LAN and 4 USB interfaces enable it to be integrated in already existing automation systems. The enclosed all-metal enclosure enables the new industrial PC to be used flexibly and maintenance-free even under harsh conditions.
The newly developed Simatic IPC127E makes it possible to reliably record, collect, process and transfer data directly in the production environment and can also be flexibly used as an IoT gateway between the cloud or the corporate IT level and production. Thanks to pre-configured versions, the right product is available to users in a very short time.
Background information:
As a result of increasing digitalization, the interfacing of production to the office IT is an ever important component of corporate policy.
Machinery from different manufacturers and on different technological levels does not speak the same data language. Thus the integration of already existing systems often poses a challenge – the solution to this is provided by open IoT gateways that enable future-oriented production concepts to also be implemented for existing systems.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.