Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release27 November 2018Digital Factory Nuremberg
Artificial Intelligence for Simatic

The picture shows the module S7-1500 TM NPU (Neural Processing Unit).
The installed VPU, Intel's new Myriad X VPU chip, is the first in its class to have a dedicated hardware accelerator for deep neural network structures. The integrated image processing unit together with the computing unit for neural networks makes the Myriad X the trailblazer for computer vision applications. The integral Intel chip facilitates new applications in industrial automation by speeding up the image-processing processes and fast local data evaluation by means of the trained models.
Users can connect compatible sensors such as cameras or microphones to the integrated interfaces of the newly developed S7-1500 TM NPU module. The data of the connected sensor systems, as well as information from the CPU program itself, can be processed using neural networks. The result of processing is then evaluated in the CPU program. Where the data of each workpiece must be configured most precisely for the recognition of workpieces using conventional image processing, this process can be structured with considerably more flexibility by applying learning procedures to identified image data. Open AI frameworks such as Tensorflow are used for this purpose.
The resulting advantage comes to bear, for example, during pick-and-place applications, in which a mobile robot must recognize, pick out and place components that are lying randomly in a crate. Added value can thus also be achieved during quality checks: Human expert knowledge regarding parameters such as consistency, color or quality of a product or a process can be transferred direct to the module through the continuous training of a neural network with assigned (image) data, e.g. by means of a connected camera.
Background information:
Artificial intelligence, with all its different facets, makes a considerable contribution, especially in industry, toward reducing the usual expense of programming and engineering, making the control logic more agile and flexible with regard to changes in the ambient conditions and structuring production processes with greater flexibility and precision.
With Future of Automation, Siemens is offering far-reaching insights into the future of automation and the role of artificial intelligence within the portfolio of Totally Integrated Automation. This means scalable solutions from the field level to the controller and edge level and all the way to the Cloud. This means that an AI solution can be scaled in terms of the environment and the target application: At the machine on the field level where fast, deterministic decisions are required, or across all machines or plants with a significantly higher quantity of data to be processed and a corresponding demand for computing power.
For further information, go to www.siemens.com/et200mp
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Andreas Friedrich
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (1522) 2103967