Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens supports OPC Foundation Initiative to extend OPC UA, including TSN down to the field level

The picture shows the scope of OPC UA

Siemens has extensive experience and a long history in the development and standardization of industrial communication systems. Siemens is actively participating in all relevant standardization bodies like IEEE, IEC, IETF, PI, OPC F, and many more not only as editor but also even as the convener and lead of the whole working group.
The latest example of Siemens leadership is the foundation of the international IEC/IEEE 60802 standardization group by Siemens. This group will standardize the so called "TSN Profile for Industrial Automation (TSN-IA Profile)" to ensure a multivendor converged TSN network approach for industrial automation where different applications and protocols like OPC UA, PROFINET, EtherNet/IP, etc. can share the same TSN network infrastructure. Additionally, an appropriate set of IEEE basic standards will be selected to run the different protocols on one and the same hardware base.
Siemens shares the vision of the OPC Foundation to extend the scope of OPC UA down to field level communication and is looking forward to contributing in standardization activities in the upcoming working groups of the OPC Foundation concerning information models for devices, necessary adaption of OPC UA core standards, application profiles, etc.
Use cases which have not been well addressed in today's industrial communication systems so far, like multi-vendor controller-to-controller communication or vertical communication from devices to upper systems via OPC UA, will be adopted first by the market. Therefore, joint working groups between PI and OPC F members were started several months ago. These working groups are addressing topics such as the standardization of Safety over OPC UA based on Profisafe mechanisms for controller-to-controller communication, and the mapping of Profinet into the OPC UA information model for multiple use cases, e.g. asset management and diagnostics. Customers can shortly benefit from these features without waiting for TSN by simply running the OPC UA protocols on existing PROFINET network installations. The PI organization contributes its technology expertise to the OPC Foundation, e.g. by opening the Profisafe mechanisms to be used via OPC UA and extending the respective rights to OPC Foundation members.
Field device level communications with cyclic IO communication, motion control and safety, will need an established ecosystem with stack providers, certification procedures, tools, and many more. Organizations like PI, ODVA, and others have put effort into completeness and quality of specifications, conformance testing, maintaining a vendor and user community, and we expect a similar approach with the new OPC Foundation setup.
Siemens bears high responsibility towards its installed base and therefore will continue in innovating Profinet to protect our customers' investments and to bring Profinet based on TSN to the next level. The converged TSN network and common hardware platforms for Profinet and OPC UA enable a smooth migration into the new TSN world. In addition, we ensure that with OPC UA including TSN, the fundamental principles in field device communication, engineering workflows, conformance testing, diagnostics, etc. will stay unchanged.
In the end, our customers will decide if and where to use OPC UA technology or Profinet technology for their individual applications.

For further information, please see www.siemens.com/opc-ua
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR2018110079DFEN

Contact

Andreas Friedrich

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (1522) 2103967