Siemens Mobility to install a 2,000 km state-of-the-art high-speed rail network that will connect 60 cities throughout the country with trains that can operate up to 230 km/h. The integrated system will create the 6ᵗʰ largest high-speed rail network in the world, and will provide 90% of Egyptians access to a modern, safe, and affordable transportation system. The fully electrified network will cut carbon emissions by 70% compared to current car or bus transport, further supporting Egypt’s efforts in transforming its mobility to a more sustainable one. Siemens Mobility will deliver 41 Velaro high-speed trains, 94 Desiro High Capacity regional train sets, and 41 Vectron freight locomotives. This contract also includes the development of eight depots and yards and 15 years of maintenance.
- Siemens successfully completed the first phase of its shallow water test of the Subsea Power Grid.
- The development program was conducted in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge.
- This will be the world's first Subsea Power Grid for medium voltage power distribution using pressure compensated technology.
Siemens has successfully concluded the first phase of its Subsea Power Grid shallow water test in Trondheim, Norway. Siemens, in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge, is in the final stages of a program to develop a barrier-breaking system that will become the world’s first Subsea Power Grid designed for distribution of medium voltage power using pressure compensated technology.
In a consortium with the general infrastructure contractor Per Aarsleff A/S, Siemens has received an order to build a light rail system in Copenhagen, Denmark, from urban transport development company Greater Copenhagen Light Rail I/S. The contract will be implemented as a turnkey project. Commissioning of the system is planned for 2024.
Siemens has received an order from the Qatar Foundation for the turnkey construction of a tram system in the capital Doha aimed at transforming Qatar into a knowledge-based society. The order is worth more than 100 million euros. The scope of supply also includes signaling and communication systems, electrification as well as the depot equipment. Siemens will also be equipping four of the stations with platform edge doors. Nineteen Avenio trams will run on 11.5 kilometers of track without any overhead contact lines. The system will be installed on the university campus and serve 25 stations. The trams will be equipped with the Sitras HES energy storage system from Siemens, with energy being supplied at the tram stops.
Fraport AG, operator of the Frankfurt Airport, has commissioned Siemens, lead in a consortium with Max Bögl Group and Keolis Deutschland GmbH & Co. KG, to deliver a fully automated Airval people mover. The Airval will connect the Terminal 2 with the new Terminal 3 and the Station at Terminal 1. The line will be 5.6 kilometers long, and have two tracks and three stations. Siemens will deliver 12 fully automated two-car trains equipped with GoA4 Communication Based Train Control Trainguard MT CBTC, the trackwork equipment, the station platform doors, communication system, depot equipment and the power supply system. In addition, Siemens will take over the operation and maintenance of the system for five years with an option to extend service for another five years. The Airval system will be designed and developed at Siemens' Val world center of competence in Toulouse, France. The fully automated people mover is scheduled to begin service at the Frankfurt Airport in 2023.
Deutsche Bahn
(DB) and Siemens Mobility are driving forward the climate-friendly transition
in transport and are testing the use of hydrogen for rail for the first time.
The aim is to test a completely new overall system consisting of a newly
developed train and a newly designed filling station.
Siemens Mobility's Vectron locomotives are used for both freight and passenger service. During the development of the locomotive, the focus was on providing a future-proof design, investment security, environmental compatibility, fungibility, retrofitting capability and convertibility. The Vectron can be delivered as a purely electrical version for operating with alternating current (AC) or direct current (DC) power systems as well as a multisystem (MS) variant in the power classes 5.2 MW, 5.6 MW and 6.4 MW. Along with the desired national train control system, the locomotives can also be equipped with the latest European Train Control System (ETCS). The locomotives are built in the Siemens Mobility plant in Munich-Allach, Germany. For freight transport in Germany, Siemens Mobility also offers the Smartron standard locomotive and the Vectron Dual Mode, a combination of diesel and electric locomotive.
S-Bahn Berlin GmbH has signed a framework contract with the consortium of Stadler Pankow GmbH and Siemens for the delivery of up to 1,380 vehicles. A firm order was placed for the first 106 trains. The 85 four-section and 21 two-section trains have a high triple-digit million-euro order volume. S-Bahn Berlin, a subsidiary of Deutsche Bahn, plans to use the new trains on the Ringbahn lines (S 41 and S 42) as well as on the system's southeastern feeder lines S 47, S 46 and S 8. These lines comprise roughly one-third of the entire S-Bahn network in Berlin. The first ten vehicles will be ready to enter service as of 2020. Subsequently, all remaining vehicles will be delivered continuously to the Berlin system up to 2023. The vehicles will be manufactured and assembled at the Berlin plant operated by Stadler Pankow GmbH.
Almost 10 billion
people will live on our planet by 2050, most of them in urban areas. About 40
percent of all energy used globally is consumed in buildings, and another one
third by industries. But resources are finite.
Resilient, adaptive, and efficient infrastructure, enabled by digitalization,
is key to sustainability. Taking action to tackle climate change and other
global sustainability issues is an urgency. With buildings and electrification
increasingly growing together and becoming more and more digitalized, they can
support the sustainable infrastructure transition and create more livable
environments.At the Light +
Building 2022 trade fair, Siemens will showcase its vision of digitalization as
the key pillar of the infrastructure transition. Our motto at the show is
“Smart infrastructure is sustainable infrastructure”, outlining our innovations
that will make this possible.Visit us at Light + Building 2022 in Frankfurt am
Main, October 2 - 6, in hall 11.0, B56.
Fluorine gas-free energy distribution for medium-voltage applicationsFluorine gas-free switchgear is a hot topic in the energy sector because this new approach contributes to sustainable power distribution. On this page you will find all information about the sustainable switchgear portfolio from Siemens.