As the global population experiences rapid growth, more people around the world are moving from the countryside to the city. In addition to the inner-city challenges posed by the urbanization megatrend, there is also an increase in the average traveling distance. As a result, the challenges for train systems are also increasing. To meet these demands, Siemens Mobility and Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) have jointly developed new auxiliary converters to improve the efficiency of on-board power systems using power semiconductors based on silicon carbide (SiC).
- An Avenio vehicle equipped with SiC technology spent one year transporting passengers in Munich and covered 65,000 kilometers in the process
- Energy use was cut by 10 percent and motor noise was reduced as well
- Joint research project conducted as part of the European development and research program PINTA
Siemens Mobility and Stadtwerke München (SWM) successfully completed a one-year test of semiconductor technology based on silicon carbide (SiC) in an Avenio streetcar in Munich in August. They have now presented the results of their research. The study found that the motor noise produced by the vehicle fell sharply and that energy use declined as well during the trips that the tram made on Munich’s public-transportation rail network. The semiconductor technology was produced by Infineon Technologies. The tests were conducted as part of the European research and development project PINTA. By taking part in the trial, Siemens Mobility significantly contributed to efforts to integrate SiC power semiconductors into rail vehicles.
The VAG Verkehrs-Aktiengesellschaft Nuremberg has ordered 27 type G1 four-car metro trains from Siemens Mobility. The contract also includes an option for a total of a further 7 trains. These trains are earmarked for service on Nuremberg's U1 line. The trains will be built in the Siemens Mobility plant in Vienna. Core components of the G1 will be manufactured in the Nuremberg metropolitan area and include such products as the drive converters, traction motors, auxiliary converter units and control equipment. The project management, development and service support will be provided from Erlangen.
S-Bahn Berlin GmbH has signed a framework contract with the consortium of Stadler Pankow GmbH and Siemens for the delivery of up to 1,380 vehicles. A firm order was placed for the first 106 trains. The 85 four-section and 21 two-section trains have a high triple-digit million-euro order volume. S-Bahn Berlin, a subsidiary of Deutsche Bahn, plans to use the new trains on the Ringbahn lines (S 41 and S 42) as well as on the system's southeastern feeder lines S 47, S 46 and S 8. These lines comprise roughly one-third of the entire S-Bahn network in Berlin. The first ten vehicles will be ready to enter service as of 2020. Subsequently, all remaining vehicles will be delivered continuously to the Berlin system up to 2023. The vehicles will be manufactured and assembled at the Berlin plant operated by Stadler Pankow GmbH.
In May 2011, the German national railway company concluded a framework agreement with Siemens Mobility for up to 300 trainsets. At this time the largest train contract that Siemens has ever won in its corporate history.The ICE 4 sets new standards in intercity traffic. A unique train concept has been developed, that means it can be individually adapted to the requirements of various transport tasks. The modular drive concept is based on independent Powercars with identical traction technology, resulting in more flexibility than ever before. High operational availability is guaranteed by a large number of reliable systems with high redundancy.All in all, DB will be receiving 1,511 cars with which it can configure 50 12-car, 50 13-car and 37 7-car trainsets. In addition, Deutsche Bahn has awarded Siemens Mobility a contract for the revision of 40 ICE 4 trains.
"Lead the TRANSITion" was the motto of this year's UITP International Mass Transit Trade Show in Montreal. At the bi-annual Global Public Transport Summit, the Siemens Mobility Division was again be represented this year with intelligent mobility solutions. From May 15 to 17, 2017, at booth (SK100) on Level 02 of the Conference Center, Siemens was showcasing integrated and sustainable transport solutions which help to get the best out of existing infrastructures – using not only state-of-the-art hardware but also intelligent management systems. This is the only way to deliver future-proof mobility services in the face of rising energy costs, limited space and growing demands. Digitalization of proven transport solutions plays a key role in achieving this goal, as it allows availability and passenger comfort to be improved and throughput to be maximized.