Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

SiC semiconductor technology in tram: Siemens Mobility and Stadtwerke München successfully conclude test

“We would like to thank Stadtwerke München for the good partnership we had during the tests of SiC semiconductor technology in an Avenio München,” said Albrecht Neumann, CEO of Rolling Stock at Siemens Mobility. “The energy-saving potential found by the test clearly demonstrates the energy efficiency of this promising technology that is designed for use in all types of trains.”
Ingo Wortmann, the Head of Mobility at Stadtwerke München (SWM), added: “One factor plays a key role in the acceptance of trams – particularly in terms of new construction projects: Our vehicles must be as quiet as possible while in service. The project conducted with Siemens shows that we can not only optimize the noise levels of our vehicles but also improve our energy efficiency. We would be very interested in this solution if these improvements could be commercially mass-produced.”
During the test in Munich, SiC semi-conductor technology was installed in one of two traction converters used by a three-car Avenio tram. The test phase included all development tests necessary to gain authorization for technology’s use in passenger service that were conducted in the company’s system test center and in the vehicle. The continuous monitoring of energy levels showed an approximate 10 percent reduction in energy consumption. The measurements also found lower noise levels during operations and an overall reduction in motor noise. The Avenio München equipped with a SiC core spent one year transporting passengers and covered 65,000 kilometers in the process.
The PINTA project is part of a far-reaching European research and innovation initiative called Shift2Rail. The goal of this initiative is to create a visionary rail system in Europe through targeted investments. Two of three project phases have now been completed: the initial planning stage and the successful vehicle test for the SiC converter. The focal point of PINTA3 will be system optimization created by the use of SiC in dual-system trams (TramTrain). The objective of the PINTA project is to fuel the introduction of SiC technology in order to lower life-cycle costs and thus bolster the rail industry in Europe. The technology is already being used in a range of industrial sectors, including automotive electromobility.
This project has received funding from the Shift2Rail Joint Undertaking (JU) under grant agreement No. 826054. The JU receives support from the European Union’s Horizon 2020 research and innovation program and the Shift2Rail JU members other than the Union.
SiC semiconductor technology in tram: Siemens Mobility and Stadtwerke München successfully conclude test
New semiconductor material, new connection technology: In Infineon's XHP2 module, silicon carbide and copper ensure greater efficiency and reliability in the tram's motor drive.
SiC semiconductor technology in tram: Siemens Mobility and Stadtwerke München successfully conclude test
SiC semiconductor technology in tram: Siemens Mobility and Stadtwerke München successfully conclude test.

For this press release

Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2020, which ended on September 30, 2020, Siemens Mobility posted revenue of €9.1 billion and had around 38,500 employees worldwide. Further information is available at: www.siemens.com/mobility.
Read more
Reference Number: HQMOPR202111256355EN

Contact

Eva Haupenthal

Siemens Mobility GmbH

+49 152 01654597