- New devices for electrical installations in industrial and infrastructure environments with a lower nominal current of 0.1 to 0.4 amperes
- Firmware update with improved control and diagnostic functions
- Failsafe group shutdown function without additional wiring
Siemens Smart Infrastructure is adding four new devices to its portfolio of Simatic ET 200SP motor starters, which can be used to start electric drives with a power output from 0.1 to 0.4 amperes (A). These types of drives are found in fans and coolant pumps, for example. The compact motor starters are installed in control cabinets and are designed to start single and three-phase motors of machines and systems, protecting them against overloads and short-circuits. They are each available in standard and safety variants.
At "SPS – Smart Production Solutions" 2019, Siemens will present sector-specific applications and future technologies for the digital transformation of the discrete and process industries. At the heart of the 4000 square meter booth will be new products, solutions and services from the Digital Enterprise portfolio, which can be used to merge the real and virtual world.
On November 26, the first day of SPS, Klaus Helmrich spoke at the Siemens press conference, which took place in the trade show Convention Center. Mr Helmrich discussed the latest trends in digitalization and the next stage of digital transformation in the discrete and process industries.
- First soft starter series with integrated Safe Torque Off function
- Enhanced protection when shutting down electric motors
- High functional density saves space and decreases cost
Siemens Smart Infrastructure expanded its soft starters portfolio for motors, with the launch of Sirius 3RW55 Failsafe and Sirius 3RW50. Soft starters ensure electrical motors used in industry and infrastructure are protected during startup and ramp-down. The Sirius 3RW55 Failsafe soft starters are the first to feature the integrated Safe Torque Off (STO) function. As specified in safety standards, the protection function for electrical drive systems ensures that torque-generating energy stops acting when motors are turned off, preventing an unwanted restart. Control panel manufacturers no longer require using separate individual components to have this function, which reduces the time and effort for wiring and maintenance works and saves space in the control cabinet. In addition, the switching time of the integrated solution is significantly shorter than for conventional, electromechanical components.
Let the good times roll: Starting September 21, about six million people from all around the world will be enjoying themselves at the Oktoberfest in Munich for two weeks. Traditionally, Siemens supplies drives and control systems as well as energy distribution for the festival's rides. Automation solutions from Siemens also control special beer pipelines – the only ones of its kind worldwide –that supply the Hacker, Winzerer Faehndl and Braeurosl festival tents with their tasty Oktoberfest brews. Because many breweries use Siemens technologies within their brewing process, Siemens doesn't only ensure fresh beer at the Oktoberfest.
- Voltage variant of Sinamics G120X for USA and Latin America
- Save space with new size for the Sinamics V20
- Adapter kit to physically and thermally separate power module and control unit for Sinamics G120
With numerous innovations, Siemens is extending its drive portfolio, improving user-friendliness and offering space-saving installation options. The Sinamics G120X converter, designed specifically for use in water/wastewater applications and in HVAC systems, is now also available in a three-phase 3AC 200V voltage variant in the power range up to 55 kW. This means that the converters can now be integrated seamlessly into applications in the USA and in Latin America. Due to its robust construction and the coating of the PCBs according to 3C3 standard the converter is suitable for harsh environments. The new module for extending the digital and analog inputs and outputs increases the flexibility and the optimal control of converter-guided applications. The Sinamics G120X now also supports the communication protocols Profibus, Modbus RTU, USS and BACnet MS/TP. It is equipped with extensive interfaces and can be easily integrated into existing or new systems.
- New power output module boosts HCS4300 heating control system performance
- HCS4200: space-saving solution for use in flat control cabinets with new CIM4210C central interface module
- Simple, convenient engineering and commissioning of industrial heating processes with TIA Portal
Siemens
has equipped the modular Siplus HCS heating control systems for
switching and controlling heater fields and elements with a new power output
module (POM) and a central interface module (CIM). With more power per output
and a space-saving solution for mounting in flat control cabinets, the flexible
heating control system is now even more versatile, and can be used for example
in applications with heat registers.
- Shorter development and commissioning times
- Software libraries enable standardization
- Commissioning tests on virtual test rack
The new Sinumerik One CNC generation is at the heart of digital transformation for machine tools. As a digital native, the controller features not only a new hardware platform, but also versatile software for the creation of a digital twin. It closes the gap between the virtual and the real world and helps to reduce development and commissioning times considerably.
- Compact device providing combined functionality for measurement, monitoring and data transmission
- Separate detection of energy consumption and energy recovery
- Operating hour and switching cycle counters enable preventive maintenance
- Commissioning, measured values and status information via Profinet
Siemens has just launched its SIRIUS 3UG546 DC load monitoring relay on the market. The new device is the most compact of its kind for direct current (DC) applications, enabling simple and precise power measurement. The SIRIUS 3UG546 is unique in our industry: It is the first and only DC load monitoring relay to combine current and voltage measurement, power monitoring, communication and various other useful functions in one single, compact device. Until now, several individual components were required for each of these functions. The innovative new approach saves space and costs.
- Next generation of Simatic ET
200eco PN: New functions for modern machine concepts and requirements
- For use in redundant,
high-availability systems thanks to S2 redundancy
- High current-carrying capacity with
power supply via L-coded plug
- High-quality industrial enclosure with IP65/67
protection for outdoor use
Siemens has launched a new generation of machine-level block I/O
devices in the form of the Simatic ET 200eco PN. The new I/O family with
IP65/67 degree of protection includes five digital I/O devices as well as an IO-Link master device and offers users a whole range of new
functions for modern machine concepts and requirements. In their new industrial
metal enclosure, the devices are reliably protected from UV radiation and
harmful substances even under adverse environmental conditions, making it
possible to use the devices outside of factory buildings. The devices are
supplied with power via an L-coded plug, resulting in a considerably higher
current-carrying capacity. In turn, this enables longer cable routes in the
field, and the supply and connection of more energy-intensive components (such
as valve terminals) without the need for more supply cables.
- Simatic S7-1500
firmware V2.8: Secure data integration, versatile diagnostics function for OPC
UA server
- Simatic S7-1200 firmware V4.4:
Improved cross-platform data transfer, OPC UA Data Access as server, OPC UA
Modelling Editor
Siemens announces the release of two firmware updates for
Simatic controllers that provide new functions. The Simatic S7-1500 firmware
V2.8 from Siemens improves cross-device capabilities for data integration and
diagnostics functions. The new Simatic S7-1200 firmware V4.4 extends the
communication functions of the Simatic S7-1200, enhancing cross-platform data
transfer with other controllers and higher-level or cloud-based systems such as
ERP, SCADA and Mindsphere. The applications are numerous, ranging from
industrial use to agriculture and infrastructure projects.