- Improved accuracy and repeatability
- Increased asset utilization and decreased operational waste
- Wide range of applications in environmental, chemical, and food and beverage industries
- Hart 7 communications
Siemens presents Sitrans Probe LU240, its newest ultrasonic level measurement Hart transmitter, a hardworking and rugged device that provides reliable level, volume, and flow measurements. Engineered for the challenges of the environmental industry, this transmitter is also suited for the chemical and food and beverage applications. Field-proven Process Intelligence echo processing separates true material level echoes from false, providing reliable readings while still allowing rapid response to actual changes in the material level. The device's reduced blanking distance decreases waste in applications while boosting asset utilization by providing continuously accurate readings even with high levels of material.
Aker Solutions and Siemens have signed a strategic collaboration agreement to further develop digital offerings in engineering, operations and services. The collaboration focuses on the creation of software applications and joint service offerings including the development of industrial digital twins that will drive efficiency throughout the entire plant lifecycle. In addition, the companies will further develop specific offerings for the oil and gas sector based on Siemens' Comos engineering platform. These solutions will help customers to reduce engineering and operational cost and enable improved decision making. The agreement builds on a long-standing, successful relationship between both companies by combining individual strengths and promoting joint offerings.
- Edge Devices to collect and process large data volumes directly at the machine
- Secure, future-proof basis for the execution of Industrial Edge applications
- Simple update procedure and software rollouts through secure link to central Edge Management System
- Savings through edge computing in the Siemens Electronics Factory Amberg
At the SPS IPC Drives 2018 in Nuremberg, Siemens will be showcasing a newly developed hardware platform for edge applications as part of its Siemens Industrial Edge concept: The compact Simatic Edge Device works on the basis of the embedded industrial PC Simatic IPC227E, and features integrated connectivity to automation on the machine level. This allows manufacturing data to be captured and processed directly at the point of production. If there is a change to the framework conditions underlying the industrial application, Industrial Edge offers facility to adjust software applications on the Edge Device, keeping them right up to date using functional, feedback-free updates. The hardware comes with a closed all-metal housing, ensuring maximum industrial functionality for flexible, maintenance-free use under even the harshest of conditions. Rapid commissioning is guaranteed using pre-installed Edge software.
- TÜV Süd certified process for system integration and solution project processing in conformity with IEC 62443-2-4 and -3-3
- Security documentation in conformity with IEC 62443
- Implementation of certified solutions with Simatic PCS 7
- Standardized processes reduce outlay for customers
Siemens is the world's first company to gain TÜV SÜD certification for the secure system integration of process automation and drive solutions in compliance with the international IEC 62443-2-4 standards. The integration projects, verified on the basis of two standard solutions in the oil & gas processing industry and in a waste incineration plant, have been certified in conformity with IEC 62443-2-4 and -3-3 and were implemented using the Simatic PCS 7 process control system. The projects involved process automation, drive solutions and comprehensive security measures and functions designed to deliver secure plant operation. The certification has a whole range of advantages to offer for customers: plant operators benefit from the precise definition of requirements, the implementation of standardized automation solutions and processes, and from the availability of documentation in conformance with standards. This documentation provides a vital foundation for verifying compliance with the technical requirements of the IT Security Act and other cyber security standards, for the sustainable improvement of IT and OT system security, and for guaranteeing the security of general supplies. The system solutions are used in sectors involving a critical infrastructure, such as waste management and the oil and gas industry.
- New Sinamics converter family series optimized for pump and fan infrastructure applications
- 0.75 to 630 kW power range allows operation with any motor
- Stable running under any network conditions thanks to integrated DC link reactor
- Sinamics G120X is digitalization-ready and can be linked directly to the cloud with Sinamics Connect 300
Siemens will be presenting a brand new converter series at this year's SPS IPC Drives. The converters of the new Sinamics G120X series are especially suited for use in pump and fan applications in industries such as water/wastewater, building technology or also in industrial environments. With a power range of 0.75 to 630 kW, Sinamics G120X converters can be operated with any motor. The converters are at their most effective running with synchronous reluctance motors from Siemens. Sinamics G120X are configured throughout for cost-optimized and resource-saving operation across all voltages and supply networks, and their characteristic compact design saves space in the control cabinet. Although not featuring an additional output reactor, the converters enable motor cable lengths of up to 150 meters. The integrated safety functions are certified to SIL3.
- Industrial PC for use as an IoT gateway enables data to be managed directly in the production environment
- Based on Windows or Linux, for networking machinery of different manufacturers and of different technological versions
- Fitted with up to 3 LAN interfaces for high connectivity
- Pre-configured versions available from stock
Siemens has expanded its product portfolio of Simatic industrial PCs to include the Simatic IPC127E. The newly developed industrial PC is suitable, for example, for use as a gateway and enables data to be managed directly in the production environment. Whether it is based on Windows or Linux, the Simatic IPC127E makes it possible to network existing systems with machinery of different manufacturers and different technological versions. Thanks to the compact enclosure of just 0.3 liters, it can be integrated with a minimum space requirement in the cabinet or directly at the machine.
- Smart connection panel with LAN link for cloud-based digitalization solutions
- Simple plug-and-play handling, also for use in legacy systems
- Analyze MyDrives now available on the latest MindSphere version
The new Sinamics Connect 300 from Siemens provides a simple plug-and-play solution for integrating converters of the Sinamics family into the IT world. The new solution is suitable for low-voltage converters and supports cloud-based digitalization solutions. MindSphere applications such as Analyze MyDrives can now be used directly via Sinamics Connect 300. Sinamics Connect 300 is an IoT gateway with its own dedicated LAN connection. The converter is connected directly to the Sinamics Connect 300 terminal block. Parameters, operating data and statuses are being transmitted over universal serial interface protocol and can be retrieved at any time. No modifications are necessary to the hardware or firmware of drives used with Sinamics Connect 300, nor do PLC programs need to be adjusted. Commissioning takes place conveniently and simply using a web server user interface. Sinamics Connect 300 does not bring about any changes to the data and signal flow of the machine automation, nor does it place any additional load on the field bus of the machine or plant. This makes the use of Sinamics Connect 300 completely independent of the automation and enables rapid, trouble-free and low-cost commissioning. The simultaneous connection of up to eight drives opens up outstanding economies of scale, and the Sinamics Connect 300 is also highly suited for machine users looking to directly upgrade heterogeneous legacy machine fleets in brown field projects.
- Integration of artificial intelligence and edge computing into Digital Enterprise portfolio
- Networking concepts from factory floors to corporate offices
- Growing ecosystem surrounding MindSphere
By expanding its Digital Enterprise portfolio and integrating future technologies, Siemens is driving forward the digital transformation of the discrete and process industries. "An ever-increasing number of industrial enterprises, particularly SMEs, are well on the way towards Industrie 4.0, and are already improving their competitive standing with digital solutions," explained Klaus Helmrich, Member of the Management Board of Siemens AG, at the SPS IPC Drives. "This applies to all sectors of industry with rapidly changing market demands in which products have to be manufactured ever more quickly, flexibly and in diminishing quantities. With the further integration of technologies such as artificial intelligence (AI) and edge computing into our portfolio, we're paving the way for the future of industry." Siemens will be present at the fair with an array of innovations and industry-specific applications, ranging from automation and edge devices using artificial intelligence in applications such as machine tools, production machinery and process plants through to integrated networking concepts from factory floors to corporate offices. These all help to drive forward the use of innovative automation and software solutions.
- Sipart PS100 for fast, easy commissioning
- Sipart PS2 positioner with improved diagnostics functions
- Siemens valve monitoring app with extensive control and analysis options
With the Sipart PS100, Siemens is presenting a new positioner that is impressively easy to commission and highly robust. The Sipart PS100 can be initialized quickly at the touch of a button, automatically adjusting itself to the attached valve. If required, it is possible to optimize the positioner for a specific application with just one further touch of a button. Just as some cameras feature portrait, sport or night mode, the positioner can be set to different modes for precise and fast adjustment, open/close operation and other applications. These functionalities save time, cut the costs of commissioning, and increase the return on investment.