Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release23 November 2018Process Industries and DrivesNuremberg
Siemens extends its positioner portfolio with Sipart PS100

Siemens extends its positioner portfolio with Sipart PS100
The Sipart PS100 is fitted with a large, easy-to-read display that allows users to see the status of the device at a glance. With its four-button operation and Namur NE107 support, the device can be configured quickly and conveniently.
The Sipart PS100 is available in two enclosure variants: polycarbonate and aluminum. Thanks to these particularly robust and durable materials, the new addition to the Siemens positioner portfolio is capable of withstanding extremely harsh and aggressive environments. The Sipart PS100 uses state-of-the-art contactless technology to detect the position of the valve. This eliminates wear, extending the device's service life and facilitating easier, faster commissioning. Equipped with a corrosion-resistant silencer, the Sipart PS100 is especially suited to applications in the chemical and power sectors.
The Sipart PS2, an established element of the Siemens positioner portfolio, has gained some new features. Optional pressure sensors improve the valve diagnostics and process monitoring, increasing the degree of utilization and availability of the plant. The enhanced positioner supports digitalization in plants. The Siemens valve monitoring app provides users with all the information they need to follow a predictive maintenance approach by performing cloud-based analyses of valve data. It makes extensive control and analysis options available to users so that they can detect in good time when service tasks need to be carried out before potential faults occur. In this way, the use of the valve monitoring app makes it possible to cut maintenance and operating costs.
Find out more at www.siemens.com/positioner
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2018110033PDEN
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 7-26616