- New development – Simatic PCS neo sets new standards in process automation
- Intuitive usability and a single workbench for all tasks
- Consistent object-oriented data management
- Unique, global, web-based collaboration in engineering and operation
- Scalable from small process modules up to the largest process plants in the world
Siemens sets new standards in process automation and is launching an innovative web-based process control system for all industries at the Hannover Messe. Simatic PCS neo is a brand-new system software, which offers companies in the process industry unique opportunities in the age of digitalization. Main features include global web-based collaboration in engineering and operation and intuitive handling representing all relevant information in a single workbench.
- Simatic PCS 7 Plant Automation Accelerator V3.0 plant and automation engineering software closes the gap between plant engineering and the process control system
- More powerful, more open version
- Increased system openness based on GSDML and NE150 standards
- Seamless engineering through the integration of various Simatic components
Siemens has extended its engineering software for planners and automation engineers, Simatic PCS 7 Plant Automation Accelerator 3.0 (PAA), to include new functions for even more flexible and integrated automation engineering. With this latest software version, Simatic PCS 7 automation projects can be configured even more easily and efficiently. With Version 3, the PAA software closes the gap between plant engineering and the process control system. The entire plant structure including measuring point data can be generated easily and synchronized between the systems. Automation engineers are supported in all phases from tender preparation (such as bills of material), automatically generated process control data from electrical engineering in the Siemens Simatic PCS 7 process control system (including controlled mass data engineering), to as-is documentation of the process automation.
- New firmware V5.2 for even easier operation of Sinamics S120 drive systems
- Integration of the web server with new, responsive design and no special commissioning tools for diagnostics, maintenance and servicing
- Parallel connection of Active Line Modules (ALM) provides an extended performance range for booksize versions
- Users benefit from increased rated power without additional chassis unit and energy exchange in the DC link
Siemens offers new features in the firmware and hardware for the Sinamics S120 drive system. Operation is made much easier in firmware V5.2 through the integration of the web server. The web server in version V5.2 has a new, responsive design, which reacts via standard web browsers regardless of the end device used (notebook, PC, tablet or smartphone). For commissioning typical diagnostics and maintenance functions or servicing, no special tools are required. The web pages are available in six standard languages and feature error indicators and warning messages including meaningful help texts and suggestions for possible solutions. Users can intuitively create, manage and delete parameter lists - even across axes - and can perform firmware updates and system restores with the old firmware version. Backups of parameter settings can be stored on the clients using the web server and browser, and reloaded in the Sinamics converter using the Restore function. In order to test functions that are subject to license, it is possible to activate a temporary trial mode. In addition, a complete overview of all functions that are subject to license is clearly displayed in the web server. For optimum display on any Internet-capable end device, the best browsers are Microsoft Edge, Mozilla Firefox, Google Chrome and Safari. Navigation is via menu or breadcrumbs.
- Higher performance, increased accuracy, full utilization of the stockyard area, and optimized energy consumption compared to staffed operation
- Pilot project for Jiangsu Binxin Special Steel Material Co. Ltd. is a first step towards intelligent upgrading of plants
To improve air quality in China's urban centers, part of the country's counter measures has resulted in stockyard of iron, steel and the production of other industrial activities to move to indoor facilities instead of traditional outdoor locations. To take an industry leadership role, while continuing to meet expanding market needs by increasing production capacity, the Jiangsu Binxin Special Steel Material Co. Ltd. (Binxin Steel) decided to upgrade its plant intelligence by moving to an innovative autonomous stockyard management system from Siemens. This also has the advantage of overcoming the challenge of hiring and retaining skilled workers and engineers, while simultaneously providing continuous, safe, secure, and reliable operations. This project is a first step towards upgrading of the company's plant intelligence.
- TÜV Süd certified process for system integration and solution project processing in conformity with IEC 62443-2-4 and -3-3
- Security documentation in conformity with IEC 62443
- Implementation of certified solutions with Simatic PCS 7
- Standardized processes reduce outlay for customers
Siemens is the world's first company to gain TÜV SÜD certification for the secure system integration of process automation and drive solutions in compliance with the international IEC 62443-2-4 standards. The integration projects, verified on the basis of two standard solutions in the oil & gas processing industry and in a waste incineration plant, have been certified in conformity with IEC 62443-2-4 and -3-3 and were implemented using the Simatic PCS 7 process control system. The projects involved process automation, drive solutions and comprehensive security measures and functions designed to deliver secure plant operation. The certification has a whole range of advantages to offer for customers: plant operators benefit from the precise definition of requirements, the implementation of standardized automation solutions and processes, and from the availability of documentation in conformance with standards. This documentation provides a vital foundation for verifying compliance with the technical requirements of the IT Security Act and other cyber security standards, for the sustainable improvement of IT and OT system security, and for guaranteeing the security of general supplies. The system solutions are used in sectors involving a critical infrastructure, such as waste management and the oil and gas industry.
- Collaboration on new overall system
- More flexible, more efficient production processes
Siemens and Festo are presenting an innovative linear motor drive and control concept, designed to offer flexible and efficient high-performance solutions for short-cycle applications. The Multi-Carrier-System (MCS) from Siemens and Festo has been integrated into the Rexroth TS 2plus transfer system, thus adding the modular MCS to Bosch Rexroth's versatile building-block system based on standardized units. The advantages of the existing systems have been merged, and users are free to combine them in almost any way they wish to achieve maximum flexibility in their processes. This opens up new possibilities in assembly technology or in battery production, for example.
- Multifunctional platform as a new type of device for Simatic Advanced Controllers – combines conventional control tasks with typical PC tasks
- Reusable high-level language applications are easily created with Eclipse or, model-based, with Matlab Simulink
- With just one item of hardware for less programming effort and a smaller space requirement
- The Advanced Controller portfolio has two new technology CPUs and handling functions for Motion Control tasks
Siemens has expanded its Simatic S7-1500 Advanced Controller portfolio for more challenging applications to include a new type of multifunctional platform that combines control and PC functions in a single device. Two new technology CPUs also widen the portfolio for midrange Motion Control tasks.
- Edge application Optimize MyMachining /Trochoidal allows real-time data processing for high availability and productivity
- Siemens Industrial Edge closes the gap between local and cloud computing in the industrial sector
- Sinumerik Edge facilitates high-frequency control data processing
As part of Siemens Industrial Edge, Siemens is launching applications for Sinumerik Edge, the machine-level platform specially designed for the machine tool industry, at AMB 2018 in Stuttgart. This is the first opportunity to see the Edge application Optimize MyMachining /Trochoidal for use in trochoidal milling.
- New Simatic MindApps for the open IoT operating system MindSphere
- Machine Monitor: Transparency for status and performance of machines
- Notifier: Message distributions from machines and access to alarm data
- Performance Monitor: Availability and productivity of the manufacturing facility
Siemens is launching a number of new apps concerning automation with Simatic systems. The new Simatic MindApps Machine Monitor, Notifier and Performance Monitor are special applications for MindSphere, the open IoT operating system from Siemens. These apps will enable users to make easy use of the advantages of cloud-based services and generate added value. The Simatic MindApps read out relevant data for analysis purposes, for example, from production machines or systems, then process them to create meaningful information, display them on dashboards, or use them for intelligent alerting and messaging.