Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release14 May 2019Digital IndustriesErlangen
Siemens extends software portfolio for workpiece quality to include another Sinumerik Edge application

AnalyzeMyWorkpiece /Monitor is the ideal addition to the range of applications currently available for workpiece analysis. The AnalyzeMyWorkpiece /Capture Edge application records selected data that can then be visualized using the AnalyzeMyWorkpiece /Toolpath PC application. The high-frequency data points support detailed visualization and a comprehensive analysis of the produced workpieces. This means that workpiece quality can be optimized even during production launch.
In addition to workpiece analysis applications, Siemens is also presenting other applications for machine availability and process optimization at EMO 2019. For machine availability, the Siemens AnalyzeMyMachine /Condition solution can be used to monitor critical machine parameters. To increase efficiency, Siemens offers OptimizeMyMachining /Trochoidal, a solution for trochoidal milling where NC programs can be optimized directly on the machine tool.
For information regarding Siemens Industrial Edge, please see
www.siemens.com/industrial-edge
For further information regarding Siemens at the EMO 2019, please see
www.siemens.com/press/emo2019 und www.siemens.com/emo
For this press release
Press Event
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 75,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Katharina Lamsa
Siemens AG
Gleiwitzer Str. 555
90475 Nürnberg
90475 Nürnberg
+49 (911) 895-7975