Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release01 October 2019Digital IndustriesNuremberg
Web-based visualization system sets new standards for industrial operator control and monitoring

At the "SPS– Smart Production Solutions" 2019, Siemens will present a completely new overall system for industrial operator control and monitoring. The web-based visualization system consists initially the Simatic WinCC Unified visualization software as well as the new generation of HMI panels, Simatic HMI Unified Comfort Panels.
The runtime of the newly developed visualization software Simatic WinCC Unified in the TIA (Totally Integrated Automation) Portal is based on native Web technologies such as HTML5, SVG and JavaScript. The high scalability of the newly platform enables end-to-end solutions, from machine-level applications all the way to the SCADA system.
When designing the system, Siemens focused on the overall openness. For this purpose, open API interfaces such as TIA Portal Openness were implemented which enable automated engineering, on the one hand, and considerably simplify data exchange during operation, on the other hand. For this, an ODK (Open Development Kit) and an OpenPipe interface are available to the user, as well as the option to integrate other applications into the user interface of WinCC Unified.
Engineering is consistently integrated in the TIA Portal, the engineering framework with modern programming languages and seamless data flow. Components created once can be re-used on all platforms, whether on the operator panel, on the PC or as apps in the Cloud- and Edge environment. WinCC Unified Runtime can be accessed via all modern Internet browsers without the installation of separate plug-ins. In the first version, WinCC Unified is available for Panel- and PC-based solutions. The use of WinCC Unified in the Edge- and Cloud environment will be possible in a later delivery stage.
Engineering is consistently integrated in the TIA Portal, the engineering framework with modern programming languages and seamless data flow. Components created once can be re-used on all platforms, whether on the operator panel, on the PC or as apps in the Cloud- and Edge environment. WinCC Unified Runtime can be accessed via all modern Internet browsers without the installation of separate plug-ins. In the first version, WinCC Unified is available for Panel- and PC-based solutions. The use of WinCC Unified in the Edge- and Cloud environment will be possible in a later delivery stage.
With the Simatic WinCC Unified system, Siemens will present a new generation of high-end HMI devices at the SPS 2019: The Simatic HMI Unified Comfort Panels are available in display sizes from 7 to 22 inches, have a glass front with capacitive multitouch technology, and offer users in the industrial environment a high degree of usability, similar to the operation of a smartphone or tablet. High brilliance in colors and contrast improve readability and operability. Visualization on the devices is based on Simatic WinCC Unified and brings many new possibilities to the devices: Dynamic SVG (Scalable Vector Graphics), extensive UI controls or "collaboration", a convenient mechanism for exchanging data between WinCC Unified stations.
The functional expansion possibilities through apps represent a paradigm shift in the SIMATIC HMI product portfolio. While the HMI panels were used exclusively for the visualization software in the past, Siemens now gives users the possibility with the integrated Edge functionality to also operate other apps on the devices at the same time.
The functional expansion possibilities through apps represent a paradigm shift in the SIMATIC HMI product portfolio. While the HMI panels were used exclusively for the visualization software in the past, Siemens now gives users the possibility with the integrated Edge functionality to also operate other apps on the devices at the same time.
For further information on Simatic WinCC Unified System, please see
www.siemens.com/simatic-wincc-unified
You can find additional information on Siemens at the SPS IPC Drives 2019 under
www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2019
www.siemens.com/simatic-wincc-unified
You can find additional information on Siemens at the SPS IPC Drives 2019 under
www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2019
For this press release
Social Media
Siemens Digital Industries (DI)
is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 75,000 employees internationally.
Siemens AG
(Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at
www.siemens.com
.
Contact
Andreas Friedrich
Digital Industries
Gleiwitzer Str. 555
90475 Nuernberg
90475 Nuernberg
+49 (1522) 2103967