- Siemens supports Hexr in the mass customization of additively manufactured bicycle helmets
- Digital Enterprise portfolio offers integrated software and automation solutions for additive manufacturing
- Additive Manufacturing Network – an online order-to-delivery collaboration platform for the industrial additive manufacturing community, helps streamline the AM production process
Bicycle helmets made to measure and in an
affordable framework for everyone - what was unthinkable a few years ago is now
becoming reality thanks to digitalization and additive manufacturing. The head
is simply scanned with a smartphone app and the process for the custom-made
helmet is initiated. Siemens, together with EOS, has supported this vision of
the bicycle helmet manufacturer Hexr. Siemens' Digital Enterprise portfolio
consists of software and automation solutions that optimize process steps along
the entire value chain of additive manufacturing. This holistic approach is
unique in the field of the industrialization of additive manufacturing. With
the help of end-to-end solutions, Siemens has created the digital twin of an
industrialized additive manufacturing factory, helping to optimize the design
and streamline the production processes for customized bicycle helmets even
before production begins. By combining simulation, design optimization and a
high degree of automation in production, the costs per part could be predicted
and significantly reduced, allowing Hexr to scale the scan-to-print application
to mass production.
- Protection during grid power outages and avoidance of peak loads
- Reduced power consumption by recovering braking energy
- Higher availability and low installation costs
Siemens is offering new Ultracapacitor Modules which ensure machine operation during grid power outages, avoid peak loads and recover braking energy. The UltraCap "DLC modules" are ideal for use as energy storage devices in machines, such as those used in wood, glass and plastic processing, metal forming technology, machine tools, handling and robotics.
- Integration of artificial intelligence and edge computing into Digital Enterprise portfolio
- Networking concepts from factory floors to corporate offices
- Growing ecosystem surrounding MindSphere
By expanding its Digital Enterprise portfolio and integrating future technologies, Siemens is driving forward the digital transformation of the discrete and process industries. "An ever-increasing number of industrial enterprises, particularly SMEs, are well on the way towards Industrie 4.0, and are already improving their competitive standing with digital solutions," explained Klaus Helmrich, Member of the Management Board of Siemens AG, at the SPS IPC Drives. "This applies to all sectors of industry with rapidly changing market demands in which products have to be manufactured ever more quickly, flexibly and in diminishing quantities. With the further integration of technologies such as artificial intelligence (AI) and edge computing into our portfolio, we're paving the way for the future of industry." Siemens will be present at the fair with an array of innovations and industry-specific applications, ranging from automation and edge devices using artificial intelligence in applications such as machine tools, production machinery and process plants through to integrated networking concepts from factory floors to corporate offices. These all help to drive forward the use of innovative automation and software solutions.
- Efficient and future-proof maintenance with Predictive Services for Drive Systems
- New Mindsphere Predictive Service Assistance app provides digital support for the service portfolio, while also offering transparency and streamlined ordering processes
- Predictive Services for Drive Systems for increased productivity and reduced downtimes for machines and plants
With Predictive Services for Drive Systems, Siemens presents a standardized extension to the local service agreement at this year’s SPS. This is based on the new Mindsphere Predictive Service Assistance app. It makes maintenance more efficient for Sinamics drive systems and/or Simotics motors in the low voltage range.
- This year’s trade fair slogan: Digitalization in Intralogistics – Implement now!
- Implementation of the Digital Enterprise portfolio for machine builders and operators throughout the value chain in intralogistics
- Highlights: AGVs (automatic guided vehicles), storage and retrieval machine concepts, and localization systems
From February 19 - 21, 2019, Siemens will be showcasing digitalization, automation and drive solutions for logistics processes at Logimat, the international trade fair for intralogistics solutions. Under the banner "Digitalization in Intralogistics – Implement now!" in Hall 3, Booth D11, Siemens will be demonstrating how its Digital Enterprise portfolio successfully facilitates digital transformation in intralogistics for both machine builders and operators. The focus is on automation and drive concepts for conveyor technology, storage and retrieval machines, and automatic guided vehicles (AGVs) as well as the offer for single-source, turn-key solutions and sorting solutions for post, parcel, luggage, and cargo. Businesses are therefore able to extend the digitalization process at any point along the value chain of an intralogistics system on a step-by-step basis and optimize the individual process steps, moving from the machine and system concept, through engineering and commissioning, to actual operation and service. This holistic approach from Siemens makes it the only company in the intralogistics sector which is capable of consistently mapping the actual machine builder’s and operator’s process chain in the virtual environment.
- „Infinite opportunities from infinite data“ is this year's trade fair motto
- Leveraging the full potential of data from merging the virtual and physical worlds
- "Digitalization knows no end"
- Expansion of the portfolio for edge computing in industry
Under the motto "Infinite opportunities from infinite data", Siemens is demonstrating at the "Digital Enterprise Virtual Experience" at Hannover Messe 2021 how the merging of the physical and virtual worlds enables industrial enterprises to act flexibly and sustainably, as they are facing huge challenges: The Covid 19 pandemic has changed markets and requirements almost overnight. Added to this are the growing individualization and the urgent need for more sustainability. This can only be mastered with the help of digitalization and automation. Siemens brings together the data generated in this process in a continuous cycle between the virtual and physical worlds. This enables companies to better understand and use data. Traditional silos between previously separate industrial domains are breaking down and new opportunities for sustainable and flexible production are being created. This enables employees in industrial enterprises to make appropriate decisions based on data or, for example, to react a lot faster to changes such as suddenly increased resource consumption.
- Nemo Link is the first transmission link between the two countries
- It enables transmission of 1,000 MW electricity using Siemens HVDC Plus technology
- Siemens built converter stations housing the state of the art HVDC equipment in both Herdersbrug (Belgium) and Richborough (UK)
- Official opening ceremony on December 5 in Herdersbrug with Belgian and UK dignitaries
Nemo Link® interconnector is a joint venture between the Transmission System Operators Elia (Belgium) and National Grid (UK), to exchange electricity up to 1,000 MW between the two countries, using high voltage direct current (HVDC) technology. Nemo Link connects the Belgian and the British power grid with a combination of subsea and underground cables. This new 140 kilometers (km) long HVDC interconnection increases security of supply for both countries, allowing the import and export of electricity, as well as supporting the integration of renewable energy in the grid. The European Commission designated it a Project of Common Interest as it contributes to an integrated European energy market.
Digitalization is changing our world – and the world of industry – in tangible ways. The digital transformation is creating new competitive advantages and business models in many companies in the manufacturing and process industry. Machine builders and plant engineers can also take advantage of this development and make it usable for their customers. For digital enterprises systems and processes can be comprehensively and uniformly optimized throughout the entire lifecycle of products and plants. At the SPS IPC Drives in Nuremberg, Germany, from November 28 to 30, 2017 – which took place this year under the motto "Discover the value of the Digital Enterprise" – Siemens presented in hall 11 specific examples of applications to show how this can be done.
- Integration of cutting-edge technologies into the Digital Enterprise portfolio enables flexible and intelligent production
With its Digital Enterprise, Siemens is taking the next step of the digital transformation – on the way to highly flexible modular production. Siemens presents numerous innovations for the discrete and process industries as well as for energy and building infrastructure. The integration of cutting-edge technologies such as edge and cloud computing, artificial intelligence or additive manufacturing into the portfolio offers users new opportunities to achieve more flexible and intelligent production. Communicative networking through Industrial 5G plays a key role.
- New drive system comprising Sinamics S210 and Simotics S-1FK2 motors
- High dynamic performance and precision plus simple One Cable Connection (OCC)
- Integrated safety functions, rapid engineering and commissioning
- Servo drive system in five power classes from 50 to 750 watts
With its Sinamics S210 converter designed specifically for use with the newly developed Simotics S-1FK2 motors, Siemens is offering a new servo drive system in five power classes ranging from 50 to 750 watts. The converters come with integrated safety functions and enable rapid engineering. They are connected to the higher-level controller over Profinet and allow simple commissioning using a web server and one-button tuning. Working in combination with the Simotics servo motors, they enable the highly dynamic movement of minimal loads as well as ultra-precise movement of medium and high loads. The motors are connected to the converters using a One Cable Connection (OCC). Typical uses for the new drive system include in particular packaging machines, handling applications such as Pick & Place, wood and ceramic processing as well as digital printing.