- Sinamics G120 converter series in new frame size FSG
- Extended push-through heat sink variants for Power Module PM240-2
- Intelligent Operator Panel IOP-2 for Sinamics G series with added functions
Siemens is extending its portfolio of Sinamics G120 converters to include a new frame size, the FSG with voltage ranges from 380 to 480 volts (V) and from 500 to 690 V. This addition means that the innovative PM240-2 Power Modules now cover the entire power range up to 250 kilowatts (kW). The extremely compact design and standard integrated optional features such as integrated DC link reactor or integrated filter to achieve category C2, enable substantial space and cost savings in the control cabinet. The new frame size also allows cable lengths of up to 450 meters to be achieved without the need for additional options. Depending on the application, the Power Module can be configured individually to customer requirements using the correct control unit and matching components.
San Francisco is considered an especially environmentally friendly city. The urban environment is characterized by an extensive public transport system. In September 2014, San Francisco's Municipal Transportation Agency (SFMTA) has awarded Siemens a contract to deliver an initial 175 light rail cars at a value of USD648 million. The order included an option for additional 85 cars. One year later, SFMTA exercised its option for another 40 light rail vehicles for the public mass transit network. This is one of the biggest orders for light rail cars ever placed in the USA. The trains are being built in the Siemens plant in Sacramento. Today, every third tram or light rail vehicle in the USA is made by Siemens.
- Real-time transmission over Profinet and Pulse Train
- Absolute single-turn encoder with resolution of up to 21 bits for greater efficiency
- New motor design for better connectivity
The user-friendly servo drive system Sinamics V90 from Siemens is particularly suited as a solution for highly dynamic applications. The system comes not only in the form of a high-inertia variant with 400 volts (V) for applications requiring smooth operation, but also as a 200 V version with low inertia motors where highly dynamic performance is called for. Fitted with either Pulse Train (PTI) or Profinet, the motion/process data and diagnostic data can be transmitted in real time between Sinamics V90 and Simatic PLCs. The low inertia motor now features an additional absolute single-turn encoder with a resolution of up to 21 bits, allowing it to determine unequivocal position values and so ensure the great positioning accuracy in the applications.
Siemens has developed new base holders for Neozed fuses in one-pole and three-pole designs and sizes D01 and D02. Made of heat-resistant plastic, the new bases replace the existing Siemens devices. Eight new variants for 16 A and 63 A rated currents were developed. The compact devices are especially safe to use and, thanks to new terminals, can be easily mounted in distribution boards. For the first time, the devices are available with LED indicators that clearly show whether the fuse has been tripped due to an overload or short circuit and must be replaced.
- Siemens demonstrates consistency of the digital twin using Easysnap application at the SPS IPC Drives 2017
- "Digital Enterprise Suite" features tools for creation of the digital twin
- Apps facilitate the use of plant data collected in MindSphere
At the SPS IPC Drives 2017, Siemens will be demonstrating the consistency of the digital twin over the entire machine life cycle using the example of a packaging machine manufactured by machine builder Easysnap. To achieve this degree of consistency, all the engineering tools required for design, configuration and commissioning interact seamlessly with each other to enable truly integrated engineering. Siemens supplies a comprehensive range of different tools embedded in its "Digital Enterprise Suite" solution portfolio which are designed to enable the creation of a digital twin and so bring about substantial improvements along the value chain. The digital twin can be created using tools such as the Mechatronics Concept Designer, which enables kinematic simulations, and the Sizer configuration tool which uses this data as the basis for determining the required electrical drive values and relevant products.
Siemens AG and Software AG announced a partnership to strengthen the presence of the cloud-based open Internet of Things (IoT) operating system MindSphere across industries. MindSphere supports industrial companies in their digital transformation and offers a development platform to a broad customer base where companies can integrate their own applications and services to promote IoT innovations. Software AG brings the highly scalable components of its Digital Business Platform to MindSphere, which help customers to flexibly manage networks of millions of end devices.
- Simotics SD Add low-voltage motors reduce drain on the grid due to low start-up currents
- Compliance with sector-specific specifications in the process industries
- Global certificates for worldwide usage
- Reduced acquisition costs coupled with extended service life
With the introduction of its new Simotics SD Add low-voltage motors, Siemens is extending the application scope of the next-generation Simotics SD low-voltage motor series it launched at the beginning of this year. This marks another step taken by the company towards the expansion of its portfolio of scalable standard motors for use in challenging ambient conditions. By offering low start-up current levels, the characteristic product feature of the Simotics SD Add low-voltage motors, this new addition to the series is opening up greater application scope: for instance, to comply with sector-specific requirements in the process industries, or in fields requiring enhanced grid stability by reducing grid loads in the event of voltage dips. The availability of country-specific certificates means that these motors can be used without restrictions in all regions and markets of importance around the world.
- Refurbishment of existing 172-strong Class 444 and Class 450 Desiro fleet
- Order volume worth more than €56 million
Siemens has received an order to upgrade the fleet of the british train operating company South Western Railway (SWR). Siemens will refurbish the existing 172-strong Class 444 and Class 450 Desiro fleet of trains, which currently operate across the SWR network. The contract is worth more than €56 million.
- New, all-round IP65-protected Panel and Panel PC for machine-related, cabinet-free visualization and automation
- Simatic HMI TP1200 Comfort Panel PRO and Simatic IPC477E PRO Panel PC: high performance and functionality, many interfaces
- Used in high-end applications and for high-performance visualization tasks
- Extended individual operation through extension units: standard components for tailor-made system solutions
Siemens has extended its system family based on IP65-protected HMI (Human Machine Interface) devices for machine-related, cabinet-free visualization and automation. The Simatic HMI TP1200 Comfort Panel PRO (PROtected) with 12-inch display diagonal and the Simatic IPC477E PRO industrial Panel PC with 15, 19 and 22-inch displays are characterized by high performance and functionality as well as a large number of integrated interfaces. The new operator control and monitoring devices are especially suitable for high-end applications and powerful visualization tasks. Flexible mounting types allow the user easy operation of the machine and an optimal view of the visualization and process.
- IoT concept for Simotics motors
- Monitoring the operating condition of motors
- Connection to MindSphere open IoT operating system
- Maximum transparency and increased productivity due to intelligent evaluation: Data analysis by Simotics IQ
With Simotics IQ, the new IoT concept for motors from Siemens, the new Simotics SD low-voltage motors are fitted with a compact sensor box which captures important operating and condition parameters and transmits them by WiFi to the cloud. These operating data can then be stored and analyzed by the Simotics IQ MindApp on MindSphere. The Simotics IQ MindApp provides the user with technical motor data and valuable analytical results on the operation and condition of the motor and proposes, for example, recommended actions for preventive maintenance. This newly acquired operating data transparency allows further increases in productivity to be achieved.