Arja Talakar has been appointed CEO of Siemens Oil & Gas, effective April 1, 2019. He will be based in Houston, Texas, the global headquarters for Oil & Gas and its parent operating company, Siemens Gas and Power.
Siemens has developed a comprehensive concept for energy systems worldwide – the first such concept that takes into account and brings together not only technology but also the areas of regulation and social engagement. The Energy Value Charter aims to create customized solutions that will empower countries to make their energy systems fit for the future. The concept encompasses suggestions for implementing sustainable power-generation technologies, together with recommendations on how legal frameworks must be adapted to ensure that the full potential of these technologies can be tapped. In addition, the concept specifies options for promoting social engagement, such as work-study programs, as well as for refinancing infrastructure while simultaneously reducing greenhouse gas emissions. Siemens presented the concept at the 2019 Energy Transition Dialogue in Berlin, in the presence of energy ministers from a range of countries.
Siemens developed the concept to create a global framework for energy solutions for its businesses. With its Energy Value Charter, the company wants to enter into a dialogue with governments in order to shape energy systems in such a way that they provide the basis for economic growth, social engagement and sustainable development.
Mariel von Schumann (47), Chief of Staff and head of Governance & Markets at Siemens AG, will leave the company at the end of June 2019, following the successful implementation of the company's new structure as part of the Vision 2020+ strategy program.
- Siemens will supply three Dresser-Rand® 5HHE-VL-3NL reciprocating compressors for what will become the largest hydrogen production unit in the United States.
A leading industrial gas company recently selected Siemens to supply three Dresser-Rand® 5HHE-VL-NL reciprocating compressors for a new, state-of-the-art steam methane reformer (SMR) in Texas. The SMR will provide high-purity hydrogen for the gas company’s customers throughout the region.
- New rail-mounted devices added to Gamma instabus product line
- New switch actuators with load current detection, new switching/dimming actuators and new sun protection actuators
- Powerful and universal applications across all devices, short installation times, low maintenance costs
Siemens Smart Infrastructure is expanding its Gamma instabus KNX-based product line with new switch actuators with load current detection, new switching/dimming actuators and new sun protection actuators. The new actuators are designed for residential and commercial buildings and provide reliable switching and monitoring of loads, switching and dimming of fluorescent lamps via 1 to 10 Volt control outputs, and control of alternating current motors for sunshades and ventilation valves.
- Modern signaling and interlocking systems
- Increases operational capacity and reduces delays
Siemens Mobility and the Passenger Rail Agency of South Africa (PRASA) have successfully installed and operationalized a new signaling system in Johannesburg Park Station, Braamfontein and Pretoria station. To date, new interlocking systems have been installed in 40 of the 92 stations in South Africa's Gauteng province as part of PRASA's drive to deliver a world class commuter railway. Gauteng is the country's most populated province, home to three of the five largest cities in the country. The new system will increase operational capacity, allow the system more flexibility and reduce delays, improving overall operations for the transit system.
- Siemens' broad energy portfolio and services will help ensure long-term reliability and efficient operations
- Integrated, redundant plant design features two SGT-600 gas turbines with DLE technology running on residue gas with high concentrations of hydrogen
- Project highlights the integrated value of Siemens Gas and Power
Braskem, the largest petrochemical company in Latin America, recently entered into an agreement with Siemens to modernize a cogeneration power and steam plant at its Petrochemical Complex in Sao Paulo, Brazil. Completion of the project is expected in early 2021.
- Safer and more efficient: Catania Airport is updated with integrated building automation by Siemens
- More reliable and accurate fire detection using Sinteso connected to the Desigo CC building management software
- Cloud-based Navigator software to optimize energy consumption
With almost ten million passengers in 2018, Catania Airport is continuing to grow, solidifying its number one position in southern Italy. This makes the hub an increasingly important strategic part of the Mediterranean aviation network. As a result, however, it faces greater security and energy efficiency challenges. This is the context in which the Sicilian airport made the decision to entrust Siemens with its integrated building automation project, intended to increase security levels and monitor overall energy consumption at the hub.
Bombardier Transportation, a subcontractor for the ICE 4 project, has determined within the framework of its quality management that individual welds on ICE 4 railcar bodies were not carried out as prescribed. This deviation is not safety relevant.
- Stimulating two senses through acoustic (EN 54-3) and optical (EN 54-23) alarm devices
- Voice messages can be emitted in two languages for faster evacuation
- High alarming reliability thanks to daily disturbance-free tests
Siemens Smart Infrastructure has launched new ceiling- and wall-mounted alarm devices. The expanded portfolio includes both acoustic and optical alarm devices in accordance with European Standards EN 54-3 / EN 54-23 and EN 54-17. One highlight of the expanded portfolio are the voice sounders with built-in voice messages because they improve the reaction time to alarms.