-
90 new trains in size XXL
- For the first time, all cars are completely integrated and set new standards
with a train length of over 200 meters
- Financing guaranteed by
the State of Bavaria
Passengers on Munich’s S-Bahn can soon look
forward to traveling on the most modern S-Bahn trains in Germany. Siemens
Mobility will deliver 90 superlative new S-Bahn trains worth more than two
billion euros after winning an EU-wide tender. The contract includes an option
for additional trains. Financing for the trains is guaranteed by the State of
Bavaria through a leasing model.
- Monitoring of all 3-phase grids from 200 V to 690 V nominal voltage
- Frequency monitoring from 15-70 Hz for more detailed information
- IO-Link enables transmission and evaluation of measured values in the
controller or higher-level systems
- Certification according to SIL 1 (IEC 62061) and PL c (EN ISO 13849-1)
standards for a wide range of applications
Siemens has launched a new generation of line monitoring relays. The SIRIUS 3UG5 line monitoring relays combine proven technology with new functions and applications. The relays are the easiest way to monitor standards-compliant grid stability and quality, ensuring proper system operation and a long service life of components such as motors or compressors. Grid monitoring relays are used in critical areas such as hospitals or the process industry, which require a high-quality, fail-safe supply of power. Other areas of application include cranes, elevators, air, and air-conditioning compressors, as well as the timber industry.
Siemens Mobility and
Deutsche Bahn have jointly launched a groundbreaking project that takes public
transportation in Munich to a new level. As part of this pioneering
collaboration, modern S-Bahn trains have been developed to provide passengers
with an even more pleasant and efficient travel experience. The new S-Bahn
trains not only promise increased capacity but also set new standards in terms
of comfort, sustainability, and technology.
- 15 additional Vectron AC and Vectron MS
locomotives
- Delivery includes locomotives with a top speed
of 200 km/h
- Milestone reached: 100 Vectrons ordered by
Akiem since 2021
Akiem, a leading European
rolling stock leasing company, has ordered an additional 15 Vectron AC and
Vectron MS locomotives from Siemens Mobility. The order was placed as part of a
framework agreement for the purchase of locomotives that was signed in December
2021. Locomotives from this new call will be delivered between 2025 and 2027.
Akiem previously ordered 20 Vectron locomotives from Siemens Mobility in December
2021 and an additional 65 units last August.
- In a pilot project, Siemens is combining its Sigreen emissions management software with BayWa Carbon Connect, BayWa’s software for emissions offsetting
- The real carbon footprint of products is made transparent across the supply chain, from emission generation and reduction to offsetting
- In an initial use case, Siemens is offsetting the carbon emissions of selected products of the Simatic S7-1500 family at the Electronics Works Amberg for the duration of the project
The technology company Siemens and BayWa AG are working together to advance CO2-optimized industrial production. As part of a pilot project, the two companies are combining Sigreen, Siemens’ software for emissions management, with BayWa Carbon Connect, BayWa’s software for emissions offsetting.
- Delivery of 15 Vectron MS locomotives
- MSC subsidiary MEDWAY Belgium NV will take
delivery of equipment and is a new customer of Siemens Mobility
- Locomotives can operate in 12 European
countries
Siemens
Mobility has received an order from MSC subsidiary MEDWAY Belgium NV for 15 Vectron
MS locomotives. MEDWAY plans to use the locomotives for cross-border freight
transport in Europe and also for supplementing container transport by ship in
serving the eastern hinterland of Antwerp.
- Industrial Connectivity Lab opens at the Erlangen site
- Test environment for industrial connectivity technologies
- 5G, WLAN, RTLS, and RFID: Users test application scenarios and interoperability in industrial conditions
The technology company Siemens has opened a new test laboratory for industrial connectivity technologies at its Erlangen site. Embedded in the Siemens Technology Center on the Erlangen campus, the Industrial Connectivity Lab offers 300 square meters of space for extensive testing of any connectivity solution in industrial environments: Industrial WLAN, 5G, real-time localization systems (RTLS), and radio frequency identification (RFID).
City of Hamburg, Deutsche Bahn, and Siemens
Mobility sign cooperation agreement for Digitale S-Bahn Hamburg 2.0
New
intelligent operations control system to be tested until UITP Congress 2025
Partners jointly invest 35 million euros
(Hamburg, July 18,
2023) With the Digitale S-Bahn Hamburg, train travel will become even more
environmentally friendly in the future. Deutsche Bahn (DB), the city of
Hamburg, and Siemens Mobility are introducing a new intelligent operations
control system for the Digitale S-Bahn in Hamburg, aiming to reduce the trains'
power consumption by up to 30 percent. The system will be tested until the UITP
World Congress 2025. The project, costing 35 million euros, is jointly funded
by DB, the city of Hamburg, and Siemens Mobility. A cooperation agreement for
the Digitale S-Bahn Hamburg 2.0 was signed by representatives of the partners
today.
- Siemens to donate EUR 500,000 to foundation for mountain rescue services
- Funds to further develop globally unique Bavarian Mountain Rescue Service's center for Safety and Training in Bad Tölz
- Half of donations from Siemens employees
Siemens and
the charitable association Siemens Caring Hands e.V. are supporting the Stiftung
Bergwacht, a non-profit foundation for mountain rescue services, with a
donation of €500,000. The foundation will use the donation to further develop
the Bavarian Mountain Rescue Service’s Center for Safety and Training in Bad
Tölz, Germany, and thus improve disaster prevention in Germany and Europe. Half
the donation is from Siemens employees and half from Siemens AG. The funds are part
of a donation pool that Siemens set up in 2021 in response to the flood
disaster on the Ahr River in the German states of Rhineland-Palatinate, North
Rhine-Westphalia and Bavaria. Over the past two years, €2.8 million from the
pool has been used to support 25 emergency, reconstruction and prevention
projects.
- Innovative Sentron 3WA circuit breaker series part of Siemens Xcelerator
- Designed to improve ease of use, reliability, and digitalization when integrating into existing systems
- Essential for critical infrastructure, such as hospitals or data centers
- 3WA1 (IEC), 3WA2 (UL489), and 3WA3 (UL1066+IEC) offer worldwide compatibility
Siemens has launched two new additional
versions of its innovative Sentron 3WA Power Circuit Breakers, alternatively
known as Air Circuit Breakers (ACBs). Series 3WA3 meets the requirements of UL
1066 and IEC 60947-2 standards, which enables customers to use it worldwide.
This is particularly advantageous for switchgear manufacturers and OEMs producing
systems for both standardization areas – IEC and UL. The 3WA2 series is
designed exclusively for the UL 489 market. The two new ACB model series
complement the 3WA1 version for IEC markets, which has been launched in the
fall of 2020. Siemens offers a full range of ACBs which are based on a
consistent system and offer great flexibility for applications around the
globe. The Sentron 3WA Power Circuit Breakers are part of the Siemens
Xcelerator portfolio. Siemens Xcelerator is an open digital business platform
that enables customers to accelerate their digital transformation easier,
faster, and at scale.