Siemens Mobility's Vectron locomotives are used for both freight and passenger service. During the development of the locomotive, the focus was on providing a future-proof design, investment security, environmental compatibility, fungibility, retrofitting capability and convertibility. The Vectron can be delivered as a purely electrical version for operating with alternating current (AC) or direct current (DC) power systems as well as a multisystem (MS) variant in the power classes 5.2 MW, 5.6 MW and 6.4 MW. Along with the desired national train control system, the locomotives can also be equipped with the latest European Train Control System (ETCS). The locomotives are built in the Siemens Mobility plant in Munich-Allach, Germany. For freight transport in Germany, Siemens Mobility also offers the Smartron standard locomotive and the Vectron Dual Mode, a combination of diesel and electric locomotive.
- RDG200 thermostat now equipped with a built-in CO2 sensor for monitoring and controlling indoor air quality
- Helps provide a healthy indoor climate and a safe place to work
- Achieves high energy efficiency and reduced energy costs
Siemens Smart Infrastructure’s RDG200 thermostat series now offers a model that is
natively equipped with a CO2
sensor and control functions. They allow the indoor air quality to be monitored
and adjusted to ensure a healthy and productive indoor air climate at all times
for people in the building, while maintaining efficient operation. When the air
quality deteriorates because the CO2 concentration rises, the ventilation system
is automatically adjusted and ensures that the right amount of fresh air is
provided to the space.
- California-based Esri, pioneer in geographic information system software
- Geodata combined with Siemens´ modeling and simulation software boosts creation of holistic digital twin of the grid for planning, simulation and real-time operations to accelerate the energy transition
- Complementary product partners are part of the Siemens Xcelerator ever-growing ecosystem of partners to accelerate digital transformation
Siemens Smart Infrastructure has partnered with Esri, the global leader
in geographic information systems (GIS) and location intelligence, to expand
its ecosystem of partners for its grid software business. The partnership
enhances capabilities for the planning, operations and maintenance of power
networks at grid operators by combining Esri’s powerful mapping and spatial
analytics software and Siemens’ electrical topology expertise. In doing so, the
companies aim to upgrade the data flow between applications for increased
planning accuracy and for better operations of the distribution grid. The
partnership´s objective is to improve the admission of Distributed Energy
Resources (DER) to the grid so that net zero can be achieved faster.
- New innovation hub for research at Siemens in Garching, Germany
- Joint research facility with Technical University of Munich in Garching’s “Isar Valley”
- Modern and open work environments in a digitally planned, sustainable building
Just nine months after construction began, a
topping-out ceremony is being celebrated for the new Siemens Technology Center
at the research campus in the university town of Garching, Germany, near
Munich. As a result, this new building – which was planned digitally and is
being built to meet stringent sustainability requirements – has thus now
reached an important milestone on the journey to Siemens’ future research activities in the
Munich area. With its modern work environments, this facility will serve as an
innovation hub that provides space for inspiration and new ideas. At this center,
more than 450 researchers from Siemens’ “Technology” unit will collaborate on
technologies of the future with around 150 employees and students from the
Technical University of Munich (TUM).
Siemens Mobility GmbH achieved the ISO 27001 certification on July 1, 2022. The ISO 27001 certification encompasses 20 Siemens Mobility locations in Germany with more than 9,000 employees and involves Siemens Mobility Business Units, such as Rolling Stock, Rail Infrastructure, Turnkey Systems and Customer Services and all disciplines, including procurement, development, production and project management. ISO 27001 is an internationally acknowledged standard specifying cybersecurity requirements that organizations must fulfill and to which they must adapt. Increasing digitalization brings benefits – as well as the need for adequate protection against cyberattacks. Rail operators face new cyber threats and cyber laws are giving rise to new requirements. Siemens Mobility offers secured products and solutions that are integrated into one holistic security architecture and provide security services. With these, Siemens Mobility secures rail systems from end to end throughout the complete lifecycle. The ISO 27001 certification is another building block in the protection of the entire development and production lifecycle for mobility systems. The ISO 27001 certification is a milestone for Siemens Mobility on the way to digitising the rail industry.
- First order for multisystem locomotives with XLoad equipment package
- XLoad enables significantly higher trailer loads
- Contract includes locomotives and their maintenance
Switzerland’s SBB Cargo International AG, in cooperation with SüdLeasing GmbH, has ordered 20 Vectron multisystem locomotives equipped with the XLoad package from Siemens Mobility. SBB Cargo International will lease the locomotives from SüdLeasing under a long-term rental plan with a flexible term. The contract also includes maintenance of the locomotives by Siemens Mobility. Vectron XLoad is an equipment package developed to improve traction performance and increase trailer loads. With this XLoad option, for example, operators on the North-South Corridor will be able to use only one rather than two four-axle locomotives for a train. The Vectrons are designed for a maximum operating speed of 160 km/h. The locomotives will be delivered beginning in 2024.
- Frame sizes 1,200 A, 1,600 A and 2,000 A
- Enhanced safety features
- Fully integrated communication and measurement features
- Smart features for planning and operation
Siemens has developed new, highly flexible
molded case circuit breaker (MCCB) frame sizes for high current applications to
perfectly address the needs of switchgear manufacturers and panel builders in
an environment, characterized by increasing complexity, digitalization, and
cost pressures. The new 3VA UL Large Frame MCCBs enable users to implement
powerful, safe, and smart systems while allowing them to improve and greatly
simplify their work processes. These 3VA UL Large Frame
MCCBs can be used worldwide. The 1,200 A and 1,600 A frame sizes meet the
requirements of IEC and UL standards. This is particularly advantageous for
manufacturers who are producing systems destined for global markets. The new 2,000
A frame is designed exclusively for the UL market. The new frame sizes will be available
in both thermal-magnetic and electronic trip unit versions. Molded case switch (MCS)
variants will also be offered.
- Siemens completes sale of mail and
parcel business to Körber
- Further step in simplifying Siemens’
portfolio achieved
The sale of
Siemens Logistics’ mail and parcel business to the Körber Group closed
successfully on July 1. In February 2022, Siemens had announced the
contract signing for the sale of the mail and parcel business to the Körber
Group for €1.15 billion (enterprise value).
Magdeburg/Brandenburg an der Havel, June 30, 2022
– Today Ostdeutsche Eisenbahn
GmbH (ODEG), together with representatives from the states of Mecklenburg-Western
Pomerania, Berlin, Brandenburg and Saxony-Anhalt and the transport authorities VBB-Verkehrsverbund Berlin-Brandenburg GmbH,
Nahverkehrsservice Sachsen-Anhalt GmbH, and Verkehrsgesellschaft
Mecklenburg-Vorpommern mbH, signed the transport contract for the Elbe-Spree
network in Brandenburg an der Havel. As part of the ceremony, one of
the new six-car Desiro HC trains was presented in Magdeburg and Brandenburg an
der Havel by train manufacturer Siemens Mobility GmbH.
- Atlantia S.p.A. finalizes the
acquisition of Yunex Traffic from Siemens Mobility for €950 million
Siemens Mobility has successfully
completed the sale of Yunex Traffic to Atlantia S.p.A. for €950 million. In
January 2022, Siemens had announced the contract signing to sell the Intelligent Road Infrastructure and Traffic Solutions
Business to Atlantia S.p.A. Following the required
approvals by the relevant authorities, the transaction has closed as of
June 30, 2022.