- Increased power density and user-friendliness through easy handling
- Plug and play installation and rapid replacement of individual modules
- Increase in redundancy and degradation rates for fuel cell plants
Building on the success of the previous BZM34 and BZM120 fuel cell modules, Siemens aims to optimize the power density and user-friendliness of fuel cell plants on board of air-independent underwater vehicles with its new BZM evo fuel cell module. A single BZM evo has a nominal power of 40 kW. Future plants will be able to provide a maximum power of 320 – 480 kW, depending on the selected type of installation and number of fuel cell modules, without exceeding the footprint of an existing BZM34 or BZM120 plant.
- Siemens Mobility and Bytemark to provide new technology
- Will expand Smart Columbus operating system
- Public sector will manage passenger relationship for trip planning and ticket purchasing
- Enhanced passenger experience
Siemens Mobility announced it will work with Bytemark, a Siemens Mobility partially-owned subsidiary, to provide a common payment solution for Columbus, Ohio's Smart Columbus travel app – the first-ever platform managed by a city, rather than a transportation operator or private party in the United States. The single-payment system that allows for both public and private mobility services to be paid using a single account-based payment system.
As urban populations continue to grow, the need to provide
reliable and efficient transportation that allows passengers to connect
seamlessly door-to-door becomes more critical. From public transportation to
ride-sharing, bike-sharing and scooter-sharing, passengers are increasingly
looking for options that allow them to select their transportation options on
demand, planning and paying for their commutes in one easy-to-use application.
Together, Siemens Mobility, HaCon, eos.uptrade, Bytemark and Padam are
providing these digital solutions that are making commutes easier and faster.
- Brownfield Engine Exchange (BEX) delivers cleaner energy, long-term reliability, improved efficiency and more powerful performance
- Making Energy Greener is one of Siemens’ continuing core focus areas as the global energy landscape evolves and changes
- Over 30 engine exchange projects worldwide to date with several recent new orders
Siemens Gas and Power is focused on helping customers navigate the world’s most pressing energy problems, both for today and tomorrow. Essential applications include providing products, solutions and services that make fossil energy greener. A recent example is a project in Alabama where Siemens is has completed its first large gas turbine section exchange in the U.S. - delivering on that commitment. In this way Siemens is helping make energy greener and more sustainable in an evolving energy landscape.
Under the banner "Innovate. Digitalize now. SmartMining." Siemens is presenting the implementation of digital mining at this year's bauma, the world's leading trade fair for construction machinery. From April 8 to 14, the company will be demonstrating at Messe München in Hall C2, Booth 325, how mining companies can ensure and increase the availability and productivity of their mining equipment with the help of a unique range of services, comprehensive support and many years of technology and industry expertise. The digital solutions range from individual aspects to the entire mining operation.
We released our third quarter results for fiscal year 2019 on August 1, 2019. The Conference Call for journalists and the Analyst Call were broadcast live.
- Contract of Chief Human Resources Officer Janina Kugel to expire by mutual agreement
At its meeting today, the Supervisory Board of Siemens AG
agreed to extend the appointment of Managing Board member Cedrik Neike (46) by
five years. The contract of the CEO of Siemens' Smart Infrastructure Operating
Company (SI) will now run until May 31, 2025. The contract of Chief Human
Resources Officer (CHRO) Janina Kugel (49) will expire by mutual agreement on
January 31, 2020.
- Oregon’s largest regional transit provider
- S700 light rail vehicle will replace city’s Type 1
fleet
- Digitalization increases vehicles’ value sustainably
over their lifecycle
- Contract includes options for up to 60 additional
vehicles
Siemens Mobility won the latest Light Rail Vehicle
(LRV) contract from Portland's TriMet, Oregon's largest regional transit
provider. This order will replace TriMet's original 26 Type-1 vehicles, from
another manufacturer, with Siemens Mobility's new S700, a low-floor
state-of-the-art vehicle jointly developed by TriMet and Siemens Mobility. The
contract includes options for up to 60 additional LRVs, which would accommodate
additional vehicles needed for further service expansions such as the MAX Red Line
Extension to Fair Complex, and the Southwest Corridor. With the completion of this new purchase, TriMet's
LRV fleet will be a fully Siemens Mobility fleet - with the first delivery
expected in 2021.