- Pakistan’s K-Electric awarded Siemens and China’s Harbin Electric International a contract to build a 900-megawatt combined cycle power plant at the Bin Qasim Power Complex in Karachi
- Siemens to supply two F-class gas turbines, steam turbines, generators and condensers
Siemens along with partner Harbin Electric International, signed an agreement with K-Electric to build a 900-megawatt combined cycle power plant at the Bin Qasim Power Complex in Karachi.
- Siemens further expands its digitalization portfolio for industry
- Technology basis is the Docker IT standard
- Siemens Industrial Edge ecosystem enables easy and flexible use of Edge apps
Siemens is planning the acquisition of Edge technology from the US company Pixeom. With this action, Siemens is strengthening its Industrial Edge portfolio by adding software components for Edge runtime and for device management. Siemens Industrial Edge provides an ecosystem, which enables the flexible provision and use of apps. This means for example that appropriate apps can analyze data locally at the machine and send relevant data to the higher-level Industrial Edge Management System for global analytics. With this acquisition, Siemens is driving forward the expansion of its Digital Enterprise portfolio and the integration of cutting-edge technologies for the digital transformation of industry.
- Sydney Coordinated Adaptive Traffic System (SCATS) Certification
- Supports cutting-edge intelligent infrastructure
- Certificate given at ITS World Congress
Siemens Mobility’ traffic light controller “Sitraffic sX” is certified as compatible with the urban traffic control system SCATS (a registered trademark Sydney Coordinated Adaptive Traffic System). New South Wales’ agency for road infrastructure and owner of the registered trademark SCATS system, Road and Maritime Services (RMS), has granted Siemens the certification after a substantial period of integration development and testing. The Compatibility Certificate confirms that Siemens Mobility’s “Sitraffic sX” traffic light controller has been tested and evaluated by RMS to functionally operate with SCATS. The official hand-over of the Certificate from RMS to Siemens Mobility took place during a ceremony at the 26th ITS World Congress 2019 in Singapore at Siemens Mobility booth.
With growing populations, cities are becoming increasingly congested, with more traffic and longer commutes. Efficiency and safety of road traffic remain top priority for many cities. By offering autonomous shuttle systems, public transport operators and cities seek to draw passengers and make public transport more attractive. At the ITS World Congress in Singapore, Siemens Mobility is examining how Singapore is transforming its transportation ecosystem, delivering an outlook on intelligent traffic systems (ITS) projects within the Asia-Pacific region as well as showcasing advances in autonomous mobility coming to life at the CETRAN test facility.
- Shared Autonomous Mobility solutions being piloted at CETRAN
- Mobility Operating Systems for Urban Centers
- Artificial Intelligence (AI) for traffic scenarios
Siemens Mobility is showcasing the latest in intelligent traffic systems technology at this year’s ITS World Congress taking place in Singapore. This includes mobility operating systems that are helping reduce gridlock on urban streets, which centralize and control traffic throughout urban areas. By connecting road users to road and infrastructure data captured via smart structures, drivers can optimize their routes and reduce their environmental impact. Through data analysis and prediction, traffic can be regulated in an efficient manner.
- Eight desalination plants with process automation, drive technology, process instrumentation and communication technology
- Total capacity of 240,000 cubic meters per day
- Order volume is a double-digit million Euro figure
Siemens has received a follow-up order from the A3C consortium (Rawafid Industrial, Advanced Water Technology, SETE and Al Fatah) to equip eight seawater desalination plants in Saudi Arabia with electrical equipment. The new plants for seawater desalination using the principle of reverse osmosis are spread along the West coast of Saudi Arabia. The total capacity of the plants will be 240,000 cubic meters per day, with a power consumption of just three kilowatts per cubic meter of produced water, which is below the usual value and will provide significant energy savings. The scope of supply from Siemens includes hardware and software engineering, power distribution, PCS7 automation, medium and low voltage converters, Industrial Ethernet communication technology and process instrumentation for eight reverse osmosis plants, plus plant commissioning. The project will follow a tight schedule, with commissioning planned from autumn 2019.
- 25 multisystem Vectron MS locomotives for maximum flexibility
- Cross-border operations on the North-South Corridor
- Deliveries begin at the end of 2020
The Swiss rail freight company BLS Cargo has ordered 25 Vectron MS locomotives from Siemens Mobility for planned operation on the North-South Corridor. They will be used in Germany, Austria, Switzerland, Italy, the Netherlands and Belgium. Delivery of the locomotives will be carried out in several phases from the end of 2020 to 2025. With this order, the Vectron fleet operated by BLS Cargo will grow to a total of 40 locomotives. The company previously ordered 15 locomotives from Siemens Mobility in 2015.
- Portfolio serving entire power range from 50 to 600 kW
- Flexible combination with connection options as cable and pantographs
- For fast and secure charging at the depot and en route
- Cloud-based control and monitoring of charging processes
At Busworld 2019, Siemens is presenting its Sicharge UC family for charging electric buses, trucks and duty vehicles at the depot and en route. The Sicharge UC charging system covers the entire power range from 50 to 600 kilowatts (kW) and can be combined with several connection options such as charging plugs and offboard or onboard pantographs. To meet growing demands from the vehicle industry for higher voltages, the station can operate at up to 1,000 volts (V). Electric vehicles with various technologies and batteries can therefore be charged flexibly, either en route or at the depot. The charging processes can be monitored and controlled via a MindSphere application. MindSphere is the cloud-based, open IoT operating system from Siemens.
- Conveyor system will move 127,500 tons of primary crushed ore per day
- New Siemens’ gearless drive technology to increase reliability and efficiency additionally by up to 4 percent
- Maintenance requirements of the drive system significantly reduced
Powered by Siemens’ new gearless drive technology, thyssenkrupp’s high-capacity overland conveyor will access one of the world’s largest copper reserves in Quellaveco. The Quellaveco mine in Peru contains approximately 7.5 million tons of copper in ore reserves – enough to wire 80 million homes or equip 90 million electric vehicles.