- Vision "We are global entrepreneurs, trusted by our partners to pioneer transportation, moving people sustainably and seamlessly from the first mile to the last.”
- Motto: “Moving beyond.”
- Provides clear and common direction to lead the mobility industry into the future.
Siemens
Mobility today unveiled its new vision and motto, which provides the leading
transportation company with a clear and common direction to lead the mobility
industry into the future. An industry which is characterized by a growing
demand for sustainable and intermodal mobility, driven by megatrends such as
urbanization and decarbonization. The vision, "we are global
entrepreneurs, trusted by our partners to pioneer transportation, moving people
sustainably and seamlessly from the first mile to the last,” and motto,
“Moving beyond,” encapsulates the Siemens Mobility DNA and reinforces
the intent to successfully provide innovative mobility solutions to customers
worldwide.
Siemens Gas and Power has entered into an
agreement with Total, a broad energy group, to advance new concepts for green liquified
natural gas (LNG) production. As part of the contract, Siemens Gas and Power is
conducting studies to explore a variety of possible
liquefaction and power generation plant designs, with the ultimate goal of decarbonizing
the production of LNG.
- Attica-Crete interconnection will ensure a more secure power supply and increase integration of renewable energy
- HVDC project will reduce half a million tons of CO2 emissions in first year of operation
- Total order volume for Siemens-led consortium €370 million
A consortium led by Siemens Gas and Power (Siemens Energy) has been awarded a turnkey contract for two converter stations for the Greek high-voltage direct-current (HVDC) link that will connect Crete, Greece’s largest and most populous island, with the mainland of Greece. The project will enable an exchange of electricity of up to 1,000 megawatts (MW) to enhance reliability of the power supply and facilitate integration of renewable energy sources in the power grid. Customer is Ariadne Interconnection S.P.S.A., a wholly owned entity of the Greek independent power transmission operator IPTO. Commissioning of the interconnector is scheduled for mid-2023. Total order volume for the consortium is €370 million.
- This new technology has been used in one of the biggest desalination plants in the Middle East to analyze, optimize and improve productivity, reducing operating times and finding faults early
- Simit software can be used to simulate field equipment and even the process of an entire plant, in real time.
- The Digital Twin enables virtual commissioning of the plant and remote training for operators.
Siemens has been collaborating with Acciona to create a Digital Twin to improve treatment plant management in one of the biggest desalination plants in the Middle East. This new technology is used to analyze, optimize and improve productivity, reducing operating times and finding faults early.
- Covid-19 poses major challenges for developing and mass-producing vaccines and medicines in existing production facilities
- Siemens and Exyte combine their strengths to offer intelligent, modular, and scalable biotech facilities
- Siemens provides solutions for process automation and digitalization
- Exyte offers ExyCell® modular technology for rapid construction
Siemens, a global leader in process automation, and Exyte, a global leader in the design and delivery of biopharmaceutical manufacturing facilities, join forces to offer end-to-end solutions for the biopharmaceutical industry by combining the digitalization expertise of Siemens with the innovation boost from Exyte.
- Siemens Mobility Mireo receives initial approval in just 38 months
- Start of operations for Mireo and Desiro HC in the Rhine Valley network planned for timetable change on June 14, 2020
In February 2017, the Ministry for Transport in the state of Baden-Württemberg ordered 24 Mireo trains and 15 Desiro HC double-decker trains to be operated by DB Regio. This marked the first order for the new Mireo regional multiple-unit trains developed by Siemens Mobility. The Mireo has received initial approval from the German Railway Authority in time for the timetable change in June 2020. Plans call for gradually incorporating the Mireo trains in regional service (RB) on the Offenburg – Freiburg – Basel/Neuenburg (Rhine) route beginning with the timetable change in June 2020.
- Siemens will provide main equipment for an electrical service platform for wind power project
- Mayflower Wind developing a lease area with capacity of up to 1.6 gigawatts of renewable energy
- Electricity for up to 680,000 U.S. households
Siemens has been awarded an order from Danish customer Semco Maritime to provide the main electrical equipment for the electrical service platform (ESP) of the offshore wind project Mayflower Wind LLC (Mayflower Wind). The project is located in a federal lease area approximately 25 miles south of Nantucket, Massachusetts in the United States, and will have a capacity to generate up to 1.6 gigawatts (GW) of renewable energy. Siemens will supply the components for Semco Maritime by 2022.
- Siemens again secures very
favorable financing conditions
- High investor demand
underscores excellent reputation on capital market
Siemens has
issued new bonds with a total value of about €4 billion, including a
tranche of £450 million (about €500 million). The transaction closed
successfully today. The proceeds of the issuance will be used for general
corporate purposes. At roughly €16 billion, investor demand was almost four
times the issue volume.
- Using
proven software and hardware, Siemens has developed a unique workplace
distancing solution that helps manufacturers to simulate and manage employee
exposure risks while enabling productivity throughout their facilities
- Combination
of Siemens’ SIMATIC Real Time Locating Systems and Xcelerator portfolio help
enable customers to manufacture with confidence and future-proof their
operations
Manufacturers are facing new challenges as
they look to restart or maintain operations during the ongoing COVID-19
pandemic. As preparations are made for the “next normal”, manufacturers must
consider additional dimensions of employee safety, including the establishment
of production environments and workflows that address physical distancing
requirements. Combining proven hardware and software, Siemens has created a new
solution that enables companies to quickly and efficiently model how employees
interact with each other, the production line and plant design. The new
solution also enables organizations to build an end-to-end digital twin, in
order to simulate worker safety, iterate on and optimize workspace layouts and
validate safety and efficiency measures to help future-proof production lines.
- Electricity and district heating for eastern part of the capital city
- From Berlin for Berlin: Gas turbine from Siemens plant in Moabit
- Highest efficiency through cogeneration
- Maximum fuel efficiency of 92 percent
Vattenfall Wärme Berlin AG today officially commissioned the Berlin-Marzahn combined heat and power (CHP) plant, which was built by Siemens Gas and Power as general contractor. The Governing Mayor of Berlin, Michael Müller, and the Vice President of the German Bundestag, Petra Pau, visited the natural gas-fired combined cycle plant with district heating extraction. Together with Tanja Wielgoß, CEO of Vattenfall Wärme Berlin AG, and Jochen Eickholt, member of the Managing Board of Siemens Energy, they inaugurated the new power plant. The combined heat and power plant is one of the most efficient in Europe and makes an important contribution to Berlin's climate-neutral energy supply.