- Project includes six SGT-A35 aeroderivative offshore gas turbine packages
- Contract includes a long-term service agreement
Siemens Power and Gas, including its Dresser-Rand business, received an order for four SGT-A35 gas turbine power generation packages and two SGT-A35-driven DATUM CO2 compressor packages for MODEC's Sépia floating production, storage, and offloading (FPSO) vessel. The vessel, which is named "FPSO Carioca MV30," will be deployed at the Sépia field operated by Petrobras, located in the giant "pre-salt" region of the Santos Basin approximately 250 kilometers (155 miles) off the cost of Rio de Janeiro, Brazil. In addition, Siemens will provide long-term expert service and maintenance for the supplied components.
- New MindApps for the open cloud-based IoT operating system MindSphere
- Analyze MyDrives provides new insight into the drive train
- Manage MyMachines/Remote enables remote access to CNCs
Siemens is launching a new app for drive systems in the field of Motion Control called Analyze MyDrives, and has also introduced Manage MyMachines/Remote, a new plug-in to upgrade its tried and tested Manage MyMachines MindApp for machine tools with the addition of a smart remote feature. Analyze MyDrives and Manage MyMachines/Remote are special MindApps designed specifically for MindSphere, the open IoT operating system from Siemens, which allow users to utilize the benefits of cloud-based services and create added value with machine operation. Digitalizing drive systems or machine tools enables extensive data generated by the drive or machine to be analyzed and put to use. By connecting to MindSphere, this process can be carried out simply by the machine manufacturer or user, significantly improving the efficiency of drive systems and machines and boosting productivity across the production network. In this way, these MindApps provide the starting point for totally new applications for drives or machine tools which enable innovative digital services such as predictive maintenance, energy data management or resource optimization.
- New low-voltage motor Simotics SD Pro suitable for mains-fed and converter operation with voltages up to 690 volts
- Multi-voltage capability and reliable adherence to efficiency class IE3 at 50 and 60 hertz
- Industry-specific and country-specific certificates for global use
Simotics SD Pro completes the next generation of low-voltage Simotics SD motors from Siemens. The new variant is equally suited for mains-fed operation or for use with a converter for voltages up to 690 volts (V). There is generally no need to use special filters at the converter output. The Simotics SD Pro motors reliably fulfill the requirements for compliance with efficiency class IE3, irrespective of whether they are operated at 50 or 60 hertz (Hz). Used in conjunction with a comprehensive range of industry-specific and country-specific certificates, they can be used in all the world's most important regions and markets, and also in wide-ranging different plant configurations. The Simotics SD Pro offers the bonus of multi-voltage capability, making it ideal for series production by OEMs. The motors can be stably operated with all power supplies in common use around the world, and fulfill the requirements for compliance with the respective efficiency class at all operating points. This motor variant operates with the utmost reliability and efficiency under even the toughest enviromental conditions such as those prevailing in the oil and gas industry. Typical applications for the low-voltage motors include pumps, compressors, fans, cranes and hoists, conveyors, chippers, coilers, grinders, shears and rolling stands.
- High-power charging stations for electric buses
- Elimination of noise pollution and harmful emissions
Siemens signed a frame contract with Movia, the largest public transport authority in Denmark, to deliver charging stations with a top-down pantograph for electric buses on request of their municipalities. The contract is a good example of how corporation between public authorities and private companies can help to improve climate change.
- Transparency for industrial plant networks and the software in use
- Comprehensive vulnerability insights
- Industrial Anomaly Detection to identify threats
- Important complementary measure for the Defense-in-Depth security concept
Siemens will present a solution for detecting anomalies in industrial networks at the Hannover Messe 2018. "Industrial Anomaly Detection" enables security-related incidents, such as unauthorized intrusions and malware, to be identified and countermeasures to be taken. The software is pre-installed on an industrial PC (IPC), and easily integrated into industrial environments. Alternatively, it will be enabled to run on network components from Siemens, such as the multiservice platform Ruggedcom RX1500 with Ruggedcom APE. The solution is especially suitable for companies in the automobile production, aerospace, chemical, pharmaceutical, food and beverage, and water/waste water industries.
- Biggest rail infrastructure order in Siemens history
- Order worth around 800 million Euros
- Approximately 4,200 track kilometers and 375 stations
- Scheduled completion by 2034
Siemens is to equip the entire Norwegian railroad network of approximately 4,200 track kilometers with the European Train Control System (ETCS) Level 2 type Trainguard combined with the interlocking type Simis W and IP-based wayside network communication solution type Sinet. The order was placed by Bane NOR SF, the state-owned company responsible for the Norwegian national railway infrastructure responsible for owning, maintaining, operating and developing the Norwegian railway network. The new digital signaling system enhances safety, punctuality and capacity on the rail system and is planned to be completed in 2034. The contract also includes maintenance services for 25 years and is worth around 800 million euros in total.
- Lineside equipment to be converted to the European Train Control System throughout Norway
- Order volume worth around 800 million euros
- Scheduled completion of rollout lines by 2034
- 25 years of service starting with the commissioning of the first line
Bane NOR, the state-owned agency responsible for the Norwegian national railway infrastructure, has contracted Siemens to upgrade the signaling equipment of the entire Norwegian rail network to the European Train Control System (ETCS). Commissioning of the rollout lines is scheduled to be completed by 2034. The contract also includes services for 25 years and is worth around 800 million euros in total.
- Real-Time Locating Systems (RTLS) as key technology for the Digital Enterprise Portfolio from Siemens
- Precise localization to improve efficiency in production and logistics
- Foundation for new flexible production concepts
With effect from March 29, 2018, Siemens has taken over ownership of the company Agilion GmbH based in Chemnitz. Agilion is a leading supplier of industrial Real-Time Locating Systems (RTLS) focusing on applications in production, logistics and maintenance. The company is recognized as a pioneer in the field of RTLS in the Ultra Wide Band (UWB) frequency spectrum. This technology enables highly precise localization within a range of just a few centimeters, tracking of a large number of different assets, and exceptionally easy commissioning. The precise real-time localization of assets such as tools or vehicles will enable manufacturers to optimize their production and logistics processes and so improve their quality, productivity and flexibility.
Petroecuador, Ecuador’s national oil company, recently selected Siemens to supply an 8-MW SGT-300 gas turbine for power generation for its Shushufindi refinery. The refinery is located in the province of Sucumbios, in the eastern part of Ecuador. Commissioning of the new unit is scheduled for the end of this year.
- 50/50 joint venture for the maintenance of locomotives
- Company to be named Locomotive Workshop Rotterdam (LWR)
- Workshop to be built in the port of Rotterdam
Siemens and Mitsui Rail Capital Europe (MRCE), a full-service locomotive leasing company, have agreed to found a joint venture for the servicing and maintenance of locomotives. The agreement stipulates that Siemens and MRCE each will hold a 50-percent stake in the joint venture and jointly manage the new company. Founding of the firm, pending approval of antitrust authorities, is expected to be completed in the first half of calendar year 2018.