- Sinamics G115D comprises motor, frequency converter and gear box and is available as one complete solution in a motor-mounted and wall-mounted version
- Comprehensive TIA portal and Startdrive integration simplifies commissioning
- Compatibility with MindConnect portfolio enables cloud-based analysis
With
Sinamics G115D, Siemens presents a new, compact, and powerful drive system
specifically designed for horizontal conveyor applications. The drive system
comprises motor, frequency converter and gearbox in one unit and is offered in
two versions – wall-mounted and motor-mounted. The Sinamics G115D drive system
is characterized by a robust design with a high IP protection class (up to
IP66) and is therefore also suitable for use in harsh environments. Thanks to
its compact dimensions, the Sinamics G115D can be installed easily even in
confined areas. The drive system can also be operated reliably over a wide
temperature range of -30 to 55 degrees Celsius. The Sinamics G115D drive system
is suitable for applications in intralogistics and airports as well as in the
automotive and food & beverage industries and is available in the power
ranges 0.37 to 7.5 kilowatts for wall mounting and 0.37 to 4 kilowatts for
motor mounting. The drive system can be put into operation quickly and easily
with comprehensive integration into the TIA (Totally Integrated Automation)
portal including the Startdrive commissioning software, or the Sinamics G120 Smart
Access Module (SAM) web server tool for setup and diagnostics. To be prepared
for the digital transformation and to enable cloud-based analyses, Sinamics
G115D is integrated into the entire MindConnect portfolio and is compatible
with Mindsphere applications such as Analyze MyDrives.
- Siemens to offer industry’s first integrated multiscale solution for soft matter as part of Simcenter portfolio
- Addition of Culgi technology to enable performance-driven optimization of advanced materials in both discrete and process manufacturing industries
Siemens announced
today that it has signed an agreement to acquire Culgi, a computational
chemistry software company with a focus on multiscale simulations in the
process industries. Culgi will join Siemens Digital Industries Software, where
its solutions will expand simulation capabilities of the
Xcelerator
™
portfolio with quantum and molecular chemistry models that seamlessly couple
with the continuum approach in
Simcenter™ STAR-CCM+™ software. This unique engineering workflow can deliver
significant cost savings and accelerate innovation in the materials and process
industries, increasing the potential for product and process transformations.
- Siemens is the exclusive global sales partner for Moby.Check in the process industry
- Simple functional solution offers advantages for mobile servicing and maintenance procedures as well as for production and logistic operations in the process industry
- Audit-proof storage of testing and maintenance tasks
- Stand-alone solution can be integrated easily into existing maintenance or ERP systems
Siemens and Log.Go.Motion - a specialist in the digitalization of processes in industry and logistics - have concluded a cooperation agreement.Effective immediately, Siemens is the exclusive global third-party distributor for the Moby.Check software solution within the process industry. Moby.Check can be used to create, control, and monitor individual digital inspection checklists for servicing and maintenance procedures as well as for production and logistics processes. The software system has been developed for global use in industry.
- Robotic fiber placement and 3D printing enable disruptive breakthroughs in today’s manufacturing processes thanks to the advantages promised by Industry 4.0, the Digital Twin, higher robotic intelligence and complex motion control.
Siemens and Ingersoll Machine Tools have expanded their decade-long partnership to support the Rockford, IL-based machine tool company of Camozzi Group on its digital journey of creating digital twins of its products and expanding into new markets. Based upon extensive experience in heavy machine tool building, Siemens cutting-edge technologies in hardware complement Ingersoll Machine Tools’ successful journey into the new market of additive manufacturing and have pushed the boundaries for industrial robots for the aerospace market with its entry-level robotic platforms MasterPrint Robotic™ and MasterPrint Continuous Filament™.
As a virtual event, the Siemens Machine
Tool Days provide insights into digital solutions for the machine tool
industry. Keynotes, #HowTo expert panels and practical examples will deal with
digital possibilities for increasing productivity in manufacturing under the
motto "Digitalization in Machine Tool Manufacturing - Thinking further!
Using the Digital Enterprise portfolio as an example, Siemens will show how the
integration of automation and digitization with future technologies such as
edge and cloud computing and artificial intelligence can be used effectively in
every phase of the value-added chain: from building a digital twin of the
product to production and machine performance to digital services.
> Register here > Explore our agenda
Today, the need for industrial digital solutions is more pressing and more important than ever before. During this event, we want to show how you can benefit from our digital solutions for the machine tool industry - from the Digital Twins of product, production and performance to every aspect of the value chain, including digital services.
- Sinumerik One Dynamics - three technology packages to increase the efficiency of CNC users when programming in the shopfloor and executing CAM-generated CNC programs
- Top Surface and Top Speed Plus for excellent motion control and perfect workpiece surfaces
With the software version NCU-SW 6.14, Siemens is launching three powerful technology packages exclusively for the CNC Sinumerik One. The Sinumerik One Dynamics packages are available in three different packages: One Dynamics Operate, One Dynamics 3-axis milling and One Dynamics 5-axis milling. The software functions contained in the technology packages support users from machine-oriented programming in the jobshop to high-performance machining of CAD-CAM-programmed workpieces with high surface quality.
- Improvement of machine tool availability through predictive maintenance with Analyze MyMachine /Condition
- Analyze MyMachine /Condition for Sinumerik Edge creates a mechanical fingerprint of the machine tool
- Condition evaluation, analysis and comparison of all connected machines using the Mindsphere application
Siemens is extending its edge application Analyze MyMachine /Condition with a corresponding Mindsphere application and thus demonstrating how edge computing and cloud computing can be intelligently combined. The Sinumerik Edge Application Analyze MyMachine /Condition, which the company presented last year at the EMO, uses high-frequency CNC data to create the mechanical fingerprint of a machine tool. In the application, users can capture and evaluate various parameters such as stiffness, friction, and backlash in the individual axes with the help of flexibly configurable measurement series. The measurement results can then be visualized and compared with reference data.
- High-frequency radar ensures
reliable readings in challenging environments
- Optional
HMI delivers easy commissioning and diagnostic
support
- Wide
range of liquids and solids applications in practically all market segments
including energy, mining, aggregates and water
Siemens presents two new additions
to the Sitrans LR100 series of 80 GHz radar transmitters. These high-frequency,
compact transmitters deliver robust, reliable measurements even in the most
challenging environments. Both deliver fast and easy setup. Sitrans LR140
features 4-20 mA simplicity and is configured via Bluetooth wireless technology
and the Sitrans mobile IQ App.
- New standard library for shorter winding times at a higher quality
- Can be used for linear winding procedures of rectangular coils
- Engineering and commissioning times of winding machines are reduced
For the faster production of e-motors, Siemens has developed a new application which optimally controls wire tension for linear winding and minimizes fluctuations in force. The Wire Brake software application for automated winding of rectangular coil former controls the tension of the copper wire. In comparison to passive systems, this enables higher winding speeds and a higher winding quality to be achieved. The functionality can be integrated directly into the machine project using the standard library "Simotion Wire Brake" which shortens engineering and commissioning costs. It contains algorithms which include the rectangular geometry of the coil former as well as the "TensionControl" components to control the wire tension brake axis and "CamGeneration" to calculate cams using reference values.
- New services enabled by the Mendix low-code platform enable data-driven decision making in factories and across enterprise data sources
Siemens Digital Industries Software is leveraging the Mendix™ low-code application development platform to help customers across industries build contextual and personalized solutions and help enable data-driven decision-making processes. With the general availability of Mendix Data Hub and new Mendix for Industrial Edge services, Siemens can help customers achieve an end-to-end view of their plants, factories, and systems and provide domain experts with actionable insights through solutions that have been developed with the right data from across the organization. The Mendix platform extends the Xcelerator™ portfolio with the ability to build multi experience apps and share data from any location, on any device, on any cloud or platform, to more quickly realize the benefits of digital transformation.