Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Easy configuration with new 80 GHz compact radar transmitters for level measurement

Sitrans LR150 offers a four-button user interface on an optional HMI for configuration or monitoring. Configuration is also available via Bluetooth wireless technology and the Sitrans mobile IQ App or remotely with 4-20 mA/HART using Simatic PDM.
The easy-to-use Quick Start Wizard will have the transmitter operational in minutes. Custom microchip technology delivers fast response and extremely high sensitivity to detect even the weakest of signals.
Reliable readings mean reduced operator exposure to hazardous situations: no need to climb tanks, lean out over sumps, or crawl into confined spaces to maintain instruments. Zero blanking distance allows measurement right up to the sensor, thereby avoiding costly overfilling. And two-millimeter accuracy enhances operational safety through precise measurement through the full range of the application.
All this robust performance is wrapped in a submersible housing constructed of corrosion-resistant materials.
Integrating critical level readings or process control data into operations can unlock new opportunities to react to safety concerns, analyze processes and identify areas for improvement. Users can monitor level measurements or diagnostic and maintenance information from the comfort of the control room or connect to Siemens MindSphere, the cloud-based, open IoT operating system or any other IoT solution of your choice.
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Read more
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability, and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020. In fiscal 2019, which ended on September 30, 2019, the Siemens Group generated revenue of €58.5 billion and net income of €5.6 billion. As of September 30, 2019, the company had around 295,000 employees worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Evelyne Kadel

Digital Industries

Klaus-Bungert-Str. 6
40468 Düsseldorf
Germany

+49 173 56 49 708