- Siemens supports Hexr in the mass customization of additively manufactured bicycle helmets
- Digital Enterprise portfolio offers integrated software and automation solutions for additive manufacturing
- Additive Manufacturing Network – an online order-to-delivery collaboration platform for the industrial additive manufacturing community, helps streamline the AM production process
Bicycle helmets made to measure and in an
affordable framework for everyone - what was unthinkable a few years ago is now
becoming reality thanks to digitalization and additive manufacturing. The head
is simply scanned with a smartphone app and the process for the custom-made
helmet is initiated. Siemens, together with EOS, has supported this vision of
the bicycle helmet manufacturer Hexr. Siemens' Digital Enterprise portfolio
consists of software and automation solutions that optimize process steps along
the entire value chain of additive manufacturing. This holistic approach is
unique in the field of the industrialization of additive manufacturing. With
the help of end-to-end solutions, Siemens has created the digital twin of an
industrialized additive manufacturing factory, helping to optimize the design
and streamline the production processes for customized bicycle helmets even
before production begins. By combining simulation, design optimization and a
high degree of automation in production, the costs per part could be predicted
and significantly reduced, allowing Hexr to scale the scan-to-print application
to mass production.
- Simotics SD Add low-voltage motors reduce drain on the grid due to low start-up currents
- Compliance with sector-specific specifications in the process industries
- Global certificates for worldwide usage
- Reduced acquisition costs coupled with extended service life
With the introduction of its new Simotics SD Add low-voltage motors, Siemens is extending the application scope of the next-generation Simotics SD low-voltage motor series it launched at the beginning of this year. This marks another step taken by the company towards the expansion of its portfolio of scalable standard motors for use in challenging ambient conditions. By offering low start-up current levels, the characteristic product feature of the Simotics SD Add low-voltage motors, this new addition to the series is opening up greater application scope: for instance, to comply with sector-specific requirements in the process industries, or in fields requiring enhanced grid stability by reducing grid loads in the event of voltage dips. The availability of country-specific certificates means that these motors can be used without restrictions in all regions and markets of importance around the world.
- Innovative woodworking control system
- Digitalization boosts productivity and flexibility
Under the banner "Digital Enterprise – Thinking industry further", Siemens is showcasing an extensive portfolio of innovative control and automation solutions for digitalizing the entire value chain in the woodworking and wood processing industry at the Ligna 2019 in Hannover from May 27-31, 2019 in Hall 16 at Booth C14.
- First new frame size in 0.4 to one kilowatt output range
- New shared DC link coupling reduces waste heat during braking and increases traversing cycle of individual axes
- Higher-level control now possible with Simatic ET 200SP CPUs and Open Controllers or Simatic S7-1500 Software Controllers
- Engineering and commissioning using Sizer and Start Drive, engineering in TIA Portal V15.1
Siemens is extending its Sinamics S210 single-axis servo drive system for mid-range applications to include a number of additional output and connected voltage variants. In the first of the new frame sizes, the system is available with an output of 0.4 to one kilowatt with 3 AC 400 volts. The new Sinamics S210 device variants come with an optional busbar trunking system and a shared DC link coupling to enable their international application. The DC link coupling permits energy equalization during dynamic reversing operations by using the integrated braking resistor to reduce waste heat occurring during braking and increasing the traversing cycle of the individual axes. Alongside S7-1500 Advanced Controllers, higher-level control of the new devices is also possible using Simatic ET 200SP CPUs (Central Processing Units) and Open Controllers or Simatic S7-1500 Software Controllers, all of which are connected over time-synchronized Profinet IRT. The drive system can be simply engineered and commissioned using the integrated web server. Alternatively, engineering can now also be performed using Startdrive in the TIA (Totally Integrated Automation) Portal from Version V15.1.
- IoT concept for Simotics motors
- Monitoring the operating condition of motors
- Connection to MindSphere open IoT operating system
- Maximum transparency and increased productivity due to intelligent evaluation: Data analysis by Simotics IQ
With Simotics IQ, the new IoT concept for motors from Siemens, the new Simotics SD low-voltage motors are fitted with a compact sensor box which captures important operating and condition parameters and transmits them by WiFi to the cloud. These operating data can then be stored and analyzed by the Simotics IQ MindApp on MindSphere. The Simotics IQ MindApp provides the user with technical motor data and valuable analytical results on the operation and condition of the motor and proposes, for example, recommended actions for preventive maintenance. This newly acquired operating data transparency allows further increases in productivity to be achieved.
World Forum and Leading Show for the Process IndustriesUnder the motto "Accelerate the digital transformation – from integrated engineering to integrated operations." we presented at the Achema 2018 trade show specific applications for how to use the potential of digitalization to enhance efficiency, flexibility, and quality – and to shorten time to market. Production can be significantly optimized and made more flexible by integrating all components in instrumentation and control and management systems and by intelligently using all of the process data generated in a common data model – the digital twin of the overall plant. Maintenance effort and costs can also be slashed dramatically by using cloud-based applications and data-based services.
On the first day of the Hannover Messe, April 1, Klaus Helmrich welcomed you to the annual Siemens Press Conference. As member of the Managing Board of Siemens AG, Klaus Helmrich is responsible for the Digital Industries Operating Company. The Press Conference took place at 6:30 PM in the Trade Fair's Convention Center, Room 1 A/B.Mr. Helmrich talked about the latest developments of digitalization and the next step towards the digital transformation in the manufacturing and process industries under the theme "Digital Enterprise – Thinking industry further!".
- New MindSphere Version 3.0 on Amazon Web Services (AWS) provides access to Siemens APIs and AWS cloud services for faster development
- Simotics IQ: New IoT concept for motors
- New partnership financing service to boost the implementation of Industrie 4.0
- Study affirms annual productivity increase due to digitalization of up to 9.8 percent
Increasing demands by consumers for individual, high-quality products at favorable prices are posing new challenges for industrial enterprises which can only be resolved by digitalization. "With the Digital Enterprise portfolio, the technical conditions have been created for Industrie 4.0. To ensure successful implementation of Industrie 4.0, what we now need is an extended model for cooperative partnership based on mutual respect: Large-scale corporations supply platforms and components, medium-sized enterprises develop their own solutions and business models on this basis, and end customers integrate these into their digital value chain," explained Klaus Helmrich, Member of the Managing Board of Siemens AG at the SPS IPC Drives. Siemens will be showcasing a range of innovations at the show designed to shorten the time to market and to improve flexibility, efficiency and quality in the process and manufacturing industries. They range from the new Version 15 of the Engineering Framework TIA Portal through the IoT concept for motors Simotics IQ to the new Version 3.0 of the open cloud-based IoT operating system MindSphere. Siemens is also offering financing services such as pay-per-use models designed to simplify the implementation of digital solutions, aimed in particular at medium-sized enterprises.