Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release22 November 2017Process Industries and DrivesNuremberg
Extended application scope for Siemens low-voltage motors

The picture shows the Simotics SD low-voltage motor.
While providing the same level of performance, highly efficient motors such as Simotics SD Add with efficiency classes IE3 and IE4 offer a greater ratio of start-up current to rated current than less efficient motors. Its special electrical design has enabled the start-up current levels in the Simotics SD Add to be significantly reduced while retaining the same compact size and without compromising on efficiency. Low start-up currents increase the service life of the motor, as they reduce the incidence of torque shocks, which stress the motor windings both thermally and also due to electrodynamic forces. This design also enables supply cables, control cabinets, protection equipment and industrial controls to be more compactly dimensioned, saving on both procurement and operating costs.
Lower start-up current levels mean that grid loads due to disturbing voltage dips can be reduced, creating greater grid stability. This is a particular benefit in regions with a less well-developed grid infrastructure and in soft grids of the kind found in countries covering an extremely large geographical area such as Canada, Russia or the USA.
To simplify commissioning, servicing, spare part procurement and the attachment of optional components, the Simotics SD Add motors are fitted as standard with a DataMatrix code. This enables all relevant information such as technical data, spare parts and operating instructions for the individual motors to be accessed on mobile terminals using the Simotics Digital Data App.
For further information on Simotics, please see www.siemens.com/simotics
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 372,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Stefan Rauscher
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7952