- Up to three additional applications on one processor module
- Siapp eliminates need for additional hardware, saving space and costs
- Secure distributed data processing 24/7
Siemens Smart Infrastructure is expanding the options for distribution grid applications with the new Siapp, a software license for the Sicam A8000 automation and remote terminal unit. The Siapp application is based on the Sicam A8000 with the powerful CP-8050 processor module. Siapp allows up to three separate custom applications to be developed, parameterized and loaded onto the remote terminal unit. Only one runtime license is needed. Siapp complies with the strictest data security standards and benefits customers including major energy suppliers, municipal utilities and industrial companies.
- Direct integration into Building Operator for control, alarming and energy reporting
- Expanded product range now available as 3-port valve
- New features such as Delta-T limitation control, make it possible to optimize plants with chillers and reduce consumption
The self-optimizing and dynamic Intelligent Valve from Siemens Smart Infrastructure has become more versatile, thanks to new features and applications for heating groups and air handling units. The device controls the flow, measures temperature and output and automatically adjusts the valve settings to the heat exchanger. The Intelligent Valve is connected to the cloud and now, for the first time, directly integrated into Building Operator, the Siemens cloud application for the remote monitoring of buildings. This makes it possible to control the Intelligent Valve and adjust its settings anytime and anywhere. For increased flexibility, the product range has been expanded to include 3-port valves, which allow variable-temperature and constant-flow control of the water supply (mixed circuits). New features such as Delta-T (DT) limitation control, differential pressure and flow temperature control ensure smooth and energy-efficient HVAC plant operation and enable the Intelligent Valve to be used in even more applications.
- Joint training against cyberattacks key in protecting digital grids
- Valuable insights on attacks and vulnerabilities enable innovative solutions and safer products
Siemens Smart Infrastructure and the NATO Cooperative Cyber Defence Centre of Excellence (CCDCOE) have signed a Memorandum of Understanding (MoU) to continue the cooperation on cybersecurity for critical infrastructure. The CCDCOE organized annual high-level cyber defence exercise Locked Shields exercise provides a key pillar to jointly build up defence capabilities. With the new agreement, the parties advance their existing cooperation on cyber security training for power grids. In experimenting with grid control software Spectrum Power, Siemens gains valuable insights on the potential attack vectors and can thoroughly test new security features or protocols for its products and solutions.
- System based on Siemens Spectrum Power supports second-by-second control of all assets and integration of RWE wind and solar farms
- Improved combination of electricity generation from renewables and conventional fuel is a major milestone for the energy transition
RWE is making its power station control system fit for the future by adopting a new technology. Optime, a new SCADA system based on Siemens Spectrum Power, gives RWE a uniform control technology. SCADA stands for 'Supervisory Control and Data Acquisition' – in other words monitoring and managing technical processes using a computer system. Previously, there were two separate systems: one for power plants in Germany and another for the Netherlands and Belgium. The new solution combines the two, while integrating RWE’s renewable energy assets in Europe. It can also accommodate additional units such as battery storage systems and diesel-powered backup generators.
- Collaboration will support businesses’ safe return to work and build smart, connected workplaces for the future
- Joint solutions, built on technology from Siemens and Salesforce, include a ‘touchless office’ and advanced contact tracing
Today, Salesforce (NYSE: CRM) and Siemens announced a strategic partnership to develop a new workplace technology suite that will support businesses globally to safely reopen and deliver the future experience for physical workplaces. The partnership will combine Salesforce’s Work.com, powered by Customer 360, and Siemens’ Smart Infrastructure solutions, including Comfy and Enlighted, to orchestrate the processes, people and things that are essential to creating safe, connected workplaces for the future.
- Charging technology for 39 parking spaces at innovative eBus depot of VAG
- Parallel charging of 20 buses with up to 150 kilowatts
- Medium-voltage connection for supply with 100 percent green electricity
Siemens Smart Infrastructure has received a contract from Verkehrs- Aktiengesellschaft Nürnberg (VAG) to equip its new “eBus port” with a medium- voltage connection and charging infrastructure. With 39 parking spaces, it will be one of the largest electric bus depots in Germany. Located on the VAG premises in the Nuremberg suburb of Schweinau, it will be supplied solely with green electricity. Construction has already started, and operations are scheduled to start in 2021.
- Systems for charging at the depot and on-route
- Charging via on-board pantograph and contact hood with 100 and 450 kilowatts
- Integrated medium-voltage connection for space-saving installation
Siemens Smart Infrastructure will provide the charging infrastructure for 21 fully electric low-floor buses in Leipzig. VDL Bus & Coach received the associated contract from the Leipziger Verkehrsbetriebe (LVB) GmbH, the public transport operator in Leipzig. The charging systems from Siemens will supply electrical energy to VDL buses on lines 74, 76 and 89 as well as at the Lindenau bus depot and are scheduled to go into operation in 2021. The electrification of local public transport is a major lever for sustainable urban planning. With its Mobility Strategy 2030, also the City of Leipzig aims to develop environmentally-friendly transport systems.
- F-gas-free Clean Air switchgear extends blue GIS portfolio to 24 kV level
- Proven and safe technologies for easy management over the entire lifecycle
- Digital features allow for increased reliability in all grids and optimized operation
Siemens Smart Infrastructure is expanding its portfolio of environmentally friendly, gas-insulated switchgear (GIS) to 24 kilovolts (kV) with a new fluorine gas-free NXPLUS C 24 medium-voltage switchgear. The use of Clean Air – a natural insulation medium – in combination with proven vacuum switching technology eliminates the need for any fluorine-based gas mixtures (F-gases), enabling climate-neutral energy distribution. The switchgear is equipped with digital features allowing for safe, reliable and cost-efficient operation.
- New 3RS2 product series for monitoring the temperature of gases, liquids, and solids in industrial and infrastructure installations
- Overall width was cut in half and allows space-saving installation
- Combining functions into one device simplifies order selection
Siemens Smart Infrastructure has transformed the temperature monitoring relays from its Sirius portfolio. The new series 3RS2 devices are available in analog and digital versions. They use sensors to measure the temperature in industrial control cabinets, of engine, bearing, and transmission oils, or cooling liquids, preventing plant malfunctions or damage that can result when exceeding or dropping below certain limit values. These relays can also monitor heating, air-conditioning, and ventilation systems, solar collectors, heat pumps, and hot water supply systems.The devices in the new Sirius 3RS2 series
are approved for safety applications up to SIL 1 / PL c, for use in industrial
furnaces, as well as for monitoring burners and ATEX applications, among other
things. Compared to the predecessor models, they feature expanded
functionalities, a narrower design, and easier operability.
- Contactless temperature measurement at main entry points in buildings
- Integrates into workflow of existing security and access solutions
- Increases protection of building occupants
Siemens Smart Infrastructure announced the launch of Siveillance Thermal Shield. This solution package quickly measures the body temperature of a person seeking to access a building and enables the results to be integrated into the video and access systems of corporations. Thermal imaging cameras are used to measure, in a contactless way, the body temperature at a distance of up to two meters, ensuring the safety of monitoring staff. If the camera screening indicates an elevated body temperature, a second reading must be taken using a medical thermometer to confirm the finding.