Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release13 May 2020Smart InfrastructureZug (Switzerland)
New Sirius temperature monitoring relays offer more functions in less space
Measuring only 22.5 millimeters wide, the
Sirius 3RS26 digital devices are parameterized via an intuitive LCD display and
can be connected to a sensor that evaluates whether the temperature is above or
below a certain value or within a specific operating range (window function). A
SIL1-certified infrared communications interface makes it possible to
wirelessly add two resistance sensors and one analog input. As a result, they
can also monitor large, three-phase motors and transformers.
The integrated LCD display provides new
functionalities, such as an energy-saving mode (ecoMode) and improved
calibration capabilities. If values exceed or drop below limit temperatures,
the plant concerned is automatically shut down.
The second limit value may be used to issue a warning.
By changing color, the display indicates the equipment status (error, warning,
limit value exceeded). If a fault occurs, such as a cable break, the relay
switches to a safe state.
Variants are available for one sensor, two
threshold values, and all common resistance sensors and thermocouples. The
devices can be reset manually, by remote access, and automatically. A memory
function ensures that the last device state is stored and recovered in the
event of a blackout. The digital devices are also available with an IO link, so
that temperature data can be forwarded to higher-level controllers and
integrated in open cloud-based IoT systems, such as MindSphere.
They are certified according to functional
safety standards (IEC 61508/62061 and ISO 13849) and can therefore be used in
safety applications up to SIL 1 / PL c. They are also approved as temperature
monitors and limiters according to EN 14597 and can be used in industrial
furnaces. Burners can also be monitored, thanks to EN 50156 certification.

The analog Sirius 3RS25 multifunction
devices are set via rotary and slide switches and can also be used as simple
two-position controllers. They detect the temperature via a sensor in the respective
medium and evaluate the data to determine whether it has exceeded or dropped
below the predefined limit temperature. They can switch loads directly via a
relay changeover output once a threshold value has been reached. The opener for
the changeover output can be simultaneously used as a signaling contact. The
product series includes devices for a resistance sensor or a type J or type K
thermocouple, which can monitor a threshold value for the most common
temperature ranges.
The new Sirius 3RS2 devices replace the
series 3RS1 predecessor models.

The new Sirius 3RS2 temperature monitoring relays measure only 22.5 millimeters in wide and are parameterized via an intuitive LCD display.
For further information on Siemens Smart
Infrastructure, please see
www.siemens.com/smart-infrastructure
www.siemens.com/smart-infrastructure
For this press release
Social Media
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 72,000 employees worldwide.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed companies Siemens Energy, the global energy business of Siemens, and Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the energy systems of today and tomorrow as well as the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy (as part of Siemens Energy), Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Heidi Fleissner
Smart Infrastructure
Siemensstr. 10
93055 Regensburg
Germany
93055 Regensburg
Germany
+49 (173) 7383392