- Re-use of domain-specific simulation models
- Standardized interfaces for more system openness
- Real-time simulation of systems and machinery
Siemens has extended its Simit simulation platform for virtual commissioning and operator training to include numerous new functions. The additions in Version 10.1 improve the simulation of automation applications through the re-use of various domain-specific simulation models over the entire lifecycle of manufacturing and process systems. Improved performance, openness and flexibility make the solution even easier to use, supporting the user in the creation of a comprehensive and integrated simulation.
- Simit Unit Administration integrated into the Simit user interface
- Simplified configuration of PLCSIM advanced coupling
- Bulk engineering using Chem Basic Library spreadsheet calculation – for chemical and pharmaceutical plant simulation
- Data transmission now also via OPC UA client coupling
Siemens has upgraded its Simit simulation platform for virtual commissioning and operator training with a new release. Version 9.1 enables Simit to also be used for virtual commissioning and operator training in modular plants, speeding up actual commissioning by as much as 60 percent and reducing unwanted standstill periods to a minimum, particularly during plant conversion and migration processes. Simit can also be used to implement a realistic operator training system. Version 9.1 comes with an array of innovations designed to improve operating convenience, support simulation modeling and contribute towards improved efficiency, openness and flexibility.
- This new technology has been used in one of the biggest desalination plants in the Middle East to analyze, optimize and improve productivity, reducing operating times and finding faults early
- Simit software can be used to simulate field equipment and even the process of an entire plant, in real time.
- The Digital Twin enables virtual commissioning of the plant and remote training for operators.
Siemens has been collaborating with Acciona to create a Digital Twin to improve treatment plant management in one of the biggest desalination plants in the Middle East. This new technology is used to analyze, optimize and improve productivity, reducing operating times and finding faults early.
- New Sinamics DriveSim Basic software solution for fast and easy simulation of drive constellations
- Seamless integration of models into commercially available simulation programs
- Validated function units accelerate development phase
With Sinamics DriveSim Basic, Siemens presents a new software solution with which for the first-time drive constellations and their behavior in machines and plants can be simulated, adapted, and optimized. With the new solution, Siemens offers a quick and easy entry into the simulation of drive technology and enables machine and plant manufacturers to accelerate their own development phase.
- New NCU 1740 for higher scalability of Sinumerik One
- Sinumerik Run MyRobot /Direct Control V2.0 and Run MyRobot /Direct Handling V2.0 available for Sinumerik One
- New functions for the Digital Twin in Create MyVirtual Machine and Run MyVirtual Machine
Siemens is expanding its offering for the "Digital Native" CNC Sinumerik One. Two years after its market launch, the technology company is presenting numerous innovations in hardware and software for the Sinumerik One at EMO Milano and the virtual Siemens Machine Tool Days. In this context, Siemens is demonstrating how the powerful machine tool controller can be used in a highly productive, flexible, and modular way and in the best possible way for digital transformation. In terms of hardware, the new NCU 1740 complements the existing NCU 1750 and 1760 as well as the PPU 1740, thus expanding its use in modular machines.
On the first day of the Hannover Messe, April 1, Klaus Helmrich welcomed you to the annual Siemens Press Conference. As member of the Managing Board of Siemens AG, Klaus Helmrich is responsible for the Digital Industries Operating Company. The Press Conference took place at 6:30 PM in the Trade Fair's Convention Center, Room 1 A/B.Mr. Helmrich talked about the latest developments of digitalization and the next step towards the digital transformation in the manufacturing and process industries under the theme "Digital Enterprise – Thinking industry further!".
World Forum and Leading Show for the Process IndustriesUnder the motto "Accelerate the digital transformation – from integrated engineering to integrated operations." we presented at the Achema 2018 trade show specific applications for how to use the potential of digitalization to enhance efficiency, flexibility, and quality – and to shorten time to market. Production can be significantly optimized and made more flexible by integrating all components in instrumentation and control and management systems and by intelligently using all of the process data generated in a common data model – the digital twin of the overall plant. Maintenance effort and costs can also be slashed dramatically by using cloud-based applications and data-based services.
- Simatic PCS 7 Plant Automation Accelerator V3.0 plant and automation engineering software closes the gap between plant engineering and the process control system
- More powerful, more open version
- Increased system openness based on GSDML and NE150 standards
- Seamless engineering through the integration of various Simatic components
Siemens has extended its engineering software for planners and automation engineers, Simatic PCS 7 Plant Automation Accelerator 3.0 (PAA), to include new functions for even more flexible and integrated automation engineering. With this latest software version, Simatic PCS 7 automation projects can be configured even more easily and efficiently. With Version 3, the PAA software closes the gap between plant engineering and the process control system. The entire plant structure including measuring point data can be generated easily and synchronized between the systems. Automation engineers are supported in all phases from tender preparation (such as bills of material), automatically generated process control data from electrical engineering in the Siemens Simatic PCS 7 process control system (including controlled mass data engineering), to as-is documentation of the process automation.