- Y-turning and Advanced Rapid Movement for even more machine tool productivity
- Reduced Dynamic Mode reduces wear and increases availability
- End-to-end keyboard and machine control panel portfolio from 15 to 24 inches
Siemens is expanding its
offering around the Sinumerik One "digital native" CNC. The new CNC
generation from Siemens, which was introduced to the market in 2019, is also
coming up with innovations in software and hardware this year. With the new
Sinumerik V6.20 software, there are new technology functions for the Sinumerik
One that simplify operation, reduce machine wear, and increase productivity.
Siemens is thus demonstrating once again how the powerful Sinumerik One machine
tool control system can be optimally used for digital transformation in a
highly productive, flexible, and modular way.
- Performance optimized, easy to use and future-proof servo drive system
- Flexible and compact – scalable depending on the application
- Easy engineering thanks to integration in TIA, integrated web server and one-button tuning function
With Sinamics S200, Siemens is launching a new servo drive system designed
for a variety of standard applications in the battery, electronics as well as other
industries. It consists of a precise servo drive, powerful servo motors and
easy-to-use cables and offers high dynamic performance. Applications that
require precision in speed and torque, such as winding and unwinding machines in
battery manufacturing and cell assembly, particularly benefit from the new
servo drive system. For this purpose, Sinamics S200 offers optimized speed
ripple, cogging torque compensation, 17/21-bit ST and 21-bit MT encoders, and
cycle-synchronous communication for optimized performance by
Profinet IRT in minimum 250us.
- Acquisition strengthens Siemens Mobility's
position as a leading software supplier to rail customers
- Optrail S.r.l. provides algorithms for a new
generation of optimization-based Traffic Management Systems for rail
Siemens
Mobility has completed the acquisition of Optrail S.r.l., an Italian-based
technology company, that provides unique algorithms for Traffic Management
Systems – TMS – based on mathematical optimization methods and operations
research. The acquisition complements Siemens Mobility’s existing Train
Planning System – TPS – portfolio and strengthens its position as a leading
supplier of software solutions to rail customers. Optrail
will remain based in Rome, Italy, and its technology will be integrated into
Hacon’s existing TPS products. Hacon, a Siemens Company, is based in Hanover,
Germany, and an essential part of Siemens Mobility’s software unit.
- New V6 software generation with new functions like a single positioner to reduce the load of the controller, and EtherNet/IP to allow third-party controllers to be connected
- Simulation via DriveSim Advanced enables virtual commissioning in advance, ensuring drive process requirements are met efficiently and cost-effectively
- New hardware architecture with functional enhancements like a second encoder interface and 3C3 (H2S and SO2) coating increases precision and robustness
Siemens is innovating the well-established Sinamics S210 servo drive system with a new hardware architecture and new V6 software generation that expand the system's range of applications. The servo drive system is especially suitable for applications with high dynamics in the power range between 50 W and 7 kW: for example, machines for packaging, pick & place applications, and digital printing.
- Siemens presents a new CNC for woodworking machines at the Ligna
- Sinumerik MC is the open CNC for customized processing machines
At the Ligna Woodworking Trade Fair 2019, Siemens is showcasing the Sinumerik MC control as a universal, open CNC system. Its optimized motion control, high-performance automation and the integrated Windows 10 operating system make it the ideal control, especially for wood, glass and stone cutting machines. With its open operating concept, the control system is also suitable for additive manufacturing, adhesive application, plate cutting, straightforward grinding, and laser or water jet cutting.
- Turnkey
contract to integrate the delivery and commissioning of fully automated,
driverless metro trains, digital
rail infrastructure including signalling, electrification, telecoms, platform
screen doors and depot
- Providing
latest digital products and platforms, optimizing
operations throughout the network for the trains, rail infrastructure and
subsystems
- 15-year
maintenance contract, first time usage of digital asset management applications
by Railigent X in Australia
Siemens Mobility is the system integrator and
reliable partner for on time delivery of the city-shaping project Sydney Metro
– Western Sydney Airport, the new metro railway line that will service between
St Marys, the new Western Sydney International Airport and the
Western Sydney Aerotropolis. The company has been awarded
a contract to deliver 12 automated, driverless 3-car metro trains, a purpose built
depot, the digital rail infrastructure including signalling, electrification, telecoms
and platform screen doors as well as system integration, testing and
commissioning. The company will also complete a 15-year maintenance contract.
Siemens Mobility is delivering the turnkey project as a member of the Parklife
Metro consortium with its partners Webuild, RATP Dev, Siemens Financial
Services and Plenary Group, all with strong international experience in
delivering infrastructure projects. The Siemens Mobility portion of the contract is 900 million Euro.
- Siemens Mobility supported RATP and Ile-de-France
Mobilités in the complete automation of Line 4
- Siemens Mobility fully automated the line with its digitalized
systems and CBTC signaling technology
- The automation of Line 4 will centralize control of operations, increase availability, reliability, and
capacity
The
modernization of Line 4 of the Paris Metro has been completed with the highest
grade of automation and the automatic driverless metros have now begun revenue
service. The digitalization
and optimization of Line 4 will allow RATP to safely increase frequency by reducing intervals
between trains from 105 to 85 seconds. Chosen in
2015 by RATP to automate Line 4, Siemens Mobility supplied their digitalized
communication and CBTC signaling systems to modernize the network. After a
trial run with no passengers that began in June, the automation of Line 4 is now
a reality. More automatic driverless shuttles will be introduced into the
line's traffic over time to achieve full automation by the end of 2023.
Siemens Mobility to install a 2,000 km state-of-the-art high-speed rail network that will connect 60 cities throughout the country with trains that can operate up to 230 km/h. The integrated system will create the 6ᵗʰ largest high-speed rail network in the world, and will provide 90% of Egyptians access to a modern, safe, and affordable transportation system. The fully electrified network will cut carbon emissions by 70% compared to current car or bus transport, further supporting Egypt’s efforts in transforming its mobility to a more sustainable one. Siemens Mobility will deliver 41 Velaro high-speed trains, 94 Desiro High Capacity regional train sets, and 41 Vectron freight locomotives. This contract also includes the development of eight depots and yards and 15 years of maintenance.
- New NCU 1740 for higher scalability of Sinumerik One
- Sinumerik Run MyRobot /Direct Control V2.0 and Run MyRobot /Direct Handling V2.0 available for Sinumerik One
- New functions for the Digital Twin in Create MyVirtual Machine and Run MyVirtual Machine
Siemens is expanding its offering for the "Digital Native" CNC Sinumerik One. Two years after its market launch, the technology company is presenting numerous innovations in hardware and software for the Sinumerik One at EMO Milano and the virtual Siemens Machine Tool Days. In this context, Siemens is demonstrating how the powerful machine tool controller can be used in a highly productive, flexible, and modular way and in the best possible way for digital transformation. In terms of hardware, the new NCU 1740 complements the existing NCU 1750 and 1760 as well as the PPU 1740, thus expanding its use in modular machines.
- Approximately
2,000 kilometers of modern, safe and integrated rail system to link 60 cities for people and goods across the country
- Siemens
Mobility to provide 41 Velaro
eight car high-speed trains, 94 Desiro high-capacity four car regional train
sets and 41 Vectron freight locomotives
- Turnkey
contract includes latest rail infrastructure technology, eight depots &
yards and 15-year maintenance agreement
- Will
create sixth largest high-speed rail system in the world
- To
complete all aspects of the project the consortium will create up to 40,000
local jobs
Siemens Mobility and its consortium partners Orascom
Construction and The Arab Contractors have signed a contract with the Egyptian
National Authority for Tunnels (NAT), a governmental authority under the
jurisdiction of the Ministry of Transport of Egypt, to create the sixth largest
high-speed rail system in the world. The Siemens Mobility share of the combined
contract is 8.1 billion EUR and includes the initial contract of 2.7 billion
EUR for the first line signed September 1, 2021.